Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Rubber Bands

Rubber Bands
Sales Price: 2.99 SGD
Review Rating: 3.75
4 Customer Reviews
5 star 2
4 star 0
3 star 1
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Various bonds in the room
From Japan
On 2017-02-15 08:34:16
Though it bought a thing with a wide width, it bought a thing with 11 mm, but there was a part with only 3 mm in height and things of varying thickness. I think that only the end portion is mixed, but since there are not too many numbers, I think that it would be fine if used as ordinary wheel garbage, but I will slightly dissatisfy it.
This review is about item#86323413.
Fixation of jig
From Japan
On 2016-05-30 07:57:05
It is used for fixation of burr filing. I can not cut that much, and I can use it properly.
This review is about item#86323535.
Check for stranded wire strands
From Japan
On 2015-09-17 16:06:54
There is no problem in particular. I purchased it somewhat cheaper than the nearby home center.
This review is about item#86323544.
Rubber band is turned in the gap of the groove and it is used to prevent painted tilt.
From Japan
On 2015-08-13 15:43:58
Price · Satisfaction is MAX. It seems that strength is also quite strong.
This review is about item#86323517.
Customer Who Viewed This Item Also Viewed
O Band - 100G Box
Rubber Bund,
Elastic Band
Rubber Bands 100g
O Band 500G Packets
Rubber Band Clamp
Mobilon Band
High band (rubber band)
Rubber Band
Rubber band
Color Daken device (Mr. Baginsuki)