Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Cut Resistant Arm Cover, Long

Cut Resistant Arm Cover, Long
Sales Price: 5.99 SGD
Review Rating: 3.17
12 Customer Reviews
5 star 4
4 star 1
3 star 3
2 star 1
1 star 3
The reviews are automatic translation.
Showing 1 - 12 of 12 Reviews
Steel cutting operation
4
From Japan
On 2017-09-04 09:51:26
It is good to protect the wrist firmly, but because it is thick, it is hot in the summer, so I want you to make it a little thinner.
This review is about item#86953553.
Machine maintenance, etc., DIY work in general.
5
From Japan
On 2016-12-11 18:29:51
The skin was weak, and he was frequently injured and I was looking for such a product.
This review is about item#86953553.
Weeding or seeding of 4-50 centimeters of grassroots books.
2
From Japan
On 2016-11-24 21:11:02
It is a place I want a length a little more. It will be appreciated if you provide some information such as dimensions to the item.
This review is about item#86953553.
To prevent cutting at work
3
From Japan
On 2016-07-07 12:32:55
The actual thing was much smaller than I thought. I plan to purchase anything about 3 times as large.
This review is about item#86953553.
Mechanical repair
1
From Japan
On 2016-05-26 19:58:16
In addition to the fact that the rubber part stretches only a little, when washing, the rubber will stretch to the full open.
This review is about item#86953553.
Used when processing the end material (scrap) after press-penetrating the product body from the metal plate
3
From Japan
On 2015-06-21 23:46:51
I used it when throwing out the end material after the press penetration. Since it was a sharp edging material, I used a hide, but cuts constantly bought this product, even in the upper part from the wrist. It was perfect for the purpose of use, but something a little hard. (I am not so thick) I think that it was possible to cover up to the elbow if it is about 5 centimeters more long. I think that it is hard and tight even if you connect two vertically. I think that it is 120 points if there is a length, if there is a little more stretchy way of sewing.
This review is about item#86953553.
To avoid heat in work using a heat source.
1
From Japan
On 2015-06-03 10:28:55
I bought the sample picture in spite of seeing the sample picture covering near the elbow and (trade name) (Long), but do you see it when it arrives? It is impression that it is short. Impression actually wearing and compared with the sample picture 3 to 4 cm shorter impression · · When looking at the catalog number there 17 centimeters · · It certainly was its length, but it got even shorter when washed, it got around the arm around it It is stretched and shorter, measuring 14 cm. It became a completely different feeling like a sample picture. I am wondering how I call it Long. Again, we are planning to repurchase items up to the elbow length.
Duct construction, demolition work, cutting work
5
From Japan
On 2014-07-14 10:38:09
Compared to the back of the hand, the fabric is thin, the air permeability is good in the summer, it is easy to dry even when washing. Also, it is easy to wear. There are also characteristics of flame retardancy, even in welding work and sparking flying work also entering from the cuffs to prevent burns in the upper arm and wrist is also excellent. Moreover, it is easy to purchase at half of the normal price.
This review is about item#86953553.
Packing and shipping services
1
From Japan
On 2014-05-29 16:32:09
I cut it easily with a new cutter blade. It was definitely better than one glove, but it was not as much as I thought. It was a feeling of thick denim.
This review is about item#86953553.
For dangerous work
3
From Japan
On 2014-04-14 15:16:48
I tried cutting it with a cutter, but it seems to be hard to break. It seems that if this is the case you can avoid your arm from injury. Although the size is different though it is a set of 2, there is no problem in use, but it seems that even after use, the size remains large and small, so it seems that there is no size, so this is very disappointing.
This review is about item#86953553.
Logging
5
From Japan
On 2014-03-30 18:21:01
cheap! I am saved. Although I used 100 cotton ones, I purchased it considering the safety of the chain saw work. There is no incompatibility at all like how the elongation like 7 gauge gloves. However, since the thickness of the arm side on the wrist side is also the same, stubborn people may hurt. I am considerably sunburned and it is discolored to orange. Fashionable with two tone. Lol. Kevlar seems to decrease strength considerably with ultraviolet rays. Let's buy the one who is worrisome. I am going to repeat again because I am satisfied with the performance and price.
This review is about item#86953553.
welding
5
From Japan
On 2014-03-22 05:49:02
Affordable and easy to use
This review is about item#86953553.
1
Customer Who Viewed This Item Also Viewed
Arm Protector FAL-TEKKOH
Kevlar Wrist Guards
Kevlar Arm Cover
Spectra CX Arm Protector
Pure Cotton Glove
HG 7G-Ed Arm Cover
Long Wrist Cover
Cut Resistant Wristband
Cut Resistant Arm Cover
Bamboo String Arm Cover
Cut resistant Soude cover Samitekku SX6
Kevlar supporters 7G-W
耐切 wounds supporters