Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Fixed Pulley Vertical

Fixed Pulley Vertical
Sales Price: 21.99 SGD
Review Rating: 4.82
11 Customer Reviews
5 star 10
4 star 0
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 11 of 11 Reviews
Used for vertical movement of drain pump for well cleaning
5
From Japan
On 2018-02-07 16:45:45
It is a cold season so we plan to install it around the end of March I think that it is a good product
This review is about item#88490044.
Prototype of product development
5
From Japan
On 2017-03-24 07:43:11
I thought it was a very good product because the movement is smoother than I expected. In addition, we will use it as necessary.
This review is about item#88490053.
For dam water
5
From Japan
On 2016-08-17 21:04:03
Currently in use, it has become very convenient.
This review is about item#88490053.
Measuring machine parts
5
From Japan
On 2016-08-10 14:02:44
Just because it meets the purpose, I'm repeating
This review is about item#88490123.
Drying spaces for laundry (up and down movement of the pole)
5
From Japan
On 2016-05-03 19:21:31
It was perfect for the installation place.
This review is about item#88490044.
Large hoisting mechanism using Yoshizu
5
From Japan
On 2016-04-29 16:40:35
I'm solid and red logo is also cool Pretty bridges are preventing and I am not dissatisfied
This review is about item#88490053.
Pull the southern tree.
5
From Japan
On 2015-11-30 14:34:58
In my house I have a tree of southern sky at the corner of my house from decades ago with my auspicious occasions. Since this tree hangs down by its own weight, VS50 is attached to the upper pillar with a hexagonal coach screw and fixed from the bottom through the rope to fix it on the eye plate. I am convinced that the southern skirt is also pleased that the waist is stretched.
This review is about item#88490071.
Production of a simple water meter
5
From Japan
On 2015-11-05 08:17:56
It installed in the top two of the tank. I am using the wire, but it moves smoothly and there is no problem.
This review is about item#88490053.
Button elevator
3
From Japan
On 2015-04-25 15:37:20
No problem
This review is about item#88490062.
For opening and closing
5
From Japan
On 2015-04-20 17:35:30
It was used for opening and closing the large door. I would like to use it for the interior with a beautiful appearance and a clean appearance.
This review is about item#88490044.
For turning direction towed with a winch
5
From Japan
On 2014-10-06 22:10:40
It works smoothly and can be used without problems.
This review is about item#88490044.
1
Customer Who Viewed This Item Also Viewed
Vertical Pulley Block
Hand Winch
Foxed Vertical Pulley Block
Rotary Winch
6mm, Rope Guide
Simple Type Pulley, Shackle Type
Fixed Block
Block, Wire-Rope Deck
Rope Guide, Pulley
Stainless Steel Pulley
Stainless beans block
Fixed pulley freshly-type isolation formula
Fixed pulley door roller type
Fixed Pulley Horizontal
Fixed block open type vertical type 1 car