Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of LED Indicator

LED Indicator
Sales Price: 2.78 SGD
Review Rating: 3.83
6 Customer Reviews
5 star 4
4 star 0
3 star 0
2 star 1
1 star 1
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Conduction confirmation
1
From Japan
On 2017-11-09 15:52:26
I bought it is not a product of this image, Please please past the item image you purchased. It could not be used due to insufficient strength of the connection terminals of the wiring.
This review is about item#87061082.
Indoor indicator light
5
From Japan
On 2017-05-15 23:22:03
It can work easily because 12V of the car can be used without preparing resistance as it is. Since it is a diode, of course, there is a polarity, but since I did not write it, I looked it up at the manufacturer's site. Http://sakazumeelectric.sakura.ne.jp/pdf/51_58.pdf The one with the white mark is connected to +. I think that it is more kindly, saved the trouble of checking that it is written on the product page.
This review is about item#87061091.
As a pilot lamp in the car
2
From Japan
On 2016-07-18 20:40:19
The terminal which is coming from the main body breaks from the root. I wish it had more strength,
This review is about item#87061107.
Board production
5
From Japan
On 2016-05-23 15:34:32
It is not too bright, easy to use easily
This review is about item#87061082.
Used for surface panel mounting
5
From Japan
On 2015-11-07 05:49:21
Affordable price
This review is about item#87061125.
Car and motorcycle
5
From Japan
On 2015-04-16 18:44:30
The price is also cheap, making it is also good. I want a blue color if possible.
This review is about item#87061082.
1