Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Tension Coil Spring

Tension Coil Spring
Sales Price: 27.99 SGD
Review Rating: 3.17
6 Customer Reviews
5 star 2
4 star 1
3 star 0
2 star 2
1 star 1
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
For Flexible Bag folder
2
From Japan
On 2017-11-05 15:18:50
The tonality was too strong. You still have to confirm the actual thing.
This review is about item#48818445.
Machine spring breakage
2
From Japan
On 2017-09-11 17:56:42
Though it was the same size than the one damaged, it felt a little weak.
This review is about item#48819136.
For door hinge return
4
From Japan
On 2016-10-26 23:04:57
It was saved because exactly the size I wanted is saved, but since a crochet sound comes out when the tension goes out, I want you to sell vinyl tubes that fit exactly in the sense of prevention of cissing, dirt, rust prevention.
This review is about item#48819084.
Used for machines that operate up and down
5
From Japan
On 2015-10-28 16:16:14
This tension spring was very carefully made. It was a very good product. In a bad place the place to catch is too big The spring part is short.
This review is about item#48818646.
For muscular strength maintenance rehabilitation
1
From Japan
On 2015-01-28 23:57:09
I bought 2 pieces at 1/28 cash on delivery. Free length 197.2 mm. Length under load 272.03 mm. Permissible load 140.24 N. We intend to use it under conditions. I used the two in the same way, but one of them has increased free length. I think that it is overloading about 7 mm, please tell me the environment where the free length will grow.
This review is about item#48819181.
For work at home
5
From Japan
On 2013-11-21 06:38:02
It was a bit hard, but it was nice to have a good size as well.
This review is about item#48819443.
1