Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of ABS Resin Plate

ABS Resin Plate
Sales Price: 6.99 SGD
Review Rating: 3.83
12 Customer Reviews
5 star 6
4 star 1
3 star 2
2 star 3
1 star 0
The reviews are automatic translation.
Showing 1 - 12 of 12 Reviews
Machine maintenance
3
From Japan
On 2018-03-17 20:30:06
Although the material itself is no problem, it can not be used as a decorative board. There are too many scratches.
This review is about item#88360386.
Used to make a box
5
From Japan
On 2018-02-16 08:36:57
It was easy to process and made it looks good. I will buy it again.
This review is about item#88360386.
For various works
5
From Japan
On 2017-10-27 18:47:39
Because it is so-called ABS, it is easy to process, it is also easy to bond and it is convenient to use for various things.
This review is about item#88360377.
For evaluation of ABS
2
From Japan
On 2017-07-04 12:02:05
At the time of opening, the protective film already stretched only on one side only partially adhered and almost floated. Scratches and garbage were also seen on the protective surface.
This review is about item#88360377.
For work
2
From Japan
On 2017-06-23 01:30:43
As soon as it arrives, one side has a protective seal affixed, whereas the other side is not protected at all. So it was full of scratches. It will not be usable for makeup etc.
This review is about item#88360377.
Machining automobile ABS products
4
From Japan
On 2017-06-05 12:20:50
I am using it for customizing ABS resin. Usability is good. If you desire greedy, it is the best if there is a thicker thing.
This review is about item#88360386.
As an auxiliary processing version of ABS material
5
From Japan
On 2016-08-21 12:29:34
I purchased a black thick-hearted ABS board because I can not get it easily. It is useful because it can be integrated by using special adhesive to bond the same material. Since individual packaging is only vinyl-protected on one side, it is a pity that there is a storage scratch on one side. I would like a full shrink at the time of storage / shipment.
This review is about item#88360386.
Automobile panel processing
3
From Japan
On 2016-08-19 16:13:25
It was used for panel processing of car interior. Actually it is good if there is a lineup of thickness a little more, but for now I managed somehow.
This review is about item#88360386.
Used as a base of a signboard
2
From Japan
On 2016-05-03 21:49:46
There was a problem in the shipping method and there was a problem with the packing as there was a problem with the shipping method, since the protective sheet was stretched only on one side, so the opposite side was full of scratches, ..., Absent
This review is about item#88360377.
Production of switch panel
5
From Japan
On 2016-03-26 16:15:40
no problem.
This review is about item#88360386.
Inner fender processing of motorcycle
5
From Japan
On 2015-07-13 23:52:27
It was easy to form and shape the shape and it was saved. There is no problem with bonding with heat bonding!
This review is about item#88360386.
Hinge repair of top box for motorcycles
5
From Japan
On 2015-02-27 13:09:53
I used it for the hinge repair of the top box for bike. Although the lock lever part of the hinge was worn out on daily use, it was easy to cut and polish, and it was able to repair firmly with the adhesive for ABS. When bringing it to a dealer, expenditure was exaggerated by exchanging parts, but the optimum material was found and it was sustained with only a small expense.
This review is about item#88360377.
1
Customer Who Viewed This Item Also Viewed
Polycarbonate Plate
Acrylic Plate, Black
Acrylic Board, Smorky
PVC Plate
Polycarbonate Board, Brown
PP kraft sheet
Set file 12 pcs angle rough
Nipper HF-476R corner 115mm
MC Nylon MC901 Cut Board
High software driver bit set
Polystyrene plate