Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Thrust Ball Bearings

Thrust Ball Bearings
Sales Price: 6.99 SGD
Review Rating: 3.50
6 Customer Reviews
5 star 2
4 star 2
3 star 0
2 star 1
1 star 1
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Friction adjustment
5
From Japan
On 2017-11-17 15:44:15
Although it has no groove, it can be used without problems. Although I had purchased it from the bearing shop until now, the price was upright cramped each time I placed an order. The handling here started and the price was also cheap so I switched it.
This review is about item#88926896.
A small model airplane on the horizontal axis Used gear reference diameter 10 mm and 20 mm Shaft aluminum pipe
1
From Japan
On 2017-05-30 20:53:18
Aluminum shaft of 3 mm diameter passes with F 3 - 8 ball, but two stainless steel washers? I am troubled because I do not enter the aluminum shaft.
This review is about item#88926844.
Part replacement / improvement
4
From Japan
On 2016-11-14 16:20:26
I bought it with the spacer in while holding down the frictional resistance. I felt it was a solid component though it was a small part. However, this time we could substitute for cheap polyslasher, so I would like to take it on another occasion.
This review is about item#88926896.
Used for RC def
2
From Japan
On 2016-04-06 17:12:03
I bought it for trial, but the ball is small and the Ca (load carrying capacity) is also small. It seems likely to be limited to applications with low load. I thought to buy NMB's 820 DSG and was sold much cheaper at other sites, so this time NSK's cheap items are kept just the plate and the ball part is poi.
This review is about item#88926844.
For bike cowling stem stem stay
4
From Japan
On 2016-03-15 14:50:13
I think that the needle bearing is smoother but there is no room for selection only in this item position in terms of size. Try using, there is no particular problem. The torque to be tightened was quite severe, and it was a little hard to make it run smoothly without play. I think that it is a satisfactory product in total because it is not expensive in terms of price.
This review is about item#88926905.
Manufacture
5
From Japan
On 2015-01-13 15:38:11
Since it is a maker item, there is no problem
This review is about item#88926923.
1