Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Birdie wagon

Birdie wagon
Sales Price: 309.99 SGD
Review Rating: 4.75
4 Customer Reviews
5 star 3
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
For load carrying
5
From Japan
On 2018-03-12 08:57:22
If you are looking for a wagon whose top board becomes flat it will be in this price range. I think that time loss is small when assembling after reading the instructions securely. Assembly can be done by women. Making is very solid.
This review is about item#89612101.
For on-site transportation
4
From Japan
On 2017-03-22 15:22:12
Structure is solid and excellent sense of stability. There is no problem with assembly as well. We are considering repurchasing.
This review is about item#89612117.
Electronic equipment adjustment, transportation
5
From Japan
On 2016-01-08 15:29:12
There was distortion at the corner of 1 shelf board, and we could not combine but we had to exchange immediately. Assembling with the ball point driver (4 mm) did not get too much trouble. I am pleased that movement is smooth, quiet because the caster is big.
This review is about item#89612162.
Transportation work
5
From Japan
On 2015-02-04 13:47:38
It is very solid and sturdy making. I think that it can be used for a long time. Design and color are simple and clean. The wheels are big and easy to move. Also, the sound is quiet. The only disappointing thing is that it is hard to assemble. It is assembled using bolts and nuts, but it is hard to do. I think that the shelf board is to increase the strength, but because it is woven into the back side, fingers do not enter the part to be fixed with bolts · · ·. Although it is only the first time to assemble it, I think that if it improves it is a very convenient durable good wagon.
This review is about item#89612101.
1
Customer Who Viewed This Item Also Viewed
Steel Wagon
Plus bit A-0
Steel Tool Cart
Eagle Wagon
Button lock clamper
7 pcs open wrench set