Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Handle

Sales Price: 2.99 SGD
Review Rating: 4.67
3 Customer Reviews
5 star 2
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 3 of 3 Reviews
To replace the handle of the basket
From Japan
On 2017-12-04 15:05:00
In conclusion, I decided to replace the handle of the 100 basketbasket from the front to the side. Since the handle which was originally attached is integrally molded, it has only to cut with a saw or the like, In order to reuse it we need some kind of reinforcement and it is not good. So, I cheaply found something like these two points, I decided to use this. (Size is also exactly good) I regret not being able to paste images on this review. Detailed background and completed photos such as my blog page Since it is posted in "Replace the handle of tray with tray" If you are interested please also look at that. I bought a trial and installed it, Since I can use it as expected, I repeated another one. I think that we will purchase further if necessary. In addition, since screws etc. are not attached to this handle (as expected) It enters separately. Screws with a nominal diameter of 4.0 mm pass through existing holes. Since the thickness of the threaded hole is about 5.0 mm, I think that it is sufficient to consider the length by adding the thickness of the material and the thickness of the nut (and washer if necessary). (I'm getting out on the page of Monotaro but, Looking at this product, image, It looks horrible as it is horny, There is a roundness on the inner side where your fingers hit, it is not too painful. However, since a big person with hands is cramped if I put four fingers on, I think that it will be three-hung.
This review is about item#89917152.
I installed it in a place I want to grab a bit.
From Japan
On 2016-02-15 15:20:16
Because my father's legs are lame, I have attached a handrail, but the handles I purchased are perfect for installing in a small place. My father is also pleased.
This review is about item#89917152.
Used as handle for oil cans
From Japan
On 2015-02-25 14:27:01
I used it for the lid of the oil can, but the feeling I saw seems to be robust, and it looks good after installation (* '∀ `*) b I also want to repeat if I have a chance to use something again.
This review is about item#89917152.
Customer Who Viewed This Item Also Viewed
Arch Grips
Plate Handle
Resin Handle
Resin Handle
Resin Handle
UPC plastic cabinet handle
Bridge Handles
Plastic Cabinet Handle
Saddle (for the mall duct)
Arch grip AGS-N
Plastic Drawer Pulls
Mall duct accessories saddle
Box-shaped handle
PC mirror