Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Nagara uprooted most

Nagara uprooted most
Sales Price: -
Review Rating: 4.12
8 Customer Reviews
5 star 3
4 star 4
3 star 0
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 8 of 8 Reviews
Used for taking weeds
2
From Japan
On 2016-11-10 06:55:16
The roots remain on the cutting edge, and it is troublesome to take one by hand.
This review is about item#1036166.
Weeding in the garden.
4
From Japan
On 2016-10-04 07:34:53
It is effective to use it when the soil is soft, such as rain. You can take it to the grassroots.
This review is about item#01036166.
Weeding in the garden
5
From Japan
On 2016-08-11 16:29:19
It is the highest for the grass that spreads out horizontally It is a little tight for the grass that grows vertically It seems to be able to cope with any kind of grass if there is little more power
This review is about item#1036166.
weeding.
5
From Japan
On 2016-07-09 23:27:12
Is the angle bad? Bad usage? Is it? Is it?
This review is about item#01036166.
Weed control
4
From Japan
On 2015-12-03 15:50:02
It is also easy to hold out with pulling out used for weed control and workability is also good.
This review is about item#01036166.
I used it to weed the vacant lot
4
From Japan
On 2015-08-15 00:32:15
If weeds are growing in some places, you can grass them to pull out with hands. However, in the dense state it was insufficient and we did not compete against the fuselage of the agricultural tool.
This review is about item#01036166.
Weeding of fields
5
From Japan
On 2015-06-13 23:55:16
I tried to use it immediately after goods arrival. This product was able to pull grass well among leaves and extract relatively large grass as well as root. The angle of the blade also cut into my height and cut in a lot. I will continue to patronize from now on.
This review is about item#01036166.
Without weeds in the garden
4
From Japan
On 2015-05-17 22:40:23
It is planting roses in the ground, because we give fertilizer frequently or weed growth is momentary momentum. That point is very easy, as the weeds escape while standing. However, I think whether to use a little trick in usage. If weeds are difficult to pull out on dry soil, dig it so that it gently scraps the soil around the base of the blade, then dig it out crowning around the edge of the blade perfectly. On the contrary, work with the soil moist is easier to pull out, but requires strength with the weight of the soil. After that, if you draw 3 or 4 times in either case, you can not take it any further unless you grasp the grass that has passed through between the blade and the blade by hand. But it's about 5 seconds. Also, since this item has this shape, I think that it can be used only for right-handed people. I think that it is a very handy item for those who are right-handed, crouching down and working hard.
This review is about item#01036166.
1