Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Straight Carbide Drill

Straight Carbide Drill
Sales Price: 4.99 SGD
Review Rating: 4.00
7 Customer Reviews
5 star 2
4 star 4
3 star 0
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Drilling of sheet glass
4
From Japan
On 2018-01-23 14:44:30
I used it to make a hole in 3 mm thick transparent plate glass. I poured water on the ordinary drilling machine at a low speed, but it was able to be more stable than I thought. The rest is durable.
This review is about item#1037173.
PCB hole drilling
4
From Japan
On 2017-11-12 16:37:58
It was very good to use The storage case was somewhat hard to open
This review is about item#1037006.
Plastic model production time
5
From Japan
On 2017-10-12 14:48:03
Various wires are attached to the wiring and piping of the engine at the time of making the model of the car by the car, but this drill is used because it is difficult to pass through the drill hole with the same diameter as the wire. Work efficiency is considerably different only when the hole diameter is 0.05 mm larger. I am using it pleasantly.
This review is about item#1036997.
Drilling of soda glass
4
From Japan
On 2017-08-06 21:01:59
I attached it to a drilling machine and used it at low speed. It was used to process plate-like glass with a thickness of 2 to 3 mm. It can be used for 70 glass processing per drill.
This review is about item#1037164.
At work
2
From Japan
On 2017-08-01 10:43:49
I felt the sharpness was very good, but it got damaged. I thought it would be nice if the price got a little higher but it was a bit more robust product.
This review is about item#1037085.
Drilling of photosensitive substrate
5
From Japan
On 2016-06-05 14:08:30
As expected it is the quality of a brand item. Moreover, with a rugged case, it is a thought that you can protect precision cutting edge. That's an exception! If it is about to be used on a photosensitive substrate (glass epo), there is no spilling of the blade until I die (laugh)
This review is about item#01037015.
For drilling glass epoxy board
4
From Japan
On 2015-08-12 09:51:21
I bought it for processing of glass epo. Until now I used a drill for ironworkers but switched to this item. The quality of ordinary drill and glass eep processing is unchanged. However, the trouble of replacing the drill blade has been reduced. I am using 0.8, 1.0 and 1.2 mm drill blades, but that point is convenient as the length and mounting diameter are the same. However, if the drill blade is very fragile, hit it for a moment or hook it, the blade edge is blistering. Please take care.
This review is about item#01037252.
1
Customer Who Viewed This Item Also Viewed
Micro drill for steel
Standard drill STC
Micro drill MD
Precision Drill
Drill MD
Precision Drill
Small Diameter Drill
Infinite miniature drill
Carbide drill coating drill
Micro Drill 3-pcs
High Speed ​​Drill
Micro Carbide router
Micro carbide end mill