Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Double Ring Grip

Double Ring Grip
Sales Price: 17.99 SGD
Review Rating: 2.80
5 Customer Reviews
5 star 1
4 star 1
3 star 1
2 star 0
1 star 2
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
I exchanged the grip
5
From Japan
On 2017-06-25 21:22:37
I bought it for grip exchange of my old bicycle, so I replaced it immediately and it was fixed easily It was good. Although it was cheap, I used detergent to improve slippage and then inserted it into the handle pipe, but this time it was possible to fix the plug in as it was.
This review is about item#1215122.
Grip exchange
3
From Japan
On 2017-02-04 14:28:23
It is easy to use because it can be used for grip exchange, but the grip force is weak.
This review is about item#1215156.
Because ergo grip got older, I changed it
4
From Japan
On 2016-10-11 09:56:30
The inside of the grip can be installed easily because it is a tubular shape of a plastic. The aluminum ring will be slight accent. However, a narrow hexagonal wrench is required for tightening. This time it was still long even with the short type so cut one side with a cutter and installed it. (One side of the lock ring will be decorated.) We do not recommend, but even with the tightening of one of the lock rings it does not move or slip with commuting only use.
This review is about item#1215138.
For replacement
1
From Japan
On 2016-09-22 21:51:55
Within less than a year, the color of the ring is bald and the rubber is aggressive and stinky.
This review is about item#1215138.
Bicycle maintenance
1
From Japan
On 2015-09-29 12:34:16
The quality of rubber is bad. After about six months past the summer, the rubber melted, became greasy, and cedar eyes also disappeared.
This review is about item#01215217.
1
Customer Who Viewed This Item Also Viewed
Grip
Sport Bike Grips
Double Ring Grip
JACK3 shield
840/2Z bit
NEW grip
Easy Grip
Double Ring Grip
Sports Grip
Sport Bike Grips
Bike Grip 125