Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Front Basket

Front Basket
Sales Price: 38.99 SGD
Review Rating: 4.50
4 Customer Reviews
5 star 2
4 star 2
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Existing basket was shallow and replaced
5
From Japan
On 2017-12-17 15:00:03
There was also the depth of the basket, so it was better as the strength was firmer than I expected. Installation was also easy.
This review is about item#1215497.
Exchange for old wizzy basket
4
From Japan
On 2017-06-01 16:30:04
I replaced it with a steel wire basket that was easily deformed and rusty. "OGK" of the manufacturer is also famous, and the construction is also solid as it is, but thought that it was good even a little bigger size. At the same time, the back basket was changed to "RB - 005" made by the same OGK, so unified feeling was born in colors and styles with front and rear baskets and the appearance became very good. Since I am parking outdoors, I'd like to expect durability.
This review is about item#1215506.
Maintenance of the city cycle
5
From Japan
On 2015-12-02 13:59:28
It was rusted by the default metal and it looked rusted and it was replaced from this something unreliebable to this product, it was made of resin and light and rusted, and the handle became lighter. Also, it is a product of a manufacturer making sports cycle helmets so I am satisfied with being strong.
This review is about item#01215497.
Exchange due to aging of metal basket
4
From Japan
On 2014-08-24 16:44:35
Rust develops immediately due to scratches or the like in a metal case, but since it is made of plastic, there is no worry of rusting. Since the mounting part is poor, it is perfect if there is improvement on that part. I feel that the size is reasonable.
This review is about item#01215506.
1
Customer Who Viewed This Item Also Viewed
Plastic Basket
Large Plastic Basket
Front Basket
Front Basket
Bike Basket Mesh
Stainless Wire Baskets Type D Type 02
Mesh Bike Basket D
Stainless Bike Basket
Stainless Steel Wire Basket Round
Decoration cake mold for laid paper
Round Type Wire Basket
Front Basket
Small Basket
Plastic Front Basket