Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Stainless Round Bar Drawer Pulls (Female Screw)

Stainless Round Bar Drawer Pulls (Female Screw)
Sales Price: 3.99 SGD
Review Rating: 4.50
2 Customer Reviews
5 star 1
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 2 of 2 Reviews
Sus Product lid handle
4
From Japan
On 2016-06-29 23:27:39
The polishing was also beautiful and very good. It was good that there was no stud bolt that would become unnecessary in length. I am satisfied that the dimensions are out crisply and cheap. I was glad that nothing wastefully stamped
This review is about item#01466797.
Bathroom folding door handle repair (replacement)
5
From Japan
On 2015-12-26 19:10:10
Because the handle on the bathroom side of the folding door of the bathroom made of resin parts and aluminum parts was broken, I replaced it. With buff finish of stainless steel, it is very beautiful, even if the bare skin touches it is totally safe and no problem. It looks like a handle for larger things, but it was perfect for size as well. Next time, I think that the handle will not break even if the door breaks. It is a somewhat difficult point for cold to touch in winter if you do not hang it with hot water, but this is inconvenient. Since screws are not attached, attention is necessary, but if prepared according to the purpose it is really good without waste, since the screws of the selected monotaro were 5 sets, it was left over. It is a bit disappointing.
This review is about item#01466763.
1
Customer Who Viewed This Item Also Viewed
ABS Chrome Handles
Panel Handle
Stainless Panel Handle
UNF U-Handle
Handle
Guard Handle
Handle With Stainless Guard
Panel handle (female thread) PHPF
Stainless Round Bar Drawer Pulls (Male Screw)
Shaft diameter with shaft 6 mm