Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Silicon rubber sheet hardness 70

Silicon rubber sheet hardness 70
Sales Price: 3.99 SGD
Review Rating: 4.83
6 Customer Reviews
5 star 5
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Press bending
5
From Japan
On 2018-02-02 15:16:56
It was good even if it was a bit larger, perfect for bending without hurting
This review is about item#2100376.
Processed as a master of rubber molded products
5
From Japan
On 2016-08-29 10:54:47
Hardness is also moderate, easy to cutter and engraving blade processing
This review is about item#2100516.
It laid it in the table of the examination room
5
From Japan
On 2016-08-24 16:13:57
I did not want the tip case to move during pipette operation and I tried laying it. It is very nice to have a firm anti-slip and not move what you put. Because it is silicon, it is easy to disinfect the desk strongly against chemicals. Silicone sheets are sold even for hundreds, but thickness and thing are different. I thought it was good to buy.
This review is about item#2100498.
Prototype of new products
4
From Japan
On 2016-07-18 20:58:47
I received what I was imagining. However, although it was rolled up and sent at the time of delivery, things of this kind can not take a rounded habit easily, so I would like to make an improvement.
This review is about item#02100394.
Antiskid when transporting aluminum panel
5
From Japan
On 2016-05-16 01:48:39
Hardness is 70, but when transporting aluminum panel, adhesion is good, NBR (nitrile rubber) sheet white hardness 65 (00001112) It does not slip.
This review is about item#02100656.
As a cushioning material for joint parts around motorcycle engine
5
From Japan
On 2015-09-28 14:31:57
There was a part around the engine of the old car around the engine, there was a part made of silicone rubber sheet as a cushioning material, but already manufacturers have parts missing and it seems that they are looking for second used parts etc Since it is not, I tried reproducing it by replacing the silicone rubber sheet which became useless. I actually tried using it, it was easy to solve it without problems at all. Here, rubber sheets of various thickness, size and hardness are stocked, it was good that we could procure material much easier than going around the home center and the electric material store.
This review is about item#02100516.
1
Customer Who Viewed This Item Also Viewed
Silicone Rubber Sheet
Silicone Plate
Silicone Rubber Sheet, 0.5mm
Silicone Rubber Sheet, 5mm
Silicone Rubber Sheet, 3mm
Silicone Rubber Sheet, 1mm
Silicone Rubber Sheet
Silicone Rubber Sheet, 10mm
Valflon sheet
High-strength silicon sheet
Colorful sponge round sheet
Hydraulic reserver for PV411 (100cc)