Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Weight Roller

Weight Roller
Sales Price: 23.99 SGD
Review Rating: 4.50
2 Customer Reviews
5 star 1
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 2 of 2 Reviews
Used for address V 125
5
From Japan
On 2016-06-03 11:18:26
I used it for address V 125, I feel I'm getting better, cheap and good.
This review is about item#03421023.
I installed it in domestic specification of Signas X.
4
From Japan
On 2014-10-19 07:24:37
Although a genuine weight roller looks like "11.8 g", it is disappointing with the same acceleration as moped at the time of signal dashing. Taiwan specification is early! When asked on the net, the weight roller of Taiwan specification was "9 g". Well ~ If you set the same 9g the acceleration will get better! And I bought it quickly. Reliability was the reason why we chose KITACO 's weight roller. Is not it? But I was worried because the price is high, but it is first and reliable? Decided to purchase at. Usage report Feeling that it gently accelerates to the 50 Km level at 5,000 rpm ordinary acceleration genuine. After exchanging, it felt that it gently accelerated to the level of 60 Km at around 6,500 rpm. Acceleration at full throttle When this is genuine It is fully open, is not it? A sense of acceleration. . . After exchanging ~ wow ~ early! Masculine Bye Bye! is. Disadvantage Fuel consumption genuine about 30 Km Replacement about 23 Km Conclusion Personally, high rotation in the low speed range is somewhat disgusting, so we are planning to replace "10 g" weight rollers. This KITACO weight roller has direction. Let's exchange it so as not to make a mistake. Weight rollers can be relieved to buy reliable KITACO made after setting is decided.
This review is about item#03420926.
1
Customer Who Viewed This Item Also Viewed
Weight Roller
Weight Roller
Sealed Chain 525ZVX3
Weight Roller
Weight Roller
Weight Roller
Slider
Weight Roller
Waitroller
Super Roller Set