Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Super Roller Set

Super Roller Set
Sales Price: 13.99 SGD
Review Rating: 4.20
5 Customer Reviews
5 star 4
4 star 0
3 star 0
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Periodic exchange
5
From Japan
On 2017-06-03 15:18:23
Used for CA1PB ZZ. Replaced with the same weight as genuine Durability is no problem so use as a substitute for genuine It is saved because it is cheaper than genuine It is a plane of delivery, although it should have been asked in the same delivery as other driving system products, but only Kore There was no contact, another day I entered the post instead of the courier I did not properly check the inside of the box, but I was also bad, but since there was no contact, I think that it is complete and I open the crankcase I noticed just before it was a dangerous place twice so I'm worried about next shipment as well
This review is about item#3433727.
Scooter Maintenance
1
From Japan
On 2017-05-30 14:43:05
I wrote 4th, but it was sending out after 1 week. It was late because everything was shipped in bulk. Previously, although it was inventory, it was canceled as if it was not there, it was informed only by e-mail. goodbye.
This review is about item#3432957.
For Commuting Today AF61
5
From Japan
On 2016-09-29 18:02:38
It used to be used with high speed pulley Kit was Donpitsari! My weight is 60 kg. The rollers are also 5 g × 3 in KITACO and 6 g × 3 in a total of 33 g, and the maximum speed is 55 km which is the same as normal but the acceleration is surprisingly surprising. (Just fuel mileage got worse enough to surprise but ...) All others are normal, but just by exchanging pulley KIT and rollers, it is so much faster and satisfying.
This review is about item#3432783.
Mission maintenance
5
From Japan
On 2016-05-23 15:48:06
Since it became old, I do not know the difference between before and after exchanging, but I'm comfortably posting it
This review is about item#03433002.
Replacement of consumables
5
From Japan
On 2014-11-23 14:24:53
Up to now I was using 3.5 g about 5000 K, but since the replacement time has come, I changed it to 4.0 g. 3.5 g had quite a bit of vibration, so we thought it would be reduced even a bit and thought 4.0 g was chosen. Weight increase of only 0.5 g, but I hope the balance between acceleration and maximum speed will not collapse!
This review is about item#03432485.
1
Customer Who Viewed This Item Also Viewed
Weight Roller
Weight Roller
Weight Roller
Long Throttle Cable