Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Thickness Gauge 25 Mai set

Thickness Gauge 25 Mai set
Sales Price: 17.99 SGD
Review Rating: 4.33
3 Customer Reviews
5 star 2
4 star 0
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 3 of 3 Reviews
When replacing the plug etc
5
From Japan
On 2017-10-27 14:46:28
For example, when you want to measure 0.75 mm, Usually we combine two 0.7 mm and 0.05 mm gauges, Since this gauge can be measured with a single 0.75 mm gauge, very convenient.
This review is about item#3990534.
Tappet adjustment
5
From Japan
On 2015-08-31 14:07:41
There are many inexpensive ones, but I bought 25 sheets that can make many combinations. If you are maintaining for many years, the thickness gauge has its own preference (shape / external size). This size is the most refreshing.
This review is about item#03990534.
Maintenance and adjustment of motorcycle engine
3
From Japan
On 2015-08-30 08:20:09
Although it purchased for the first time, there was a width than I expected, and it was unsuitable for measuring a fine place like a motorcycle. By the way, in Honda's 50cc 4-stroke vertical type, its use with a tappet was too bad and could not be used to measure points. Also, if there are only a few sheets used for measurement, it is a little troublesome that the number of sheets is large. Other than that I do not have any particular dissatisfaction, but I also felt that I should choose the one that suits my intended purpose.
This review is about item#03990534.
1
Customer Who Viewed This Item Also Viewed
Thickness Gauge
Jis Equivalent Product Thickness Gauge
Thickness Gauge
Thickness Gauge
Thickness Gauge
Tactile Push Switch
Thickness Gauge
Mini racing grip
Thickness Gauge Set, 12.7 width
Thickness Gauge
THICKNESS GAUGE
Thickness Gauge
Thickness Gauge set