Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Ballpoint Pen

Ballpoint Pen
Sales Price: 2.99 SGD
Review Rating: 4.36
11 Customer Reviews
5 star 7
4 star 3
3 star 0
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 11 of 11 Reviews
Write to drawing
4
From Japan
On 2018-04-17 15:40:43
Convenient when you want to write in the blank part of the drawing in detail. It seems that hands are also thin, so it will not fit the hands like gloves of craftsmen. I got punyuguri attached, I am satisfied rightly.
This review is about item#8529623.
Used in several types of color coding for notebook entry
5
From Japan
On 2018-04-01 17:17:51
I used 0.5 mm from the front, but when I borrowed 0.38 mm used by the acquaintance, I bought it because the pen running was well well grasping feeling. There are color variations, I got lost to choose. When I actually purchased it, I felt satisfied because I felt something wrong with the colors I used.
This review is about item#8529605.
When writing in the notebook.
5
From Japan
On 2017-12-07 03:42:10
Because it is a thin pen, it is convenient for a narrow notebook to write. Also, since it is friction, if you write it by mistake, you can erase it, there is no worry that the notebook will become dirty with correction tape. However, it is regrettable that it is easy to blush, although it is a thin pen. It is a ballpoint pen I want to keep favorite from now on.
This review is about item#08529605.
During office work
5
From Japan
On 2017-04-27 14:36:12
I have used many types of color, I can write it and erase it as a ballpoint pen I like it very much.
This review is about item#8529684.
Notes
5
From Japan
On 2017-03-27 08:12:39
I am grateful to you for finding it without looking for it. I am glad that there are many variations to handle. Goods could be used without problems.
This review is about item#24341162.
Studying the qualification exam
5
From Japan
On 2016-09-29 17:30:09
Ideal for writing in a detailed learning map. It was thin and difficult to hold because the hand was large, but if you put the child's pencil's rubber from the top, it is perfect and dissatisfaction is dissolved! It is!
This review is about item#8529623.
Office work
1
From Japan
On 2016-06-27 16:15:29
I purchased thought that it was the same as what I purchased before but the body is too thin to write hard. The pen tip is too hard.
This review is about item#08529605.
The taste of writing
4
From Japan
On 2016-04-15 16:46:48
Although it is good, the body slides thinly. It's tired when power is turned into strange if it's work to write for a long time. Please make a grip or rubber attachment by all means.
This review is about item#08529605.
Use at work
5
From Japan
On 2015-12-27 08:31:56
I thought 0.5 mm was a bit thick, but 0.38 is perfect for the application. It was good.
This review is about item#08529605.
For thin writing
4
From Japan
On 2015-11-06 10:02:15
It is satisfying to write thin. I felt that 0.5 mm friction was easy to write.
This review is about item#08529605.
It is a schedule, schedule.
5
From Japan
On 2015-06-25 16:46:02
It is optimal because it becomes a notebook that you can understand even after seeing it without being crushed because changes frequently occur. It was developed well.
This review is about item#08529614.
1
Customer Who Viewed This Item Also Viewed
Friction Lights
Correction Tape
Carpenter Saw Spare Blade
Ballpoint Pen Refill
Correction Tape Cartridge
Flange full surface packing (VALKARON gasket)