Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Drawn cup needle roller bearings

Drawn cup needle roller bearings
Sales Price: 2.99 SGD
Review Rating: 4.14
7 Customer Reviews
5 star 4
4 star 1
3 star 1
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Honda 6 bolt 4 L Monkey engine internal parts exchange
5
From Japan
On 2017-10-23 21:50:58
It is used for the bearing of the mission which is driven (press-fitted) into the crankcase with the engine of 6 volt Monkey, so it is genuine and no parts are set, so one of 2 needle roller bearings is this size. The other one is a special size, so use genuine parts for another car (MD90). Originally it was the same manufacturer as the bearing which is genuine installed by the manufacturer. Therefore, reliability will not be a problem either.
This review is about item#12136784.
Bearings for variable speed pulley of Proxon milling machine
4
From Japan
On 2017-05-16 20:58:50
I used this for exchanging plain bearings with inner diameter 8φ and outer diameter 12φ, but I think that the outer diameter dimension was just as good as 2/100 mm, so that it can be press-fitted. The inner diameter dimension was a little big, and the shaft was able to rattle. The sound became larger compared to plain bearings.
This review is about item#12136687.
Exchange due to wear of the bearings of the printing press.
2
From Japan
On 2016-11-23 23:03:51
In the image photograph of the homepage, since the oil hole was opened, I thought that there was an oil hole and bought it. However, there was no oil hole in the commodity that arrived, and it was regrettable that there were restrictions on the place of use and it remained.
This review is about item#12136802.
As a DIY
3
From Japan
On 2016-08-08 20:37:52
It is good for cheap price. It is made abroad but there is no problem.
This review is about item#12136723.
Component replacement
5
From Japan
On 2016-02-19 11:53:16
It was a great help to buy small parts that I gave up from one piece.
This review is about item#12136784.
As a machine part
5
From Japan
On 2015-11-30 14:13:03
Satisfied with all the price etc.
This review is about item#12136732.
As a machine part
5
From Japan
On 2015-11-30 14:13:03
Satisfied with all the price etc.
This review is about item#12136732.
1