Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Freestanding cross bag

Freestanding cross bag
Sales Price: 27.99 SGD
Review Rating: 4.40
5 Customer Reviews
5 star 3
4 star 1
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Garbage collection in the landscaping industry
From Japan
On 2017-11-29 15:19:38
The size, hand-held part seems not to be dangerous as the autonomous method protrudes like a steel rod with a rope type without any problem. Since the fabric is single except for the bottom, how tight is it
This review is about item#19067922.
Transport of cookware
From Japan
On 2016-08-05 14:05:15
I used it for moving cooking utensils by moving. It was solid and easy to use because it does not break like a plastic bag.
This review is about item#19067913.
For cleaning the fallen leaves etc.
From Japan
On 2016-06-07 07:10:58
There are various products from self-standing bags from each company, but the material and arrangement of framework for independence are different for each product, there is a big difference in feeling of use. Especially, the type using steel bone is deformed during use, so I definitely want to avoid it. So I would like to specify the bone specification in the product description. In this product, the FRP bone is contained only in the four sides in the longitudinal direction, and the four sides of the opening are the type in which the rope is sewn. Because of this, self-sustenability is inferior compared with other types made by other companies, which also has FRP core in its mouth (Japan Matthew's Garden BAG etc.), so the shape of the mouth tends to collapse, so it may take time to put in fallen leaves , As with the thing of the total FRP core, there is an advantage that trouble such as the bone jumping out when it becomes old is also unlikely to occur, is both good and bad. The type of folding is similar to the way folding paper bags, it takes a little more time than the total FRP type, and it feels a little fitting due to the repulsive force of the rope. The body and the fabric of the belt seems to be relatively thick and durable.
This review is about item#19067922.
From Japan
On 2016-05-24 18:55:38
It is easy to put in garbage and clean up can be done quickly,
This review is about item#19067922.
It is used for withered leaves and grass collection in agricultural work.
From Japan
On 2016-04-19 22:20:26
Since it is self-contained, the amount also enters, and it is very useful to keep it as it is, such as rainy weather the next day.
This review is about item#19067922.
Customer Who Viewed This Item Also Viewed
Large Sandbag, Square
Condor Dedicated Dust Cart Bag Large
Carrier Bags
TRUSCO Work Bucket
Wonder Hooton
Power BAG
Garden Bag
Foldable Collection Box
Heal Kyokabe
Large Trash Bag
Waste Container 450L