Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Hand wrap

Hand wrap
Sales Price: 17.99 SGD
Review Rating: 3.86
7 Customer Reviews
5 star 5
4 star 0
3 star 0
2 star 0
1 star 2
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Cleaning of precision parts
5
From Japan
On 2018-01-02 10:20:39
Alcohol rises unexpectedly, but there is no problem in use if you get used to it. It is better to put some marbles in order to bulge the liquid level.
This review is about item#20420672.
When washing parts
5
From Japan
On 2017-09-17 21:28:14
Put alcohol and use it when cleaning parts and boards. If it is a 150 ml type, I think that there is nothing to say that the movement of the moving part is poor as pointed out by other people. The real logo is different from that of the picture, it is written as a hand wrap with a retro font.
This review is about item#20420672.
Oil soiling wipe of precision parts
1
From Japan
On 2017-08-25 11:47:43
It is hard to use. Pushing the pump may stop and not come up. I think that it is better to refrain from purchasing because there is no returned goods correspondence
This review is about item#20420663.
Precision Equipment Part Assembly Adjustment
1
From Japan
On 2017-08-18 13:05:39
I purchased it because I wanted something more expensive than other companies' products of the same capacity but more easy to use. But even if you push the silver part above the good or bad sucker, it will not move smoothly as if it were Bali. If I do not do it, I will not go down to the bottom. If I do it several times ... I thought it was not at all. It was a product that could not be returned although it may have been a loser. I realized that it was better to think and purchase products that are not sale or cheap but can not be returned
This review is about item#20420663.
Lens cleaner
5
From Japan
On 2017-01-31 09:18:38
The seal affixed to the surface of the product was good, but it was not affixed. However, under the old Showa typeface, it may have been rather "handwrap" written. The product can be used normally, feeling that the pipes in the inside are solid and firm. I knew that it would be nice to put marbles so that they can be used even with a small capacity, but we have increased the parasol with a crystal blanket in our house. It is still better if it does not evaporate spontaneously, but since it is just after purchase it is now.
This review is about item#20420672.
I will use it at work
5
From Japan
On 2016-10-26 06:24:42
This time, I think that it is very easy to use. Since the maker is also different from the previous one, I think that I want to use it with confidence.
This review is about item#20420672.
Allow alcohol, acetone and so on to penetrate the tissue and use it to wipe dirt
5
From Japan
On 2016-05-25 14:36:13
This product is good because the tube part sucked in is made of metal. If other products made of resin, acetone or the like is put in, it will melt or come off.
This review is about item#20420672.
1
Customer Who Viewed This Item Also Viewed
FINE Hand Lap Glass, Pump Dispenser 300mL
Scissors
  • Scissors
  • CROWN (Office Supplies)
  • 7.99 SGD
Hand Lap, Glass, Pump Dispenser
Hand wrap SCC
Polyethylene Hand Lap, Pump Dispenser
Clean Pot
Fairy Rose Wokkupan
Drawing sentenced circle , small 400 g
Hand Lap, Glass, Pump Dispenser