Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of T Slot Nut

T Slot Nut
Sales Price: 3.99 SGD
Review Rating: 4.00
11 Customer Reviews
5 star 6
4 star 2
3 star 1
2 star 1
1 star 1
The reviews are automatic translation.
Showing 1 - 11 of 11 Reviews
Change the movable part of the vice of the disc grinder stand
3
From Japan
On 2018-05-18 22:35:58
Purchase the second time in another size. The surface finish is dirtier than the first time. You can clearly see the remaining steps after the blade. The width of the lower row is 16.2 mm The width of the upper row is 9.8 mm (caliper measurement) The 0.2 mm difference in dimension display is slightly larger. Chamfer processing of corners is absolutely none, leaving sharp corners. The lower stage is polished about 0.4 mm and used. Chamfer is also used for further processing. There seems to be a difference depending on the product lot. The hole in the center is M8. I am in trouble because I can not fix the large crossing with minus crossing in the dimension description of professional materials. It is saved if there is a little more accuracy.
This review is about item#20320073.
Mounting on a milling stand etc
5
From Japan
On 2018-03-03 15:51:12
It was completely different from the previously purchased T slot nut, it was able to be used uncensored, the former used to take in the face to get in the milling stand, it was comfortable to use this time.
This review is about item#20320073.
Mold fixing
1
From Japan
On 2018-01-24 09:18:05
It is NG with apparent quality. It looks like rusty, and when I inquired, it was about attachment of cutting oil. I purchased it from various traders until now, but such an article is the first time. I hope improve the appearance quality.
This review is about item#20320082.
Radio controlled parts production on desk milling machine
4
From Japan
On 2017-11-29 18:39:23
It was used for fixing a vice and a rotary table on a desk milling machine. Although it is my first use, I think that it was good even if it was one larger size. Up to now it was a thing I made my own but it takes time and effort to make it so easier to buy it.
This review is about item#20320073.
Purchase 4 pieces as a bench for desktop drilling machine DP2250R
5
From Japan
On 2017-03-11 16:23:45
It is more beautiful finish than the photo, it does not matter as it is dimensioned. Since it is strong enough for fixing the vice, it is fixed with two bolts.
This review is about item#20320082.
Work fixing for milling work
5
From Japan
On 2016-11-03 00:45:28
It is helpful to have a type with short longitudinal direction also in the line-up. If you have a rotary table that is as small as DIY, the T slot is so short that you can not replace the stud bolt close to the workpiece.
This review is about item#20320098.
Fix to prevent distortion by welding
5
From Japan
On 2016-09-29 17:42:18
I think the tap of the moment screw or worse may have not done so
This review is about item#20320134.
For fixing the slide table and the vice
5
From Japan
On 2016-06-07 19:10:04
I am using it without problems. I think that it is a good product.
This review is about item#20320107.
Mold fixation to press machine
2
From Japan
On 2016-05-17 16:37:58
Although it seems that there is no problem in terms of function, the quality of cro-dyeing is glossy and not very good.
This review is about item#20320134.
Creating Jigs
4
From Japan
On 2016-04-21 15:07:56
It is cheap, so I am satisfied because I can get it in a small amount.
This review is about item#20320082.
Fixed table
5
From Japan
On 2016-04-11 11:28:04
Especially it can be used without problems.
This review is about item#20320082.
1
Customer Who Viewed This Item Also Viewed
T Slot Bolt
Square-Shaped T Slot Nut
T-Slot Nuts
Stud Bolt
Uni Clamp
T Slot Nut
Step Clamp
T-Slot Nut
T-nut (iron / cloth)
T slot Nut penetration item
BJ749 T-slot nuts
T-Nut Material
PADS FOR SCREW JACKS
Panel holding plate (one-sided)
Flange Nut
Stud Bolt
T-Slot Nuts