Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Stainless steel ring catch

Stainless steel ring catch
Sales Price: 4.99 SGD
Review Rating: 4.71
7 Customer Reviews
5 star 5
4 star 2
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Chain connection
5
From Japan
On 2017-11-24 17:55:47
No problem if ordering after checking dimensions when ordering.
This review is about item#21036557.
To prevent falling off.
5
From Japan
On 2017-11-02 21:53:07
Although it sells also at a home center, when thinking to purchase more than one, the same thing is not got because there are no numbers other than it! Although it depends on the size, since there is not much tensile strength, it is not recommended to use the place where the load is always applied, but it is used with the wire to prevent the tool and tool from coming off.
This review is about item#21036548.
Grass kieper fall stopper
5
From Japan
On 2017-10-11 16:10:11
It is convenient to utilize for falling slip of the glass keeper.
This review is about item#21036566.
Good quality
4
From Japan
On 2017-04-26 14:31:47
Although it can be used without problems in particular, Mizumoto made cheaper than the equivalent one.
This review is about item#21036557.
To consolidate.
5
From Japan
On 2017-04-22 20:30:46
It is used for the connection part, but basically it does not desorb and it is a basic direction and it is basic death. It is smart in appearance and convenient for root saving of chain.
This review is about item#21036548.
Connection between antenna rotation stay and wire rope
5
From Japan
On 2017-04-09 17:58:34
It is made of stainless steel, it is resistant to corrosion and the part of the screw also has good quality
This review is about item#21036566.
Tie of chain of gate
4
From Japan
On 2016-10-14 16:30:23
I use it without any problems. I do not know about durability yet.
This review is about item#21036557.
1
Customer Who Viewed This Item Also Viewed
Ring Catch, Regular Type
Ring Catch
Quick Link
Strong ring catch
Waverly ring catch
Stainless Ring Catch
Steel snap hook
Stainless steel ring catch
Stainless freely band
Kewpie Key Holder
Stainless steel ring catch
Individual folder B5