Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Flare piping set wire with

Flare piping set wire with
Sales Price: 79.99 SGD
Review Rating: 3.25
4 Customer Reviews
5 star 2
4 star 0
3 star 0
2 star 1
1 star 1
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Air conditioner new installation, exchange
2
From Japan
On 2017-07-31 20:55:56
Those necessary for air conditioner installation work are all packed for each piping distance, which is very convenient for those who do not construct large quantities. However, although I bought a set of 7 meters this time, when I opened it at the work site, there was only 3 m of drain hose. It is a shortage that is also short for 4 m equivalent to standard construction. Regardless of a set mistake, we can not understand if this is the original product composition. Is it meant to drain the drainage in the middle of piping? Running to buy a hose for extension in the middle of the construction, I decided to spend extra time and effort instead. It is a very convenient product, so I would like to strongly ask for improvements.
This review is about item#22911954.
Cooler replacement
5
From Japan
On 2017-07-14 16:16:34
All necessary items for piping work were included and it was convenient and good.
This review is about item#22911936.
Air conditioner installation work
5
From Japan
On 2017-04-09 13:46:52
The handling of construction was soft, plumbing · electric construction was easy to do and was the best.
This review is about item#22911945.
Home air conditioner DIY installation
1
From Japan
On 2017-01-04 20:50:38
Previously it was a home center, I was purchasing, usually the length of high pressure, low pressure is different, but this item is the same length, so connection can not be performed cleanly
This review is about item#22911927.
1
Customer Who Viewed This Item Also Viewed
Non Adhesive Tape
Flare Pipe Sph-C
Flare Pipe Set Sph
Weather resistance drain hose
Flare Tubing Set
Drain branch joint
Water purifier pipe
Foam upward freely pipe