Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of LED head light H4 DC / AC dual use Hi / Lo switching 6-80 V / 6 W / 800 LM

LED head light H4 DC / AC dual use Hi / Lo switching 6-80 V / 6 W / 800 LM
Sales Price: 20.99 SGD
Review Rating: 2.00
5 Customer Reviews
5 star 0
4 star 0
3 star 2
2 star 1
1 star 2
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
I wore it to my son's bike (250 cc)
2
From Japan
On 2017-10-12 14:54:03
It was easy to replace from the H4 valve. There are also LEDs costing 20,000 yen, but buy it for a cheap one, please. Although it is white light indeed, it seems to be different from brightness, and it was hard to see at night from my son, and I returned it to H4.
This review is about item#24966034.
bike
3
From Japan
On 2017-10-05 16:18:24
I use it for Yamaha gear. As it is cheap, the brightness is as described. Occasionally there are problems, but it can not be helped.
This review is about item#24966034.
Adopted in old car Limited to type without external protrusion due to housing interference embedded sp - domain interference
1
From Japan
On 2017-04-22 12:14:25
It will be touched with 6 ~ 80V. It did not light up at 6 V and it was okay at 12 V
This review is about item#24966034.
Honda bay lighting 110 110 head light
1
From Japan
On 2017-01-27 18:21:36
I purchased it because I did not need wiring like HID, but it did not light up.
This review is about item#24966034.
Motorcycle headlight bulb replacement
3
From Japan
On 2016-08-19 13:43:41
For the time being, Ponkin OK! Because of the small amount of light, we should consider the price and think about the fashion level in urban areas. It is a look at it including durability.
This review is about item#24966034.
1