Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of 2WAY carbon heater

2WAY carbon heater
Sales Price: -
Review Rating: 4.83
6 Customer Reviews
5 star 5
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
heating
4
From Japan
On 2018-02-08 15:25:52
When I saw packaging I was worried a bit smaller than I imagined, but warm as it is ... But with this size I got a little high.
This review is about item#66584647.
Used for heating for calves when the temperature is low in winter
5
From Japan
On 2018-01-24 22:51:02
There are switching of 400 W, 200 w, but if there is even 100 W I think it's good.
This review is about item#66584647.
Under the desk to dry the paint
5
From Japan
On 2018-01-22 15:27:48
It is very convenient to use it vertically and horizontally as you are commented on It is wattage which is also gentle for electricity bills because there is a switching of strength of 200 / 400W. Also, because it is lightweight, it is also used for drying of paint.
Making a cake that can not use heating. At your feet! !
5
From Japan
On 2017-12-24 16:50:47
It is compact and useful for vertical and horizontal use. I think that the power consumption is also suppressed and it is good.
This review is about item#66584638.
Countermeasures against cold at customer's feet when visiting
5
From Japan
On 2017-12-21 16:25:06
I was looking for carbon heaters that can be used both in portrait and landscape, so it is very handy.
This review is about item#66584647.
Office
5
From Japan
On 2017-01-07 13:37:17
I am using it under the office desk, but it is very convenient because it can be used both vertically and horizontally.
This review is about item#26335462.
1
Customer Who Viewed This Item Also Viewed