All Category

Brake Parts

The types of brake systems are brake pads, brake shoes, disc rotors, brake rods, brake hoses, master cylinders, calipers, etc. When the brake pads and brake shoes are pressed against the disc rotor and drum brake, friction occurs, braking force is applied, and braking becomes possible. The brake pads and brake shoes will differ depending on how you ride the car, but both will wear due to use. Sudden braking will lead to a decrease in braking force. The brakes are important and require regular inspection.
View : Grid List
Filter

Items 1 - 40 of 3364

Set Ascending Direction
  1. Brake shoes for motorcycles
    NTB Brake shoes for motorcycles
    Uses NAO (non-asbestos organic) developed by new technology. Achieves comfortable braking with less squealing and abnormal noise! Spring included * This product is an important safety part, so be sure to outsource the replacement work to a certified maintenance company. If you replace it by yours... Read More
    Rating:
    86%
    from S$14.99
    Min. 2 days
  2. Brake Pad (Red Pad)
    DAYTONA Brake Pad (Red Pad)
    A best-selling model that pursues long-selling controllability, effectiveness, and disc aggression that has been loved since 1984. It has a wide temperature range and can handle all weather conditions. There is a reason to continue to be loved. * "Red Pad" is a registered trademark of D... Read More
    Rating:
    94%
    from S$39.99
    Min. 2 days
  3. Custom type disc rotor
    SUNSTAR Custom type disc rotor
    Rating:
    100%
    from S$389.90
    Min. 4 days
  4. OES series 2-piston caliper [common name: old crab]
    brembo OES series 2-piston caliper [common name: old crab]
    Based on the model that was genuinely adopted by many motorcycle manufacturers in Europe, while ensuring high-dimensional performance and reliability, Brembo's OES series has excellent cost performance and is stable and popular. Among the many brake caliper manufacturers, the well-balanced pa... Read More
    Color  Black 
    Rating:
    100%
    from S$199.90
    Min. 6 days
  5. Brake master cylinder [VRC] Clamp Standard
    GALESPEED Brake master cylinder [VRC] Clamp Standard
    Forged radial master cylinder equipped with a uniquely developed variable ratio lever. The fulcrum to action point of the lever can be adjusted in increments of 0.25 mm up to 2 mm, and the brake touch, which was influenced by the combination with the caliper, can be brought closer to the best con... Read More
    Diameter (Φmm)  17.5  Type  Standard (clamp) 
    from S$659.90
    Min. 4 days
  6. Radial 4 piston caliper 108mm
    BERINGER Radial 4 piston caliper 108mm
    AEROTEC 4POT RADIAL. For the right. Berlinger is a total brake system manufacturer that features reliable technology cultivated in the manufacture of aircraft brakes and high originality represented by radial masters that use bearings. * This product is an important safety part, so be sure to out... Read More
    Type  For right 
    from S$1,299.00
    Min. 5 days
  7. Caliper support + crab Brembo + front
    G Craft Caliper support + crab Brembo + front
    It is a caliper support that can attach the standard brake custom, Brembo 84mm pitch 2 pod caliper to the front fork of Honda GROM125 / MSX125. The support is machined from high-strength aluminum A2017 material used for aircraft and race machines to make it lightweight. It is useful for improving... Read More
    RoHS directive (corresponding to 10 substances)  Correspondence  Vehicle type  GROM / MSX125 front fork  Specification  Silver anodized 
    from S$95.99
    Min. 4 days
  8. BRAKING WK020L
    DAYTONA BRAKING WK020L
    In the five years since the birth of BRAKING's TOP model "SK", he has won seven world titles. The SK2 series was developed by taking advantage of this experience. BRAKING high-performance disc rotor series developed and designed to "safely and quickly control" the high pow... Read More
    from S$469.90
    Min. 4 days
  9. Brake pads for motorcycles
    NTB Brake pads for motorcycles
    Uses copper-free polishing material. * This product is an important safety part, so be sure to outsource the replacement work to a certified maintenance company. If you replace it by yourself, you will be responsible for it and we will not be able to compensate you. * Even if the model and engine... Read More
    Part No. 
    Rating:
    90%
    from S$17.99
    Min. 2 days
  10. Non-Fade Brake Shoe
    KITACO Non-Fade Brake Shoe
    Stable braking power, high durability, affordable price setting! Lineup centered on mini bikes! If there is little deterioration even at high temperatures, stable braking force is demonstrated by using inning materials. Uses non-asbestos material * This product is an important safety part, so be ... Read More
    Rating:
    86%
    from S$22.99
    Min. 2 days
  11. SBS Brake Pad
    SBS SBS Brake Pad
    The sbs brake pad has a three-layer structure, which is the crystallization of the technical capabilities necessary to achieve stable and best performance even in harsh conditions. If you grasp it, the braking force will be exerted as much as you grasp it. It synchronizes with the feeling of the ... Read More
    Rating:
    87%
    from S$28.99
    Min. 2 days
  12. Golden pad χ
    DAYTONA Golden pad χ
    The golden pad, which has been supported for many years for its straightforward controllability that overturns the common sense of sintered metal pads, has been renewed for the first time in 10 years! The concept remains the same, and the controllability and effectiveness have been further enhanc... Read More
    Rating:
    91%
    from S$57.99
    Min. 2 days
  13. MEGA ALLOY X PAD Sintered
    RK JAPAN MEGA ALLOY X PAD Sintered
    Rating:
    95%
    from S$47.99
    Min. 2 days
  14. Breeder rubber cap
    DAYTONA Breeder rubber cap
    You can easily change the image by adding a one-point color around the caliper while preventing dust from entering the breeder. * This product is an important safety part, so be sure to outsource the replacement work to a certified maintenance company. If you replace it by yourself, you will be r... Read More
    Inner Diameter (Φmm)  About 5  Color  Black 
    Rating:
    80%
    from S$5.59
    Min. 2 days
  15. Hyper Sintered
    DAYTONA Hyper Sintered
    Emphasis is placed on durability and comfort in general driving. The wear resistance, which is also a feature of sintered metal, has been further refined, and the wear resistance has been improved by about 10% compared to the golden pad. There is little wear on the pads and the wheels are not eas... Read More
    Rating:
    92%
    from S$42.99
    Min. 2 days
  16. Professional brake shoe
    DAYTONA Professional brake shoe
    Developed for riders who use the brakes hard, not only for racing but also for street use. Environmentally friendly non-asbestos organic material is used for the shoe material. Compared to other shoe materials (asbestos type, rubber type used by many genuine products, etc.), it demonstrates excel... Read More
    Rating:
    90%
    from S$26.99
    Min. 2 days
  17. Brake shoe with spring
    Vesrah Brake shoe with spring
    Flat lining brake shoes are normal brake shoes made with genuine specifications. The material of the lining is aramid fiber, inorganic fiber, lubricant, and abrasion resistant material, which are mixed and stirred and hardened with phenol resin. If the cam and pin parts of the brake shoe are proc... Read More
    Rating:
    91%
    from S$22.99
    Min. 2 days
  18. Brake pad (hyperpad)
    DAYTONA Brake pad (hyperpad)
    Five "Daytona brake pad series" that can be selected according to performance such as braking force, controllability, durability, application, and vehicle type. * This product is an important safety part, so be sure to outsource the replacement work to a certified maintenance company. I... Read More
    Rating:
    96%
    from S$26.99
    Min. 2 days
  19. Smoke Tank for NISSIN Brake Master
    DAYTONA Smoke Tank for NISSIN Brake Master
    Optional item for DAYTONA / NISSIN tank separate brake master. Light smoke specification reservoir tank assembly (without hose). Large size. * This product is an important safety part, so be sure to outsource the replacement work to a certified maintenance company. If you replace it by yourself, ... Read More
    Specification  For brake (large size) 
    Rating:
    99%
    from S$33.99
    Min. 2 days
  20. M / C repair kit 1/2 inch Master Yaw
    DAYTONA M / C repair kit 1/2 inch Master Yaw
    Repair parts for NISSIN horizontal brake master cylinder. Piston x 1, primary & secondary cup x 1, boots x 1, spring x 1, circlip x 1. NISSIN Horizontal Brake Master Cylinder Repair Parts * This product is an important safety part, so be sure to outsource the replacement work to a certified m... Read More
    Rating:
    83%
    from S$28.99
    Min. 2 days
  21. Non-fade disc pad
    KITACO Non-fade disc pad
    For the street. * This product is an important safety part, so be sure to outsource the replacement work to a certified maintenance company. If you replace it by yourself, you will be responsible for it and we will not be able to compensate you. * Motorcycle maintenance qualification is no longer... Read More
    Material  Non-asbestos material 
    Rating:
    94%
    from S$25.99
    Min. 2 days
  22. FINE ALLOY 55 PAD Semi-Metal
    RK JAPAN FINE ALLOY 55 PAD Semi-Metal
    FINE ALLOY 55 Outstanding ease of control. Thank you for the long-distance group. Semi-metal pad with 55% copper flakes. Demonstrates stable braking force, fade resistance, and wet stability from low to medium speeds to high speeds. It is recommended for people who drive a lot in the city because... Read More
    Rating:
    92%
    from S$31.99
    Min. 2 days
  23. M / C repair kit 11MM Master Yaw
    DAYTONA M / C repair kit 11MM Master Yaw
    Repair parts for NISSIN horizontal brake master cylinder. Repair kit for piston size 11 mm. * This product is an important safety part, so be sure to outsource the replacement work to a certified maintenance company. If you replace it by yourself, you will be responsible for it and we will not be... Read More
    Type  Standard / short common  Size  11mm only 
    Rating:
    95%
    from S$31.99
    Min. 2 days
  24. Brake pad (resin pad)
    Vesrah Brake pad (resin pad)
    The etymology of Besura is an acronym for Best Stop Lining, which means the brake that exerts the best braking force. Besura is a Japanese product and has been patronized by users in Japan, the United States, Europe, and around the world. Assortment by manufacturer from domestic cars to foreign c... Read More
    Rating:
    93%
    from S$47.99
    Min. 2 days
  25. Disc Plate
    No Brand Disc Plate
    Since it is heat-treated, it has excellent durability and heat resistance. It is recommended to replace it with the brake pads at the same time. * This product is an important safety part, so be sure to outsource the replacement work to a certified maintenance company. If you replace it by yourse... Read More
    Rating:
    90%
    from S$34.99
    Min. 2 days
  26. Brake switch for NISSIN brake master
    DAYTONA Brake switch for NISSIN brake master
    Repair parts for NISSIN horizontal brake master cylinder. Switch assembly It can also be used for retro brake master cylinders. * This product is an important safety part, so be sure to outsource the replacement work to a certified maintenance company. If you replace it by yourself, you will be r... Read More
    Rating:
    91%
    from S$15.99
    Min. 2 days
  27. ACPL/GOODRIDGE BANJO BOLT P1.25S
    ACTIVE ACPL/GOODRIDGE BANJO BOLT P1.25S
    Bolt used to fix the banjo adapter. You can choose from a wide variety of colors. * This product is an important safety part, so be sure to outsource the replacement work to a certified maintenance company. If you replace it by yourself, you will be responsible for it and we will not be able to c... Read More
    Included Accessories  2 crash washers 
    Rating:
    76%
    from S$7.99
    Min. 2 days
  28. Air leader (SUS)
    DAYTONA Air leader (SUS)
    You can easily change the image by adding a one-point color around the caliper while preventing dust from entering the breeder. * This product is an important safety part, so be sure to outsource the replacement work to a certified maintenance company. If you replace it by yourself, you will be r... Read More
    Overall Length (mm)  26  Material  Stainless steel 
    Rating:
    84%
    from S$22.99
    Min. 2 days
  29. Brake Shoe (Non Asbestos)
    KITACO Brake Shoe (Non Asbestos)
    The special lining with good grip that does not deteriorate even at high temperatures enhances the cooling effect by the pattern "groove", makes it difficult for dust to collect, and keeps the braking effect. * This product is an important safety part, so be sure to outsource the replac... Read More
    Rating:
    99%
    from S$28.99
    Min. 2 days
  30. Ceramic sintered
    ZCOO Ceramic sintered
    A pad developed and set so that the more you hold it, the more effective it is, so that you can squeeze the cotton rather than the braking that works hard. Furthermore, in order to decelerate smoothly as desired, we pursued "comfortable deceleration" that slows down more than the rider ... Read More
    Rating:
    93%
    from S$79.99
    Min. 2 days
  31. Smoke Tank for NISSIN Clutch Master
    DAYTONA Smoke Tank for NISSIN Clutch Master
    Optional item for DAYTONA / NISSIN tank separate clutch master. Light smoke specification reservoir tank assembly (without hose). * This product is an important safety part, so be sure to outsource the replacement work to a certified maintenance company. If you replace it by yourself, you will be... Read More
    Specification  For clutch 
    Rating:
    99%
    from S$31.99
    Min. 2 days
  32. Brake pads (sintered metal)
    Vesrah Brake pads (sintered metal)
    The etymology of Besura is an acronym for Best Stop Lining, which means the brake that exerts the best braking force. Besura is a Japanese product and has been patronized by users in Japan, the United States, Europe, and around the world. Assortment by manufacturer from domestic cars to foreign c... Read More
    Rating:
    92%
    from S$42.99
    Min. 5 days
  33. Front master C
    DAYTONA Front master C
    A classic horizontal tank separate brake master. The wide lineup that can be selected according to the master cylinder piston diameter and color of the normal vehicle expands the range of customs! The clamp holder has a mirror hole (M10 x P1.25 positive screw included). For handle outer diameter ... Read More
    Rating:
    100%
    from S$159.90
    Min. 2 days
  34. M / C Repair Kit 5/8 "M / C Yaw
    DAYTONA M / C Repair Kit 5/8 "M / C Yaw
    Repair parts for NISSIN horizontal brake master cylinder. 5/8 inch only * This product is an important safety part, so be sure to outsource the replacement work to a certified maintenance company. If you replace it by yourself, you will be responsible for it and we will not be able to compensate ... Read More
    Rating:
    100%
    from S$28.99
    Min. 2 days
  35. Rubber brake hose
    ALCANhands Rubber brake hose
    Brake hose of the same quality as the genuine product. The pressure during braking is accurately transmitted to the caliber to achieve smooth braking operation. In pursuit of safety, the joint from the hose to the fitting is double caulked to improve sealing performance. It also comes with a copp... Read More
    Color  Black  Set Contents  Hose x 1, aluminum gasket x 4 
    Rating:
    66%
    from S$66.99
    Min. 2 days
  36. EARLS / GOODLIDGE Olive
    ACTIVE EARLS / GOODLIDGE Olive
    Rating:
    100%
    from S$3.99
    Min. 2 days
  37. Stainless 10mm Banjo & Packing
    PMC Stainless 10mm Banjo & Packing
    An orthodox banjo bolt that has no decoration like the genuine type. The material is stainless steel, which has high strength and does not rust. Delivered as a set of 2 banjo bolts and 4 special packings. * This product is an important safety part, so be sure to outsource the replacement work to ... Read More
    Size  Total length 32 Under head 26 PC1.25 
    Rating:
    90%
    from S$23.99
    Min. 2 days
  38. M / C repair kit 14MM master CYL
    DAYTONA M / C repair kit 14MM master CYL
    Repair parts for NISSIN horizontal brake master cylinder. Piston x 1, primary & secondary cup x 1, boots x 1, spring x 1, circlip x 1. NISSIN Horizontal Brake Master Cylinder Repair Parts * This product is an important safety part, so be sure to outsource the replacement work to a certified m... Read More
    Rating:
    97%
    from S$28.99
    Min. 2 days
  39. Z1 / Z2 rear brake switch
    PMC Z1 / Z2 rear brake switch
    Original reprint. Early model-style compact body specifications. If the brake lights do not work properly, it is very dangerous because it may lead to a serious accident. Especially if you have been using it for a long time, it is a part that you should replace once. * This product is an importan... Read More
    Lead Wire  2 (black / green) 
    Rating:
    90%
    from S$19.99
    Min. 2 days
  40. Breeder Rubber Cap 4 pieces Red
    DAYTONA Breeder Rubber Cap 4 pieces Red
    You can easily change the image by adding a one-point color around the caliper while preventing dust from entering the breeder. * This product is an important safety part, so be sure to outsource the replacement work to a certified maintenance company. If you replace it by yourself, you will be r... Read More
    Color  Red  Inner Diameter (Φmm) 
    Rating:
    70%
    from S$5.89
    Min. 2 days
View : Grid List
Filter

Items 1 - 40 of 3364

Set Ascending Direction