Rainwater Tanks
Other Related Pages
- SANEI Rain water intake setIt is attached to the vertical part of the house and sends rainwater to the rainwater tank. It can be attached to the main detached house. It is attached by cutting the vertical part of the house. When the tank is full, the overflowing rainwater is discharged to the house. With 3 wire bands and d... Read More
- AS ONE Tank B SeriesSuitable for wafer cleaning and etching. * Piping, drain, heater, and thermometer will be installed according to the specifications.from S$65.99Min. 2 days
- Kodama Plastics Rain water tank cock* Personal delivery is not possibleSuitable for RWT-110
- C.I. TAKIRON Takiron rainwater storage tank AmaneYou can store rainwater from the top. The attached water collecting joint has a perforated plate that makes it difficult for fallen leaves to enter, making it difficult for initial rainwater to enter. In addition, it corresponds to each manufacturer's strategy. Watering the garden water at ho... Read MoreColor Beige Material / Finish Polyethylene (PE)
- SANEI Rain water tankSpace-saving ground installation type. * Please prepare a stand separately. * Not for drinking water. It cannot be used for hand washing or washing toilet seats. * Check the load-bearing strength of the house and the condition of the installation location before installing. * If freezing is expec... Read Morefrom S$289.90Min. 4 days
- GAONA Gaona rainwater tank rainwater storage (fashionable water saving 140L water storage)It is a tank that can collect and store rainwater from rain gutters. You can save water by using the stored rainwater for gardening and watering home gardening. It can also be used as emergency water in the event of a disaster. The compact design allows it to be installed in tight spaces. An adap... Read Morefrom S$599.90Min. 7 days
- DAILITE Open cylindrical tank N type 300LThe tank body is made of polyethylene and has excellent chemical resistance except for some solvents. Inorganic chemical storage tankTrusco Part No. 135-1108 Capacity (L) 300 Outer Diameter (mm) 745 Height (mm) 792 Mass (kg) 8 Material Polyethylene (PE) Specification Tank top open typefrom S$559.90Min. 6 days
- SANEI Rainwater tank with dedicated standSpace-saving ground-mounted type with a dedicated stand * It is not drinking water. It cannot be used for hand washing or washing toilet seats. * Check the load-bearing strength of the house and the condition of the installation location before installing. * If freezing is expected, drain the wat... Read Morefrom S$959.90Min. 4 days
- KAKUDAI MFG Rainwater hoseWith 2 bandsLength (m) 1 Hose Inner Diameter (Φmm) 32 Material PVC
- Bestco Folding Water tank Wide mouseA water tank that can be used according to your lifestyle, from disaster prevention to outdoor activities, leisure, and sports.Capacity (L) 16 Mass (g) 400 RoHS directive (corresponding to 10 substances) Correspondencefrom S$14.99Min. 8 days
- Anzen Kougyou For rainwater tank Faucet* Personal delivery is not possible.from S$22.99Min. 5 days
- Bestco Folding Water tankA water tank that can be used according to your lifestyle, from disaster prevention to outdoor activities, leisure, and sports.RoHS directive (corresponding to 10 substances) Correspondencefrom S$9.69Min. 8 days
- AS ONE Tank / B Series LidSuitable for wafer cleaning and etching.Material PTFE (fluororesin)from S$239.90Min. 4 days
- Sanko San BulkContents with a maximum specific gravity of 1.9 or less can be filled, and stacking after filling is also possible in two stages. It is a UN certified product. Excellent safety (food solution / medicinal solution) The capacity of 5 drums can be covered by the space of 4 drums. Compatible with che... Read MoreCapacity (L) 1050 Outer Dimensions (Opening W x Depth D x Height H) (mm) 1200×1000×1166 Water inlet diameter (mm) 144.5 Trusco Part No. 459-4053 Mass (kg) 80from S$2,899.00Min. 8 days
- SANEI Rain water intakeIt is attached to the vertical of a house to send rainwater to a rainwater tank. Can be attached to major detached houses. Cut and attach the vertical part of the house. Rain from the vertical will collect in the tank through this product, and when the tank is full, the overflowing rainwater will... Read MoreDiscontinued
- Bestco Accordion water tankA water tank that can be used according to your lifestyle, from disaster prevention to outdoor activities, leisure, and sports.Capacity (L) 10 Mass (g) 200Discontinued
- Suiko Joint (40A)Used to attach a valve to the drain. Member for conversion to standard screw 40A. * Personal delivery is not possibleDiscontinued
- MITSUGIRON Rain water tankYou can increase the capacity by connecting the tanks. When the water is full, it will be drained automatically. Comes with a cock that can drain only the required amount. Collects rainwater and reuses it. For emergency water, watering flowers, etc.Color GreenDiscontinued
- Suiko Joint (25A)Used to attach a valve to the drain. Member for conversion to standard screw 25A. * Personal delivery is not possibleTrusco Part No. 858-5905Discontinued
- Try Company TRY mede tank"Photocatalyst" was processed into non-woven fabric and attached to the inside of the plastic tank. The function of the photocatalyst is to store tap water for 3 years without replacement. As a drinking water storage container in the event of a disaster.Discontinued
- Globen English tank basic set 227LIt can be easily attached to existing rain. It will save you money on water bills. You can easily connect additional tanks. For disasters such as taking in rainwater from rain and using it as storage, for sprinkling water (cooling effect by sprinkling water in summer), for watering (for watering ... Read MoreHeight (mm) 960 Trusco Part No. 809-2637 Width (mm) 600 Length (mm) 600 Material High density polyethylene resinDiscontinued
- Globen English tank Linked tank setIt can be easily attached to existing rain. It will save you money on water bills. You can easily connect additional tanks. For disasters such as taking in rainwater from rain and using it as storage, for sprinkling water (cooling effect by sprinkling water in summer), for watering (for watering ... Read MoreLength (mm) 600 Specification With linking kit Height (mm) 960 Set Contents English tank, linking kit Material High density polyethylene resin Width (mm) 600 Trusco Part No. 809-2638Discontinued
- GA (Green Ace) PC cock (with nut)A resin water supply cock that can be easily attached to the tank. * Do not use for flammable liquids and solvents.Heat Resistance Temperature (℃) 60 Material PolyethyleneDiscontinued
- DAILITE Chemical and food tank (N type)Made of polyethylene, with a scale, convenient for weighing. Storage and transportation of chemicals and food. * The lid is sold separately. * We do not deliver to private homes (detached houses / apartments).Operating Temperature Range -20~40℃ Specification Open type Color WhiteDiscontinued