Transportation & Lifting
Logistics supplies are indispensable at sites where products, tools and materials are moved. There are transportation equipment, wagons, workbench, casters, ladders, stepladders, steps, scaffolding, cargo handling, and temporary equipment. It is very convenient to use different tools according to the purpose. There are carts, hand trucks, basket cars, etc. as transportation equipment, and it is necessary to select the tool to use depending on what you carry. There are cargo tightening, towing, chain block, hoist, winch and wire, sling, hoisting equipment and balancer in the cargo handling relationship, which is used for fixing or suspending products, tools and materials.
Other Related Pages
- MonotaRO Load Tightening Belt Metal BuckleTightening and loosening are easy and easy to work with. Luggage is also less likely to be scratched. It is useful in various situations such as outdoors and shopping. Tightening lightweight items. Prevents load collapse indoors and in warehouses. Prevents the opening of trunks and furniture. *Th... Read MoreOperating Load (kg) 100 Belt Width (mm) 25 Breaking Load (kg) 300 Belt-End Finish Endless Material (Belt) Nylon Material (Buckle) Zinc die cast
- MonotaRO Folding Steel TrolleyFoldable for easy storage !! Safe with rubber all around. *Even if it is within the load capacity, please do not use it to climb over a step with a heavy object on it. There is a risk of collapse and damage. *Please do not load items in such a way that the center of gravity is biased or higher th... Read MoreMaterial (Main Unit) Steel Material (Wheel) TPR rubber
- MonotaRO Aluminum LadderMade of aluminum, it is lightweight and can be easily carried by women. Not only for home use such as kitchen and living room, but also for office use. Since it is foldable, it can be stored in a small space even when stored. * Be sure to read the attached instruction manual before use.Storage dimensions / depth (mm) 155 Top plate dimensions / depth (mm) 160 Maximum Working Load (kg) 80 Specification Folding standard type
- MonotaRO Swivel Caster Rubber Wheel Plate TypeIt is a general plate mounting type rubber wheel caster. * Do not apply more than the allowable load. * Do not use with an unbalanced load. * Please note that there may be minor scratches due to the characteristics of the material.Brake None Stopper None Material (Wheel) Rubber Shape Swivel caster
- MonotaRO Eyebolt Stainless SteelThe ring-shaped head is convenient for use through ropes, chains, wires, etc. * Check the working load and use within that range. * Please refrain from reusing products for which the degree of deterioration due to fatigue and aging and the usage history are not clear, as it may disrupt safe work.... Read MoreMaterial Stainless steel (SUS304)
- MonotaRO Folding Workbench AluminumIt is a workbench that can be used in various situations such as car washing and other cleaning. You can choose from 3 sizes depending on the height and length of the top board. Since it is foldable, it can be stored in a small space when stored. * Be sure to read the attached instruction manual ... Read MoreMaximum Working Load (kg) 100 Storage dimensions / height (mm) 140 Top plate dimensions / width (mm) 300 Type Folding standard type
- MonotaRO Caster Swivel Wheel Rubber Plate Type with StopperIt is a general plate mounting type rubber wheel caster. * Do not apply more than the allowable load. * Do not use with an unbalanced load. * Please note that there may be minor scratches due to the characteristics of the material.Brake Included Stopper Rotation stopper Material (Wheel) Rubber Shape Swivel caster S
- MonotaRO EyeboltSince it is treated with trivalent chrome, it is kind to the human body and nature. Also improved corrosion resistance. The ring-shaped head is convenient for use through ropes, chains, wires, etc. * Please check the working load and use within that range. * Please refrain from reusing products f... Read MoreMaterial Carbon steel (SS400) Surface Treatment Trivalent chromium
- MonotaRO Press caster free wheel rubber W with stopperIt is a general rubber wheel caster for medium load. A caster with a double stopper that can stop the rotation of the wheels and at the same time stop the rotation. For casters such as trolleys and workbenches. * Do not apply more than the allowable load. * Do not use with an unbalanced load. * P... Read MoreBrake Compliant Stopper Double stopper (rotation + rotation) Material (Wheel) Rubber Shape Universal car W
- MonotaRO Roller Cabinet Tool Chest with DrawerA steel wagon that is convenient for storing and moving tools and parts. The tray with a convenient drawer that can store tools is covered with an EVA rubber mat to prevent scratches. * Because it is an imported product, there may be some paint peeling or inconspicuous scratches or dents. For sto... Read MoreCaster Diameter (Φmm) 100 Total Load Capacity (kg) 175 Mass (kg) 19 Number of Tiers 3 tiers Load Capacity (kg) 40 / top plate / 15 / drawer / 60 / tray Drawer Internal Dimensions (mm) 645×348×80 Tray Inner Dimensions (mm) 705×350×80 Outer Dimensions, Width W x Depth D x Height H (mm) 736 x 382 x 805 (excluding handle) Material (Cargo) EVA Caster Fixed x 2, swivel x 2 Wall Thickness (mm) Pillar 1.5, drawer head 0.6, other 0.8 Material (Wheel) Rubber Material (Main Unit) Steel Specification Tray position fixed Drawer Yes Stopper Yes (×2)
- MonotaRO Stainless Steel S HookA stainless steel S-can that is resistant to rust. For hanging and hooking * Do not use for any other purpose. * There are some tolerances in the notation dimensions. * Do not apply a load that exceeds the reference working load. * Do not use for life-threatening purposes such as hanging a person... Read MoreType S hook Material SUS304
- MonotaRO Lashing Belt Plastic BuckleSince the buckle is made of resin (POM), it will not rust even when used outdoors. It is easy to tighten and loosen. Luggage is also less likely to be scratched. It is useful in various situations such as outdoors and shopping. Tightening lightweight items. Prevents load collapse indoors, outdoor... Read MoreOperating Load (kg) 10 Belt Width (mm) 25 Breaking Load (kg) 50 Belt-End Finish Adjuster Material (Belt) Nylon Material (Buckle) POM
- MonotaRO Plastic Platform Dolly TPR Swivel Wheels x 4All 4 wheels are equipped with light and flexible casters for easy movement! The compact size makes it easy to use, and it is lightweight because it is made of resin. For transportation *Please do not load more than the load capacity as it may lead to an accident. In addition, please do not load ... Read MoreLoad Capacity (kg) 100 Platform Height (mm) 115 Mass (kg) 2 Wheel Width (mm) 20 Platform Width (mm) 365 Caster 4 wheel freely, silent type Platform Dimensions (Depth) (mm) 495 Wheel Diameter (Φmm) 75 Material (Cargo) Resin Material (Wheel) Thermoplastic rubber (TPR)
- MonotaRO Trolley foldable type compact made of resinIt is very convenient for storage because it becomes flat when folded. Since the flat size is 14.5 cm, it can be stored if there is a gap of 15 cm. The top plate has four non-slip parts for stable transportation while driving. In addition, the top plate has three handles, so it is very convenient... Read MoreLoad Capacity (kg) 100 Platform Height (mm) 125 Wheel Width (mm) 26 Platform Width (mm) 385 Dimensions when Folded, Width W x Depth D x Height H (mm) 385×730×145 Mass (kg) 5.6 Platform Dimensions (Depth) (mm) 595 Wheel Diameter (Φmm) 75 Handle Height (mm) 820 Color Black Material (Cargo) Polypropylene (PP) Material (Handle) Steel
- Tamura Sogyo Sling Belt Z Type (JIS4 Grade, Both Ends Eye Type)Strong belt sling of JIS highest grade (4th grade). It uses strong polyester thread and has excellent features such as tensile strength, durability, abrasion resistance, and low elongation. There is a white core thread inside, making it easy to understand the disposal criteria when the belt is wo... Read MoreType Eye shape on both ends Accuracy Grade JIS Class 4 Material Polyester
- Nissa Chain Oval SleeveIt is a part for end treatment of wire rope.Material Aluminum
- NANSIN Twin Wheel Caster Screw-in typeScrew-in twin wheel castersType Design caster Stopper None Material (Wheel) Nylon Caster Type Screw-in free wheel caster Shape Swivel caster Wheel Type Twin wheels
- MonotaRO Platform Trolley Folding Compact Plastic Lightweight Rubber WheelsBecause it uses silent bearings, it is a quiet dolly that makes less noise when used than a normal dolly. It is very convenient for storage because it becomes flat when folded. Since the flat size is 14.5 cm, it can be stored if there is a gap of 15 cm. The top plate has four non-slip parts for s... Read MoreLoad Capacity (kg) 100 Platform Height (mm) 125 Wheel Width (mm) 26 Platform Width (mm) 385 Dimensions when Folded, Width W x Depth D x Height H (mm) 385×730×145 Mass (kg) 5.6 Platform Dimensions (Depth) (mm) 595 Wheel Diameter (Φmm) 75 Handle Height (mm) 820 Color Black Material (Cargo) Polypropylene (PP) Material (Wheel) Rubber Material (Handle) Steel Noise countermeasures Yes
- MonotaRO Connectable Mini Plastic Platform Dolly TPR Wheels StackableQuiet and comfortable running with light casters. It is very convenient because you can freely connect vertically and horizontally according to your luggage. In addition, stacking (stacking storage) is also possible, so it does not take up much space when storing. Both parallel stacking and cross... Read MorePlatform Height (mm) 100 Mass (kg) 2 Wheel Width (mm) 27 Platform Dimensions (Depth) (mm) 285 Caster 4 wheels freely Platform Width (mm) 420 Wheel Diameter (Φmm) 63 Load Capacity (kg) 80 Material (Top Plate) Resin Feature Stackable Material (Wheel) TPR
- MonotaRO Eye NutSince it is treated with trivalent chrome, it is kind to the human body and nature. Also improved corrosion resistance. The ring-shaped head is convenient for use through ropes, chains, wires, etc. * Check the working load and use within that range. * Please refrain from reusing products for whic... Read MoreMaterial SS400 Surface Treatment Trivalent chromium
- MonotaRO Bogie Foldable Resin Lightweight Running Rubber WheelsLight casters for comfortable running! Foldable for easy storage. Lightweight resin top plate. Casters are already installed, so no assembly work is required. *Please do not load items in such a way that the center of gravity is biased or higher than the load. *The load is displayed as a uniform ... Read MoreWheel Diameter (Φmm) 100 Platform Height (mm) 145 Load Capacity (kg) 150 Wheel Width (mm) 26 Platform Width (mm) 452 Dimensions when Folded, Width W x Depth D x Height H (mm) 452×705×235 Mass (kg) 7.6 Platform Dimensions (Depth) (mm) 705 Handle Height (mm) 825 Material (Main Unit) Board: Plastic / Handle: steel Feature Lightweight Material (Wheel) Natural rubber Caster Silent type
- HAMMER CASTER Screw-in Type 420A Swivel Wheel (Rubber Integrated Wheel)A screw-in type caster that can be swiveled. Steel office equipment, furniture, indoor carriers, etc. * Nuts are not includedType 420A free car Stopper None Caster Type Rotating screw-in caster Type of Sign Screw-in type Wheel Type Single wheel Shape Swivel caster
- HAMMER CASTER 420G Swivel Wheel (Nylon Wheel Urethane Wound Wheel)It is the most produced and used caster. Can be used with fixed 420R / 420GRP with the same mounting height.Type 420G swivel car Stopper None Caster Type Plate type swivel caster Wheel Type Single wheel Shape Swivel caster Finish of Hardware Trivalent chromium conversion treatment
- Geo. Prince Takeshita Stainless steel eye nutMade of stainless steel, it has excellent corrosion resistance and heat resistance. Electrical equipmentRoHS directive (corresponding to 10 substances) Correspondence Finish Electrolytic polishing Material Stainless steel (SUS-304)
- MonotaRO Container Carry Foldable ResinSince it is foldable, it can be folded and stored when not in use, which is very convenient without taking up space for storage. Also, since it is equipped with casters, it is very useful for moving luggage. Carrying luggage * When using, be sure to fix the resin stoppers (2 pieces) fitted on the... Read MoreMaterial (Main Unit) Container: PP / Handle: Aluminum Material Resin Material (Caster) Wheel: PVC, Shaft: Metal
- HAMMER CASTER Screw-in Type 420EA Swivel Wheel (Rubber Integrated Wheel)Screw-in casters, ideal for steel office equipment, furniture, and equipment that requires beauty and lightness, such as indoor carriers. Can be used with 420EA.Type 420EA universal car Finish of Hardware Chrome plating Stopper None Caster Type Rotating screw-in caster Material (Wheel) Rubber integrated wheel with resin bush Wheel Type Single wheel Shape Swivel caster
- TOCHIGIYA Heavy Duty Caster Holder (Caster Stopper)It is a caster holder developed for super heavy casters and heavy casters with little stopper effect. If you insert it from the side of the wheel, the turning part will be fixed at the same time as the wheel. Can be used on all heavy casters. Ideal for super heavy vehicles.RoHS directive (corresponding to 10 substances) Correspondence Material PE Load Rank Super heavy load Surface Treatment Yellow
- MonotaRO Tool Cabinet Rolling Cart 5 Stage Drawer TypeDrawers open and close smoothly on bearing rails. In addition, it can be pulled out to the maximum, so it can be used widely and is convenient. It is a highly practical size that considers the usability of the work site. The tray and top plate are covered with EVA mats to prevent scratches. In ad... Read MoreDrawer load capacity (kg) 1-3 steps: 15, 4 steps: 25, 5 steps: 25 Allowable Load (kg) 100 Caster Diameter (Φmm) 124 Key 2 pieces Maximum Load of Top Plate (kg) 40 Mass (kg) 44 Number of Shelves 5 Main Unit Dimensions, Width W x Depth D x Height H (mm) 768×458×896
- Taiyo Seiki Iron Works Spring hook metal fittingsThe rivets and springs are made of stainless steel. * Please check the working load.
- TRUSCO Lightweight Plastic Platform Trolley Cartio (Folding Handle Type)A lightweight and durable Pro Tool trolley. The running noise is quiet due to the adoption of sound-saving casters. Achieves weight reduction by exposing the rib structure. In addition, the echo from the floor is reduced, allowing you to drive quieter. Elastomer resin wheels reduce tire marks. Tr... Read MorePlatform Height (mm) 162 Caster 2 free casters x 2 fixed casters Handle Height (mm) 900 Surface Treatment Handle: powder coating Feature Lightweight Material (Handle) Steel Material (Wheel / Hardware) Steel Noise countermeasures Yes
- MonotaRO Tool Cabinet Cart 7-Tier Drawer Type 100Φ PP WheelsDrawers open and close smoothly on bearing rails. When you lock it, all 7 steps are locked. It can be used together with the separately sold Monotaro Tool Chest (MonoX1306RD/MonoX1306BK). * When closing the drawer, please close it properly until the end. *As this is an imported product, there may... Read MoreCaster Diameter (Φmm) 100 Allowable Load (kg) 160 Mass (kg) 32 Maximum Load of Top Plate (kg) 40 Main Unit Dimensions, Width W x Depth D x Height H (mm) 620×335×880 Number of Shelves 7
- MonotaRO Cart Foldable Compact Resin Lightweight / Light DutyThe dolly is foldable and compact. Compared to resin, the mass is lighter and easier to handle. The handle can be stored flat when folded, and it is lightweight and easy to carry. Since it is a caster made of polypropylene (PP), it has durability close to that of nylon casters. For transportation... Read MorePlatform Height (mm) 125 Wheel Width (mm) 20 Dimensions when Folded, Width W x Depth D x Height H (mm) 285×730×130 Platform Width (mm) 385 Mass (kg) 4.3 Load Capacity (kg) 50 Platform Dimensions (Depth) (mm) 595 Wheel Diameter (Φmm) 75 Handle Height (mm) 795 Material (Handle) Aluminum Color Blue Material (Wheel) PP Material (Cargo) Polypropylene (PP)
- Nissa Chain RIZE LockLeeds Lock is for temporary fixing and reinforcement of simple equipment at exhibitions. Also for installing signboards and large POPs in stores. An attachment with a built-in self-lock that can be easily tightened by pulling the wire rope without the need for special tools. Installation time can... Read MoreRoHS directive (corresponding to 10 substances) Correspondence
- NANSIN SR Type Screw-in Caster (Elastomer Wheel)Shaft Length L (mm) 14 Material (Wheel) Elastomer Stopper None Caster Type Screw-in free wheel caster Wheel Type Single wheel Shape Swivel caster
- Ishikawa Seisakusho IK series castersMaterial (Wheel / Hardware) Rubber and steel
- MonotaRO Twin Wheel Caster Bolt Type* Do not use for anything other than its intended purpose.Bolt Length (mm) 15 Material (Wheel) 6 nylon Color Black Wheel Type Twin wheels
- Tacoman Tripod HeadPlease prepare 3 logs or pipes. With just one spanner, you can easily complete a tripod. For the leg members, we recommend Φ48.6 single pipe 3m. For the safety of your legs, please use the tripod base (TS-20B, sold separately) for Φ48.6 single pipe. Electrical installation, pipe construction, lan... Read MoreSuitable Pipe Wall Thickness (mm) 1.9 or more
- YUEI CASTER Screw-in ST type free wheel (double bearing) with stopper (rubber wheel)It is a general screw type caster with running performance and load capacity. By making the structure of the swivel part a two-stage structure, smooth swivel is possible. The rotation of the wheel can be locked by the stopper.RoHS directive (corresponding to 10 substances) Correspondence Material (Wheel) Hard rubber Type ST Swivel Caster Type Screw-in type caster Wheel Type Single wheel Shape Swivel caster S Finish of Hardware Trivalent unichrome Stopper With rotation stopper
- H.H.H. Mfg. Pipe TrolleyEasy installation pipe can be used from 35mm to 60mm diameter Resin wheels make running quiet * If the span is long, be careful of bending and breaking of the pipe.Overall Length (mm) 180 Operating Load (kg) 250 Trusco Part No. 375-1058 Mass (g) 700
- KONDOTEC Eye bolt (W thread)It is a convenient product as a hanging piece.RoHS directive (corresponding to 10 substances) Correspondence Material Iron Surface Treatment Unichrome