Sealer Stand Type
A stand sealer is a machine that generates heat at the clip and closes the mouth of bags made of plastic. Also known as a step-on type sealer, it is an item that is often used in factories and processing plants because various bags can be made up from small bags to large bags. Compared to the manual type, it can be sealed with a light foot and can be easily handled even by those with weak power. The heating time varies depending on the material and thickness, such as polyethylene and polypropylene, so it is a good idea to select an appropriate machine according to the application.
Other Related Pages
- SURE (ISHIZAKI ELECTRIC MFG) Stand sealerSince it can be crimped just by stepping on the pedal, you can work safely and carefully with both hands. The cooling timer allows the sealed surface to be crimped cleanly and stably. * We do not deliver to private homes (detached houses / apartments).Temperature of Sealing Part (℃) 250 Seal Width (mm) 5 Power Supply 100V Material Body: Aluminum die-castfrom S$1,499.00Min. 5 days
- FUJI IMPULSE Foot sealerPowerful sealing can be achieved simply by depressing the pedal. Set the heating time with a timer and set the bag on the seal. The heating time of the timer varies depending on the type and thickness of the packaging material. * Water and powder cannot be usedSpecification (Maximum seal thickness) 0.3 mm Power Input (V) 100 Mass (kg) 20 Seal Width (mm) 2・5 Seal dimensions (width W x length L) (mm) 2・5×300 Seal Length (mm) 300 Main Unit Dimensions (Width x Depth x Height) (mm) 390×520×920 Trusco Part No. 462-8462 Power Consumption (W) 470/1050from S$1,499.00Min. 5 days
- FUJI IMPULSE 5mm width heater for FR-450-5, FR-450-5WIt becomes a heat source that generates heat and seals by passing an electric current. Each model has its own heater wire, such as thickness, width, length, and material.Seal Width (mm) 5from S$98.99Min. 2 days
- FUJI IMPULSE Fi seriesSet the heating time with a powerful sealing timer with a light stepping operation, and set the bag on the seal part. After that, just step on the pedal and the seal will be completed. The FiK series can change the angle of the seal part from horizontal to 45 degrees toward the floor. By lowering... Read Morefrom S$1,999.00Min. 23 days
- FUJI IMPULSE Belt sealerIt also has speed. While maintaining the feature of the impulse sealer that it can be sealed immediately without preheating by turning on the power switch, it has the greatest feature of the belt sealer and the speediness that is its strength. On-pal is installed as standard to eliminate waste in... Read MorePart No. SE-SBTA132-20Wfrom S$6,899.00Min. 23 days
- FUJI IMPULSE FA seriesThe most powerful automatic sealer. Press the touch panel of the control unit to set the heating time, etc. After setting the sealing conditions according to the packaging material used, you can select "automatic continuous operation" or "manual operation" by stepping on the a... Read MoreSeal Width (mm) 10from S$3,999.00Min. 23 days
- FUJI IMPULSE FR seriesFoot-operated sealer equipped with a fixed angle table. The attached table can be easily adjusted in height by hooking it on the angle. FEP-N1 (inner two-row printer) and FEP-OS-N1 (outer two-row printer) can be installed as options. * Please note that some models cannot print on the outside.Seal Width (mm) 10 Mass (kg) 27 Seal Length (mm) 450 Dimension (mm) 515×560×1040Hfrom S$2,699.00Min. 23 days
- SURE (ISHIZAKI ELECTRIC MFG) Stand sealer NL seriesYou can crimp by stepping while holding the bag with both hands. Suitable for sealing large bags. Stable sealing work is possible by adopting a cooling timer.As ONE Part Number 1-5285-21from S$1,499.00Min. 20 days
- FUJI IMPULSE FiK seriesSet the heating time with a powerful sealing timer with a light stepping operation, and set the bag on the seal part. After that, just step on the pedal and the seal will be completed. The FiK series can change the angle of the seal part from horizontal to 45 degrees toward the floor. By lowering... Read MoreSeal Width (mm) 10from S$1,999.00Min. 23 days
- Asahi Industry (Insect Trap, Packaging Equipment) Foot sealer + WN-300-10 Seal length x width (300 x 10) For welding onlyYou can make a strong seal just by stepping on the pedal. By lowering the workbench to the bottom, it is ideal for sealing large bags. It has excellent load capacity because it is a workbench with a fixed nut. For packaging metal products, various parts, factories, and packaging at food processin... Read MoreSeal Width (mm) 10 Power Input (V) 100 Trusco Part No. 113-2957 Power Consumption (W) 1350 Mass (kg) 23 Seal Length (mm) 300 Main Unit dimensions, Width (mm) 340 Main Unit Dimensions, Depth (mm) 380 Main Unit Dimensions, Height (mm) 900 Material Aluminum casting / painting Specification Dedicated for welding Set Contents Heater wire: 2, fuse: 2, PTFE tape: 2 Thickness (mm) [Maximum seal] 0.4from S$999.00Min. 5 days
- SURE (ISHIZAKI ELECTRIC MFG) Stand sealerIt can be used for various purposes such as commercial, agricultural, and household bag covers. The heating element can be easily replaced.Type Double-sided impulse / stand sealer Width (mm) 420 Sealing Area (mm) 300×5 Mass (kg) 21 Seal Length (mm) 300 Temperature of Sealing Part (℃) About 300 Table Dimension, Depth (mm) 145 Rating (at 50Hz - at 60Hz) 100V-2000W Power (W) 1440 Voltage (V) 100 Length (mm) 400 Table Dimension, Width (mm) 300 Heating Method Impulse Height (mm) 920 Seal Width (mm) 5 Sealing Time (sec) 0.3~1.5Discontinued
- SURE (ISHIZAKI ELECTRIC MFG) Stand sealerSince it is a double-sided heater, it is ideal for thick gussets and laminated bags. It can be used for various purposes such as commercial, agricultural, and household bag covers. The heating element can be easily replaced.Mass (kg) 18 Height (mm) 920 Type Direct / Laminating Toshier Seal Length (mm) 290 Temperature of Sealing Part (℃) Room temperature to 200 Rating (at 50Hz - at 60Hz) 100V-300W Heating Method Double-sided heat Length (mm) 280 Seal Width (mm) 10 Table Dimension, Width (mm) 300 Table Dimension, Depth (mm) 145 Width (mm) 365 Sealing Area (mm) 290×10 Voltage (V) 100 Power (W) 300Discontinued
- SURE (ISHIZAKI ELECTRIC MFG) Stand sealerIt can be used for various purposes such as commercial, agricultural, and household bag covers. The heating element can be easily replaced.Sealing Time (sec) 0.5~2.2 Rating (at 50Hz - at 60Hz) 100V-470W Length (mm) 350 Type Impulse / stand sealer Power (W) 470 Heating Method Impulse Voltage (V) 100 Width (mm) 380 Table Dimension, Width (mm) 300 Height (mm) 920 Mass (kg) 19 Seal Length (mm) 300 Seal Width (mm) 2.5 Sealing Area (mm) 300×2.5 Table Dimension, Depth (mm) 145 Temperature of Sealing Part (℃) About 260Discontinued
- SURE (ISHIZAKI ELECTRIC MFG) Stand sealerIt can be used for various purposes such as commercial, agricultural, and household bag covers. The heating element can be easily replaced.Type Impulse / stand sealer Seal Length (mm) 450 Length (mm) 350 Heating Method Impulse Sealing Time (sec) 0.5~2.8 Sealing Area (mm) 450×2.5 Mass (kg) 20 Temperature of Sealing Part (℃) About 260 Height (mm) 920 Table Dimension, Depth (mm) 145 Width (mm) 520 Rating (at 50Hz - at 60Hz) 100V-570W Power (W) 570 Table Dimension, Width (mm) 370 Voltage (V) 100 Seal Width (mm) 2.5Discontinued
- SURE (ISHIZAKI ELECTRIC MFG) Stand sealerThe heater can be easily replaced. It is ideal for standing work and sealing of large bags, and can be sealed while holding the bag.Mass (kg) 25 Seal dimensions (width W x length L) (mm) 5×450 Power Input (V) 100 Power Consumption (W) 1380 Specification Maximum seal thickness 0.6mm Trusco Part No. 449-0142 Dimensions, Width W x Depth D x Height H (mm) 520×400×920Discontinued