Shipping Tags / Packing List Slips
A tag / delivery pack is a tag that is used to identify a shipment, a tag label that calls attention, and a delivery pack that is convenient for loading and unloading slips. The tag can be easily wrapped around the package with a wire and can be filled out on paper. The label sticker and tag tape are used for the purpose of calling attention to the handling of luggage with messages and illustrations such as “Handling Precautions” and “Caution”, and for sticking the address name directly on the cardboard and packaging.
Other Related Pages
- SEKISUI Kraft Tape Printed Message Tape for PackageEasy-to-use tape that can be used for packaging and display at the same time. If you use it as a display sticker, you can use about 250 sheets.Color Red base white letters Deployment Force (g/10mm) 40.8 Tensile Strength (N/10mm) 60
- ESCO Label tapeMaterial Kraft paper Sign Meaning Handle with care Inner Diameter (Φmm) 76(3”)from S$9.69Min. 2 days
- MonotaRO Blank Tags with Wire TiesIt is a standard luggage tag with a wire. It's a plain type, so it's convenient because you can write various things. As a luggage sorting and display label *Please do not use it for anything other than its intended purpose. *Be sure to wear gloves when working so as not to injure yoursel... Read MoreMaterial Fine paper, iron Color White RoHS directive (corresponding to 10 substances) Correspondence
- MonotaRO Delivery packA delivery pack with full adhesive. You can attach it directly to the package to enclose a delivery note. There is an opening on one side of the short side, from which you can enclose a delivery note. If necessary, fold the tongue of the opening back to the adhesive surface to make it completely ... Read MoreMaterial Polyethylene, paper Display Items Plain
- PAPYRUS COMPANY Delivery pack (completely sealed, full adhesive on the back)Completely sealed specifications for peace of mind and glue specifications on the entire back surface! There is no need to worry about slips falling after pasting. For sending invoices, invoices, leaflets, etc.RoHS directive (corresponding to 10 substances) Correspondence
- MonotaRO Delivery pack completely sealedA completely sealed delivery pack with full adhesive. You can attach it directly to the package to enclose a delivery note. Since the delivery note can be enclosed from the notch on the back side, it will be completely sealed and the contents will not pop out. The body of the pack is transparent ... Read MoreMaterial Polyethylene, paper Type Completely sealed Display Items Plain
- RINREI TAPE Fragile Tape (Chinese / English / Japanese)The industry's first notation mark in three languages is also listed. Adopted the notation of several languages such as public information on the tape. With a compact design layout, you can use about 250 sheets with a 30m roll, which is very profitable. This is a global tape that supports the... Read MoreSign Meaning Easy goods, FRAGILE HANDLE WITH CARE Base Material Kraft paper Adhesive Synthetic rubber Elongation (%) 9 Tensile strength (N / cm) 65.2 RoHS directive (corresponding to 10 substances) Correspondence
- PAPYRUS COMPANY Delivery packBecause it is a pocket type, documents can be taken in and out even after pasting. Full glue specification on the back! For sending invoices, invoices, leaflets, etc.Size Long 4 envelope Mass (g) 520 Type Back glue RoHS directive (corresponding to 10 substances) Correspondence
- TRUSCO Medium label with wireYou can fill in the plain type.Material Paper, wire Type With wire type Display Items Plain
- TRUSCO Tag with WireYou can fill in the plain type.Material Paper, wire Type With wire type Display Items Plain
- RINREI TAPE Handling craft tapeCraft paper can be easily cut by hand! * The cut line is not included.Sign Meaning Handle with care Base Material Kraft paper Adhesive Synthetic rubber Elongation (%) 9 Tensile Strength (N/10mm) 64.8 RoHS directive (corresponding to 10 substances) Correspondence
- HEIKO Caution stickerIt is a sticker that clearly conveys precautions for home delivery.Material High-quality paper
- Taka Mark (SASAGAWA) Blank White TagsIt is a tag with a wire. You can fill in.
- RINREI TAPE Craft craft tapeCraft paper can be easily cut by hand! * The cut line is not included.Sign Meaning Caution Base Material Kraft paper Adhesive Synthetic rubber Rewinding Force (N/10mm) 0.49 or more Tensile Strength (N/25mm) 147 Tensile Strength (N/10mm) 64.8 RoHS directive (corresponding to 10 substances) Correspondence
- KAKUKEI Color tag with wireJournal display is convenient depending on the color.
- MonotaRO 20 wire color tagsIt is a plain type and you can write various contents. In addition to shipping identification, it is also ideal for wrapping tools. Standard display tag used by attaching the wire part to the product *Please do not use it for anything other than its intended purpose. *Be sure to wear gloves when ... Read MoreMaterial Fine paper: iron Standard beans
- Sfactory Color wire tagIt is a plain type and you can write various contents. In addition to shipping identification, it is also ideal for wrapping tools. It is a standard display tag that is used by attaching the wire part to the product.Material Paper, steel
- MonotaRO Tag seal 2000 piecesA sticker to be attached to a packing box to call attention. There are two types, one on each of the front and back of one sheet. As a packing tag *Please do not use it for anything other than its intended purpose. * Avoid hot and humid places and store in a place away from fire.Specification Seal type Material Paper
- PAPYRUS COMPANY Delivery pack (on delivery note)Due to the two-color printing on the entire surface, the slips and numbers inside cannot be seen through. (You can use the slip as it is!). Completely sealed specifications. With surface perforation that makes it easy to take out slips after arrival. Full glue on the back.Type Back glue Display Items In delivery note RoHS directive (corresponding to 10 substances) Correspondence
- Taka Mark (SASAGAWA) Waterproof Paper TagsMaterial Wash paper (140g / m 2) RoHS directive (corresponding to 10 substances) Correspondence
- Denka Caralyan Tape (Fragile Warning)Because it uses a special base material, it can be easily cut straight without a cutter. It has excellent water resistance and chemical resistance due to the special PE treatment applied to the surface.Adhesive Rubber type
- YUTAKA MAKE TagThe handling method can be displayed in an easy-to-understand manner.Specification Seal type Mass (g) 20 Mass (g/sheet) 1 RoHS directive (corresponding to 10 substances) Correspondence
- Taka Mark (SASAGAWA) Tag B FlowerIt is a tag with a wire. You can fill in.Type One hole RoHS directive (corresponding to 10 substances) Correspondence
- KAKUKEI Waterproof paper tag with wireIt's okay to get wet. For outdoor use such as planting
- Tac Kasei Seto pack adhesiveEasy to use with attention to detail. Since the adhesive is partially attached, it is easy to stick to relatively large objects and uneven surfaces.Type Partial adhesion Display Items Blue line
- Taka Mark (SASAGAWA) Tag B BeanIt is a tag with a wire. You can fill in.Type One hole RoHS directive (corresponding to 10 substances) Correspondence
- PAPYRUS COMPANY Delivery pack (pocket type partial glue)It will be a "partial glue type" with glue on both ends. Since it is a pocket type, slips can be freely taken in and out after pasting.RoHS directive (corresponding to 10 substances) Correspondence
- Tac Kasei Seto pack, plainIt is a general-purpose type that can be used vertically or horizontally, making it ideal for sending documents, small items, precision parts, etc. at the same time. Yellow paper mount, 4 side stickerType Partial adhesion Size Long 3 envelope Display Items Plain
- TRUSCO Tag `` Shojo strictly prohibited '' character typeAttach it to your luggage and use it to call attention.Material Paper Mass (g) 20 Type Seal type
- MORIYA Sangyo Delivery packA transparent bag with glue for attaching slips such as delivery notes and bills to cardboard cases. Since it is a non-separator type without release paper, it does not generate dust. The special shape of the entrance makes it "easy to put in", and also makes it possible to "preven... Read MoreSize Long 3 envelope Type Glued only at both ends Display Items Transparent
- ESCO 50mmx50m Display TapePacking work and caution display can be performed at the same time, and it can also be used as a display sticker. (No cut line)Specification Side reading Sign Meaning Disposal Number of Page 250 Tensile Strength (N/10mm) 60 Core Diameter (Φmm) 76(3")from S$9.69Min. 2 days
- PAPYRUS COMPANY Delivery pack (pocket type)Because it is a pocket type, documents can be taken in and out even after pasting. Full glue specification on the back! For sending invoices, invoices, leaflets, etc.Size Long 3 envelope Type Back glue RoHS directive (corresponding to 10 substances) Correspondence
- PAPYRUS COMPANY Delivery pack (partial glue in delivery note)It will be a "partial glue type" with glue on both ends. Because it is completely sealed, there is no need to worry about slips falling off after pasting.Type Partial adhesion Display Items In delivery note RoHS directive (corresponding to 10 substances) Correspondence
- Tac Kasei Seto pack adhesiveFrom gluing to bag making, the introduction of the new model enables integrated work from the conventional two processes, making it possible to shorten delivery times and reduce costs. It is useful in the distribution industry.Type Partial adhesion Size Chain store unified slipfrom S$29.99Min. 2 days
- PAPYRUS COMPANY Re-peeling delivery packFor long 4 envelope sizes. Since it uses re-peelable glue, it can be peeled off cleanly! For sending invoices, invoices, leaflets, etc. * In rare circumstances (changes in humidity / temperature, adherends, etc.), the adhesive surface may be damaged or glue may remain when peeled off.RoHS directive (corresponding to 10 substances) Correspondencefrom S$39.99Min. 2 days
- YUTAKA MAKE Bean tag with wireYou can fill in the plain type. Luggage displayMaterial Paper, wire Mass (g) 10 Type With wire type RoHS directive (corresponding to 10 substances) Correspondence
- TRUSCO TagAttach it to your luggage and use it to call attention. Attach it to your luggage and use it to call attention.Material Paperfrom S$1.29Min. 2 days
- hapila Address StickerEasy and easy address sticker Easy, easy, household packing suppliesMaterial Paper needle (PH-S309 / W, PH-S309 / B) Sign Meaning For address entryfrom S$1.69Min. 2 days
- SASAGAWA Tag LabelA sticker that conveys the sender's "feelings". The final touch on the luggage box. Your usual luggage will be transformed into a hearty and special delivery. A little care will reach the other party.Material Coat tack paper RoHS directive (corresponding to 10 substances) Correspondence
Filter by categories