Inner PE coating. It is a product that complies with the Food Sanitation Law.
For beverages at the time of visitors and outdoors.
* Do not leave the beverage in it (especially cold beverages) * Please consume alcoholic beverages as soon as possible. * Never use it in a microwave oven or toaster o... Read More
A shopping bag that can be used in various situations such as stores and offices. It is a milky white type that makes it difficult to see the contents. Comes with a convenient hole that can be hung on a hook at the store. There is a perforation between the hook hole and the main body, so if you h... Read More
Material HDPE (high density polyethylene) Color Milky white Type Surface embossing
A shopping bag that can be used in various situations such as stores and offices. It is a semi-transparent type. Comes with a convenient hole that can be hung on a hook at the store. There is a perforation between the hook hole and the main body, so if you hang it on the hook and pull the main bo... Read More
Material HDPE (high density polyethylene) Type Surface embossing Color Translucent
"Saran Wrap (R)" has good adhesion, is firm and firm, and is durable. It is difficult for oxygen to pass through. It is difficult for water to escape. Heat resistant temperature 140 ℃. You can use it in the microwave with plenty of space. Cold resistant temperature is -60 ℃. It keeps it... Read More
Allowable Low Temperature (℃) -60 Heat Resistance Temperature (℃) 140 Material (Blade) Tinplate
Roll paper for cash register. It comes in a plastic bag to prevent paper burns.
For cash register
*Avoid places with high temperature and humidity, or places exposed to direct sunlight. * Please note that the recording part may be discolored if it comes into contact with the following objects. (T... Read More
Paper Thickness (mm) 0.075 Core Diameter (mm) 12 Length (m) 63 Outer Diameter (mm) 80 Material Thermal paper Color White
Since it is less permeable to light, air, and moisture than ordinary plastic wrap film, it is more storable when wrapping food in refrigerators and freezers. In addition, because it has better fire resistance than ordinary plastic wrap, it can be used as a substitute for a drop lid or a plate whe... Read More
It is the most common and cheap split chopstick that is easy to split because it has a groove in the split. Using Vietnamese afforestation material (MO material), it is stronger than aspen material and is easy to crack. In addition, the surface is also characterized by having few stains and strea... Read More
Mass (g) 410 Type Genroku Accuracy Grade Class 1-2 Material Reforestation materials (MO materials) Overall Length (mm) 203
A table duster that you can choose from thin and thick. It dries faster and is easier to use than cotton-based wipes. It is a supple material with good water absorption, so it is easy to squeeze.
For cleaning tables, etc.
* Please wash your hands with a neutral detergent for the kitchen. * Please... Read More
Wooden metal fittings for slit hole-mounted shelf installation system. Please purchase on the left and right.
For horizontal wooden shelves
* The weight of the shelf support varies depending on the mating pillar. Please select the appropriate product from the design stage in consideration of the ... Read More
Thickness (mm) 2.6 Finish Chrome Material Steel special steel
Since it is a pop-up type, it is easy to take out one by one. Uses polyethylene, which is convenient for storing and freezing food.
For food storage and freezing.
* Do not use for anything other than its intended purpose. * Since it is a combustible material, do not place it near a fire or heat s... Read More
Allowable Low Temperature (℃) -20 Thickness (mm) 0.01 Dimensions, Width x Length (mm) 250 (including gusset) x 350 Material Polyethylene Color Translucent Type With gusset
It can be used for a wide range of purposes, from -40 ° C frozen food packaging to high-temperature boil sterilization at 100 ° C for 30 minutes. Since L-LDPE is laminated on a nylon base, it has excellent impact strength, piercing strength, and cold resistance. It has good heat-sealing propertie... Read More
Thickness (mm) 0.075 Applicable Standard Compliant with Food Sanitation Act
A paper cup with a design pattern. Inner PE coating. It is a product that complies with the Food Sanitation Law.
For beverages at the time of visitors and outdoors.
* Do not leave the beverage in it (especially cold beverages) * Please consume alcoholic beverages as soon as possible. * Never use ... Read More
Great for storing samples. A wide variety of sizes from mini size to jumbo size. Food storage containers that are easy to stack. Entec's High Pack is pigment-free and has a colorless finish.
For organizing parts. For kitchen, kitchen, food storage and storage.
* The lid of the high pack may b... Read More
Heat Resistance Temperature (℃) (Body) -20 to 120, (Lid) -30 to 60 RoHS directive (corresponding to 10 substances) Correspondence Material (Lid) EVA resin Material (Main Unit) PP (polypropylene) Shape Square Specification With antibacterial agent Microwave ○ (excluding lid)
Polyvinylidene chloride (PVDC) wraps have excellent barrier properties that prevent the odors of the food filling the refrigerator from mixing in and also delay the oxidation of the food, so the food lasts longer. Since it has a high heat-resistant temperature and is not easily torn, it can be us... Read More
Allowable Low Temperature (℃) -60 Heat Resistance Temperature (℃) 140 Width (cm) 30 Length (m) 50 Material (film) Polyvinylidene chloride (PVDC) Material (Blade) Tinplate Microwave ○
Compared to cotton-based cloth, it dries faster and is a supple material with good water absorption, making it easy to squeeze. Since it is perforated, it can be easily cut to a size that is easy to use.
For cleaning tables, etc.
* Please wash your hands with a neutral detergent for the kitchen. ... Read More
Thickness (mm) 0.3 Mass (g) About 130 Material Cloth: Rayon, Polyester, Core: Paper
It is a sturdy shopping basket.
For shopping at supermarkets.
* Do not put anything heavier than necessary inside.
Nesting Height (mm) 22 Capacity (L) 29 Inner Dimensions (width W x depth D x height H) (mm) 340×220×230 Outer Dimensions, Width W x Depth D x Height H (mm) 465×346×247 Mass (g) 680 Material PP (with antistatic agent)
A hole puncher for spray cans that can be used with both thin and thick cans. The spike part has a rubber cap to prevent the contents from scattering. 【how to use】 1. Release the remaining gas in a place where there is no fire in advance. 2. Hold the can with one hand, open the handle of the ho... Read More
Body Dimensions (L x W x Thickness) (mm) 265×85×20 Applicable Dimensions (mm) Can diameter about Φ30-65
A paper cup that uses unbleached base paper. Useful for both hot and cold. There is a PE coating on the inside.
* Because it is not exposed, black spots and uneven color may appear.
It's easy to cut with the "properly sharp window"! It's hard to rewind! "One shot!" Easy wrapping with Kureha cut! "Neat sharp window" prevents rewinding! The flap that you pinch makes it easier to pinch the edge of the wrap. By embossing the "rewind pre... Read More
Standard 3m size! Two-stage telescopic type! The attachment part of the horizontal bar (kanzashi) rotates according to the wind direction.
For creating stores in the restaurant and sales businesses using the streamers. For service information and menu information.
* The horizontal bar (kanzashi) ... Read More
Horizontal Bar (mm) 850 Overall Length (mm) 1600~3000 Material Pipe (steel + polyethylene coating)
Commercial aluminum foil with many turns. Since the foil cutter uses a paper blade, the entire outer box can be disposed of as burnable garbage. The stoppers on both sides prevent the foil from popping out.
It can be used for various purposes such as shaping the shape of the product with a film, separating it, protecting it from drying, sauce, oil, dust and dirt, and making the product look beautiful. Safe, secure and high quality. Manufactured and cut in a clean room.
* Microwave can be used. (The ... Read More
It catches small debris in the triangular corners and keeps the kitchen clean.
For draining triangular corners.
* Do not use for any purpose other than its intended purpose. * Do not place near fire or in places with high temperatures. * Do not wash away oily or hot items. * Please do not pour cu... Read More
Mass (g) 120 Dimensions, Width x Length (mm) 285×255 Color Blue Type For corner sink strainer Material PE
You can take out the paper cup with one push. Easy to install with the magnet on the back. By using the included screws, it can be installed even in places without magnetism.
For storing and taking out cups and paper cups. For all water supply locations such as offices, factories, and warehouses.... Read More
Dimensions, Width W x Depth D x Height H (mm) 157×145×435 Included Accessories 2 mounting screws Mass (g) 600 Suitable Size 7 oz (for 205 ml) Material ABS + PC + magnet Number of Storage Approximately 50 7-oz paper cups
The triangular corner catches small debris and keeps your kitchen clean. Because non-woven fabric is used, it absorbs oil and is hard to get slimy, suppressing the generation of bad odors.
For draining triangular corners.
* Do not use for any purpose other than its intended purpose. * Do not plac... Read More
Dimensions, Width x Length (mm) 310×265 Mass (g) 82 Type For corner sink strainer Material Non-woven Color White
It stands on its own with a stand pouch. [How to use] 1. Fill the food with a funnel, funnel, etc. from the spout part on the top of the bag. 2. Push the included cap straight into the spout, and then tighten the screws clockwise. [Compatible with boil sterilization] Fill the spout part at the to... Read More
Material Barrier ONy 18 μm / Dry / LLDPE 130 μm Heat Resistance Temperature (℃) Boil up to 80 degrees 30 minutes Mouth Inner Diameter (Φmm) Φ16 (center mounted)