Furnitures for Commercial & Restaurant
Other Related Pages
- OSMAC Paulownia folding convenient deskWhen not in use, the shelves can be stored inside the legs and folded. Since the top plate is made of paulownia wood, it is light and easy to carry. It can also be used as a memorial table in front of the Buddhist altar, a mini table for reading, and a serving table.Color Brown Mass (g) 2500from S$109.90Min. 9 days
- MARNA G plus Easy cushion waffleFrom babies to the elderly, they gently support everyone in a variety of situations. In addition to its unique shape, it is very functional! It has a rounded shape that gives you a sense of security. If you put it on the wheelchair from the front, you can prevent the upper body from shaking. It a... Read MoreMass (g) 755from S$58.99Min. 3 days
- FUKUI CRAFT For Ryugu set ABS top plateRubber sheet processing is applied to the four corners on the back of the top plate to prevent slippage and scratches during stacking.from S$99.90Min. 7 days
- AIMEDIA Sitting Floor CushionThe legs are not numb, and the posture is beautiful with the spine stretched even when sitting upright or cross-legged. Dispersion of body pressure Reduces fatigue and reduces the burden on the lower back. Comfortable to sit on the buttocks without getting tired even if you continue to sit for a ... Read MoreColor light brownfrom S$38.99Min. 2 days
- TKG Cotton cushions NagomiThe batting at the time of setting will be synthetic cotton.
- Suzuya Cotton Cushion IT Yotsuba 202 SetThe batting at the time of setting will be synthetic cotton.Standard Setfrom S$33.99Min. 2 days
- Suzuya Cotton Cushion IT Hanako 132 SetThe batting at the time of setting will be synthetic cotton.Standard Set
- Suzuya Cotton Cushion IT Yamato lattice 184 Cover onlyThe batting at the time of setting will be synthetic cotton.Material 100% cotton Standard Cover onlyfrom S$13.99Min. 7 days
- TKG Cotton cushion Cushioned plainCotton cushion Tsumugi-like plain No. 1-9
- Richell Kurutto Chair IvoryYou can turn it over and use it properly according to your growth and scene. With the attached fixing belt, it can be firmly fixed to the dining chair. You can use it as a chair with a table by attaching a chair table.Suitable age (years) 7 months to about 5 years old
- Suzuya Cotton Cushion HY Rabbit cover onlyType Cover only Material 100% cotton Color Blue
- Suzuya Cotton cushion Cushion HY Kamojima 51004D cover onlyThe batting at the time of setting will be synthetic cotton.Material 100% cotton Standard Cover onlyfrom S$22.99Min. 7 days
- EBM EBM Commercial Cushion Cover Length Hemp FruitIt is a chuck type and can be attached from the top of the cushion.from S$38.99Min. 6 days
- Suzuya Cotton Cushion IT Yotsuba 202 Cover onlyThe batting at the time of setting will be synthetic cotton.Material 100% cotton Standard Cover onlyfrom S$14.99Min. 7 days
- Suzuya Cotton Cushion HY Shosoin 51083 SetThe batting at the time of setting will be synthetic cotton.Standard Setfrom S$43.99Min. 7 days
- EBM EBM Commercial Cushion Cover Length PlainIt is a chuck type and can be attached from the top of the cushion.from S$33.99Min. 4 days
- EBM EBM Commercial Cushion Cover Length White100% cotton Protects the cushions of the store from dirt.from S$29.99Min. 6 days
- Richell Kurutto chair tableIt can be easily attached to a chair. With a 2-step slide adjustment function according to your body shape. A baby chair whose height changes when you turn it back.Material Polypropylene, ABS resin
- Suzuya Cotton Cushion HY Rabbit 51052 SetThe batting at the time of setting will be synthetic cotton.Color Red Standard Setfrom S$39.99Min. 7 days
- Suzuya Cotton Cushion IT Hana Kanako 132 Cover onlyThe batting at the time of setting will be synthetic cotton.Material 100% cotton Standard Cover onlyfrom S$14.99Min. 7 days
- Suzuya Cotton Cushion HY Shokurain 51083 Cover onlyThe batting at the time of setting will be synthetic cotton.Material 100% cotton Standard Cover onlyfrom S$22.99Min. 7 days
- FUKUI CRAFT Kakujin no Zen Zhu Ten BlackIt has excellent durability, is strong against impact, and is hard to break. Good adhesion of paint. Separate type can be stacked! * Washing machine not availableMaterial ABS resin, thermoplastic resin Heat Resistance Temperature (℃) About 60from S$46.99Min. 7 days
- Matsuyoshi & Co Kids chairA brightly colored kids chair. The legs and back are clean white. * Please note the following points for products shipped directly from the furniture manufacturer.・ Measure the dimensions of the installation location and check if the product you ordered can be installed before ordering.・ We can... Read MoreMaterial Leg / steel, upholstery / vinyl leatherfrom S$159.90Min. 13 days
- Oliver Pipe chairUpholstery: Vinyl leather Wood: Beech molded plywood Legs: Φ22.2 Pipe / powder coating. Stacking up to 4 legs.Material Steelfrom S$469.90Min. 7 days
- Suzuya Cotton Cushion IT Yamato Lattice 184 SetThe batting at the time of setting will be synthetic cotton.Standard Setfrom S$33.99Min. 7 days
- EBM Garden sun chairStackableMaterial Polypropylene maker part number 6463500from S$169.90Min. 2 days
- EBM EBM Commercial Cushion Cover Length KannoIt is a chuck type and can be attached from the top of the cushion.from S$35.99Min. 6 days
- EBM Cover length for EBM cushions"Kyo Yuzen", a traditional beauty inherited from ancient times The refined hand-dyed taste is used as the interior of the store.from S$35.99Min. 4 days
- FUKUI CRAFT Sengoku Zen NashijiIt has excellent durability, is strong against impact, and is hard to break. Good adhesion of paint. * Washing machine not availableMaterial ABS resin, thermoplastic resin Heat Resistance Temperature (℃) About 60from S$76.99Min. 7 days
Filter by categories