Inner PE coating. It is a product that complies with the Food Sanitation Law.
For beverages at the time of visitors and outdoors.
* Do not leave the beverage in it (especially cold beverages) * Please consume alcoholic beverages as soon as possible. * Never use it in a microwave oven or toaster o... Read More
"Saran Wrap (R)" has good adhesion, is firm and firm, and is durable. It is difficult for oxygen to pass through. It is difficult for water to escape. Heat resistant temperature 140 ℃. You can use it in the microwave with plenty of space. Cold resistant temperature is -60 ℃. It keeps it... Read More
Allowable Low Temperature (℃) -60 Heat Resistance Temperature (℃) 140 Material (Blade) Tinplate
Since it is less permeable to light, air, and moisture than ordinary plastic wrap film, it is more storable when wrapping food in refrigerators and freezers. In addition, because it has better fire resistance than ordinary plastic wrap, it can be used as a substitute for a drop lid or a plate whe... Read More
It is the most common and cheap split chopstick that is easy to split because it has a groove in the split. Using Vietnamese afforestation material (MO material), it is stronger than aspen material and is easy to crack. In addition, the surface is also characterized by having few stains and strea... Read More
Mass (g) 410 Type Genroku Accuracy Grade Class 1-2 Material Reforestation materials (MO materials) Overall Length (mm) 203
Since it is a pop-up type, it is easy to take out one by one. Uses polyethylene, which is convenient for storing and freezing food.
For food storage and freezing.
* Do not use for anything other than its intended purpose. * Since it is a combustible material, do not place it near a fire or heat s... Read More
Allowable Low Temperature (℃) -20 Thickness (mm) 0.01 Dimensions, Width x Length (mm) 250 (including gusset) x 350 Material Polyethylene Color Translucent Type With gusset
It can be used for a wide range of purposes, from -40 ° C frozen food packaging to high-temperature boil sterilization at 100 ° C for 30 minutes. Since L-LDPE is laminated on a nylon base, it has excellent impact strength, piercing strength, and cold resistance. It has good heat-sealing propertie... Read More
Thickness (mm) 0.075 Applicable Standard Compliant with Food Sanitation Act
A paper cup with a design pattern. Inner PE coating. It is a product that complies with the Food Sanitation Law.
For beverages at the time of visitors and outdoors.
* Do not leave the beverage in it (especially cold beverages) * Please consume alcoholic beverages as soon as possible. * Never use ... Read More
Polyvinylidene chloride (PVDC) wraps have excellent barrier properties that prevent the odors of the food filling the refrigerator from mixing in and also delay the oxidation of the food, so the food lasts longer. Since it has a high heat-resistant temperature and is not easily torn, it can be us... Read More
Allowable Low Temperature (℃) -60 Heat Resistance Temperature (℃) 140 Width (cm) 30 Length (m) 50 Material (film) Polyvinylidene chloride (PVDC) Material (Blade) Tinplate Microwave ○
A paper cup that uses unbleached base paper. Useful for both hot and cold. There is a PE coating on the inside.
* Because it is not exposed, black spots and uneven color may appear.
It's easy to cut with the "properly sharp window"! It's hard to rewind! "One shot!" Easy wrapping with Kureha cut! "Neat sharp window" prevents rewinding! The flap that you pinch makes it easier to pinch the edge of the wrap. By embossing the "rewind pre... Read More
Commercial aluminum foil with many turns. Since the foil cutter uses a paper blade, the entire outer box can be disposed of as burnable garbage. The stoppers on both sides prevent the foil from popping out.
It can be used for various purposes such as shaping the shape of the product with a film, separating it, protecting it from drying, sauce, oil, dust and dirt, and making the product look beautiful. Safe, secure and high quality. Manufactured and cut in a clean room.
* Microwave can be used. (The ... Read More
You can take out the paper cup with one push. Easy to install with the magnet on the back. By using the included screws, it can be installed even in places without magnetism.
For storing and taking out cups and paper cups. For all water supply locations such as offices, factories, and warehouses.... Read More
Dimensions, Width W x Depth D x Height H (mm) 157×145×435 Included Accessories 2 mounting screws Mass (g) 600 Suitable Size 7 oz (for 205 ml) Material ABS + PC + magnet Number of Storage Approximately 50 7-oz paper cups
It stands on its own with a stand pouch. [How to use] 1. Fill the food with a funnel, funnel, etc. from the spout part on the top of the bag. 2. Push the included cap straight into the spout, and then tighten the screws clockwise. [Compatible with boil sterilization] Fill the spout part at the to... Read More
Material Barrier ONy 18 μm / Dry / LLDPE 130 μm Heat Resistance Temperature (℃) Boil up to 80 degrees 30 minutes Mouth Inner Diameter (Φmm) Φ16 (center mounted)
A high quality PET cup with high transparency. Has excellent oil resistance and chemical resistance. It is recommended not only for drinks but also for salads and sweets.
Ideal for taking out miso soup, pork soup, and soup. Heat resistance 80 ℃.
If the delivery destination is a private house (detached house / apartment house), the shop name is required. Please note that delivery may not be possible if there is no store name. * Depending on the delivery location, t... Read More
Freeze in the freezer and thaw in the microwave! Can be tightly sealed with a W zipper. With a convenient memo field! This product complies with the Food Sanitation Law "Standards for Foods, Additives, etc."
Allowable Low Temperature (℃) -30 Thickness (mm) 0.06 Material Polyethylene
A disposable paper napkin for business use. It is a simple design recommended for restaurants such as restaurants, restaurants, cafes, and taverns.
For wiping off dirt such as table and hands when eating and drinking.
* Please refrain from using it for any other purpose. * Please do not reuse aft... Read More
Dimension (mm) 248×248 Number of Folds 6 folds Mass (kg) About 1 Material Pulp Type Six-fold Shape Straight Color White
It can be easily used from restaurants, coffee shops, sushi restaurants, etc. to homes. Reliable quality is backed by excellent features and characteristics. It adheres perfectly to containers made of various materials. It is a film that is easy to stretch and hard to tear. Since it has moderate ... Read More
Fresh and fluffy, just as it is. The cost of cold storage bags has been reduced, and the lineup has been renewed! Recommended for customers who handle products that they want to take home coolly, such as confectionery, bakery, and food products! There are many size variations!
Confectionery Bread... Read More
Protect your sweets with a highly moisture-resistant film. It is possible to maintain freshness by using it in combination with an oxygen scavenger. Be sure to perform a mounting test before using.
A tube type vacuum bag with a V notch that does not require scissors. It can handle from -40 ℃ freezing to 100 ℃ 30 minutes boiling.
* Not compatible with household degassing sealer machines (embossed bags).
Since it uses Japanese paper type non-woven fabric, there is little condensation and it does not wet the product. In addition, the appearance of luxury is also improved.
For maintaining the freshness and quality of fresh foods and processed foods. (Recommended for those who want to avoid water dr... Read More
Ingredient CMC (carboxymethylcellulose) RoHS directive (corresponding to 10 substances) Correspondence
APET product, a highly transparent round cup. It can be used for various purposes.
If the delivery destination is a private house (detached house / apartment house), the shop name is required. Please note that delivery may not be possible if there is no store name. * Depending on the delivery loc... Read More