All Category

Paints

We handle various paints for a wide range of applications such as machinery, iron products, buildings, furniture, and roads. Oil-based paint has a beautiful finish and excellent adhesion. Water-based paint uses water instead of organic solvents, so it is highly safe and recommended for indoor painting. Rust inhibitors, rust converters, and zinc sprays are suitable for preventing material corrosion. Floor coatings can protect concrete and asphalt and draw lines. We also have special paints such as waterproof paints for roofs and rooftops, and varnishes and stains for wood parts.
View : Grid List
Filter

26 Item(s)

Set Ascending Direction
  1. nax formula algo NO.1 metallic color sample book
    NIPPON PAINT nax formula algo NO.1 metallic color sample book
    nax Formula Argo is a color communication tool that allows you to select original colors that suit each product or plan. It is a color card consisting of 98 metallic colors, 84 solid colors, and more sophisticated discerning colors, 7 ultimate colors and 7 base coats, for a total of 196 colors. P... Read More
    Classification of the Hazardous  Non-dangerous goods 
    Rating:
    100%
    from S$76.99
    Min. 2 days
  2. Gloss Adjuster for Water-based Gloss Paints (Mixing Type)
    Kanpe Hapio Gloss Adjuster for Water-based Gloss Paints (Mixing Type)
    ■[Adjust water-based glossy paint to your desired gloss] By mixing a certain amount, you can adjust the water-based glossy paint to your desired gloss. ■[Possible to paint on vinyl cloth by adjusting!] By using this adjusting agent and diluting it by about 25%, you can also paint water-based glos... Read More
    Color  Milky white  Diluent  Please mix it with the paint as it is.  Classification of the Hazardous  Non-dangerous goods  Feature  Glossy 
    from S$12.99
    Min. 2 days
  3. Thinner Autumn/Winter/Spring 1.0kg [For EA942FB, FC]
    AS ONE Thinner Autumn/Winter/Spring 1.0kg [For EA942FB, FC]
    As ONE Part Number  64-7955-08  Classification of the Hazardous  Non-dangerous goods 
    from S$22.99
    Min. 7 days
  4. Thinner Spring/Summer/Autumn 1.0kg [For EA942FB, FC]
    AS ONE Thinner Spring/Summer/Autumn 1.0kg [For EA942FB, FC]
    As ONE Part Number  64-7955-09  Classification of the Hazardous  Non-dangerous goods 
    from S$22.99
    Min. 7 days
  5. Diluent 1.0kg [for EA942FE-1, -3]
    AS ONE Diluent 1.0kg [for EA942FE-1, -3]
    As ONE Part Number  64-7955-13  Classification of the Hazardous  Non-dangerous goods 
    from S$27.99
    Min. 7 days
  6. Water-based Paint Colorant Tone Colorant 7000
    ROCK PAINT Water-based Paint Colorant Tone Colorant 7000
    Colorant for low VOC, low odor water-based paint Since VOC (volatile organic compounds) are not used and there is almost no odor, it can be used for toning low-VOC, low-odor water-based paint without impairing its features. We use carefully selected pigments with excellent weather resistance, so ... Read More
    Type  Water-based paint colorant  Where to Use  Outdoors  Classification of the Hazardous  Non-dangerous goods  Feature  Weather resistance 
    Rating:
    87%
    from S$24.99
    Min. 2 days
  7. Safety Waltz Polyurethane thinner
    OTANI PAINT Safety Waltz Polyurethane thinner
    from S$139.90
    Min. 5 days
  8. Flame-retardant paint thinner
    WASHIN PAINT Flame-retardant paint thinner
    If the viscosity of the oil-based paint is high and difficult to apply, add thinner to adjust the viscosity. It is used to wash the brush used for oil-based paint. It is a non-dangerous material with no flash point. For diluting oil-based paints and cleaning painting tools.
    Classification of the Hazardous  Non-dangerous goods 
    from S$279.90
    Min. 6 days
  9. Waterproof solvent (epoxy thinner)
    DAN Chemical Waterproof solvent (epoxy thinner)
    Classification of the Hazardous  Non-dangerous goods 
    from S$33.99
    Min. 6 days
  10. RAL Color Sample Book
    Hafele Japan RAL Color Sample Book
    It is a color sample book of European RAL standard. color sample
    Classification of the Hazardous  Non-dangerous goods 
    from S$29.99
    Min. 2 days
  11. Thinner Autumn/Winter/Spring 1.0kg [For EA942FA]
    AS ONE Thinner Autumn/Winter/Spring 1.0kg [For EA942FA]
    As ONE Part Number  64-7955-10  Classification of the Hazardous  Non-dangerous goods 
    from S$25.99
    Min. 7 days
  12. Thinner for spring/summer/autumn 1.0kg [for EA942FA]
    AS ONE Thinner for spring/summer/autumn 1.0kg [for EA942FA]
    As ONE Part Number  64-7955-11  Classification of the Hazardous  Non-dangerous goods 
    from S$25.99
    Min. 7 days
  13. Diluent 1.0kg [for EA942FE-101, -102]
    AS ONE Diluent 1.0kg [for EA942FE-101, -102]
    As ONE Part Number  64-7955-12  Classification of the Hazardous  Non-dangerous goods 
    from S$23.99
    Min. 7 days
  14. Water-based & Oil-based Residual Paint Treatment Agent (Harden & Throw Away(
    Atom House Paint Water-based & Oil-based Residual Paint Treatment Agent (Harden & Throw Away(
    It can easily solidify and treat 1-liquid paints such as water-based, oil-based, lacquer, varnish, and stain paints and thinning liquids. Approximately 400 mL of waste paint can be treated with one 35 g bag of this product. Disposal agents for water-based and oil-based paints, lacquers, varnishes... Read More
    Processing Capacity  Up to about 400ML with 35g  Classification of the Hazardous  Non-dangerous goods  RoHS directive (corresponding to 10 substances)  Correspondence 
    from S$3.09
    Min. 2 days
  15. Waste Paint Solidification Agent (Paintmaster)
    NEXTRY Waste Paint Solidification Agent (Paintmaster)
    If it is a water-based paint, it will exhibit a stable effect on any kind of paint regardless of the type of paint or manufacturer. It may be possible to treat difficult-to-harden paint by mixing it with another hard-to-harden paint. [Features] - If the amount of additive required for the reactio... Read More
    Included Accessories  Measuring spoon/Instruction manual  Ingredient  Diatomaceous earth  Color  Light brown  Main Application  plastic  Storage Environment  Store in a dark place with low humidity  Classification of the Hazardous  Non-dangerous goods  Property  Ocher fine powder  Addition amount  5-8% of paint mass 
    Rating:
    60%
    from S$67.99
    Min. 2 days
  16. building deck green thinner
    DNT building deck green thinner
    Low odor. Isoparaffin-based solvent is used, so there is little adverse effect on people and the environment. Long-lasting strong anti-fungal effect and durability. Good workability and finish. brush, roller, spray * Stir well to make a uniform coating before painting. *Be sure to use the specifi... Read More
    Viscosity  23℃ 85~100KU  Diluent  Building deck thinner  Classification of the Hazardous  Designated combustibles  Name of The Hazardous  Flammable liquids  Quantity of the Hazardous  4kg  Gloss  Matte  Feature  Antifungal, durable, thinner  Film thickness  30 μm / time  Heating Residue (%)  70~75 
    from S$99.90
    Min. 8 days
  17. Neo Gosei #300 Thinner
    SHINTO PAINT Neo Gosei #300 Thinner
    * We do not deliver to private homes (detached houses / apartments). * Depending on the delivery location, the delivery date may be postponed and additional shipping charges may be incurred. * Since it will be delivered by a large vehicle of 4 tons or more, we may ask the customer to pick up the ... Read More
    Classification of the Hazardous  Designated combustibles  Name of The Hazardous  Flammable liquids  Quantity of the Hazardous  3.5kg 
    from S$169.90
    Min. 9 days
  18. Color sample book (pocket version) 2019 edition
    Japan Paint Manufacturers Association Color sample book (pocket version) 2019 edition
    "Standard colors for paints" issued by the Japan Paint Manufacturers Association is a color that stores many practical colors such as buildings, structures, equipment, landscape equipment, interior colors, and colors defined by the Japanese Industrial Standards (JIS). It is a must-have ... Read More
    Specification  Standard color for paint  Type  2019 K edition  Classification of the Hazardous  Non-dangerous goods 
    Rating:
    94%
    Discontinued
  19. GOANZEN filler Rough roughening accelerator
    SOMAY-Q GOANZEN filler Rough roughening accelerator
    * Please use the special accelerator at a ratio of up to 5% of the volume of the main agent.
    Classification of the Hazardous  Non-dangerous goods 
    Discontinued
  20. Refrigerant tube rack Hot-dip galvanizing repair agent
    NEGUROSU DENKO Refrigerant tube rack Hot-dip galvanizing repair agent
    ROVAL1 and ROVALSP300 are room temperature galvanized paints with a zinc content of 96%. Demonstrates an excellent rust preventive effect.
    Suitable for  Hot-dip galvanized finish  Main Component  Zinc  Classification of the Hazardous  Non-dangerous goods 
    Discontinued
  21. Color sample book (pocket version)
    Japan Paint Manufacturers Association Color sample book (pocket version)
    * Expiration date is the end of December 2019.
    Specification  Standard color for paint  Content  2017 J version  Classification of the Hazardous  Non-dangerous goods 
    Rating:
    91%
    Discontinued
  22. Repair material for hot dip galvanizing
    NEGUROSU DENKO Repair material for hot dip galvanizing
    A room temperature galvanized paint with a zinc content of 96%. Demonstrates an excellent rust preventive effect. * When using ROVAL SP300, until you hear a rattling sound Shake it up and down enough. * After using ROVAL SP300, if there is any residue, the nozzle may be clogged, so after turning ... Read More
    Suitable for  Hot-dip galvanized finish  Classification of the Hazardous  Non-dangerous goods 
    Discontinued
  23. Aqueous 3kg paper can
    CEMEDINE Aqueous 3kg paper can
    For building interior JIS A 5537 JAIA F ☆☆☆☆ 4VOC standard compliant Water-based solvent-free Interior base wood work Can be used for bonding wooden bricks and styrofoam
    Classification of the Hazardous  Non-dangerous goods 
    Discontinued
  24. Refrigerant tube rack High corrosion resistance plated steel sheet / hot dip galvanizing repair agent
    NEGUROSU DENKO Refrigerant tube rack High corrosion resistance plated steel sheet / hot dip galvanizing repair agent
    A silver-colored repair agent with a metallic luster. It has both a rust preventive effect and a beautiful finish. * When using ROVA SP, shake it up and down sufficiently until it makes a rattling sound. * After using ROVASP, if there is any residue left, the nozzle may be clogged. Therefore, tur... Read More
    Main Component  Zinc  Classification of the Hazardous  Non-dangerous goods 
    Discontinued
  25. Hot-dip galvanizing repair agent
    NEGUROSU DENKO Hot-dip galvanizing repair agent
    ZRC has excellent adhesion and can be used with a single application.
    Suitable for  Hot-dip galvanized finish  Main Component  Zinc  Classification of the Hazardous  Non-dangerous goods 
    Discontinued
  26. Selion Wall
    ABC Trading Selion Wall
    Deodorant plastering material for interior walls * Insufficient kneading may cause color unevenness. * Too much water can cause sagging and poor curing. * Please use the interior filler to adjust the base. * Be sure to apply anti-staining treatment to the base where the stains appear. * If you wi... Read More
    Material  Sericite  Color  White  Coating Thickness  0.5~1.0  Main Application  Interior wall  Application Method  Iron  Drying Time (hours)  24 or more  Where to Use  Indoor  Classification of the Hazardous  Non-dangerous goods  Standard application amount (g / m 2 About 3.3 
    Discontinued
View : Grid List
Filter

26 Item(s)

Set Ascending Direction