All Category

Paint Thinners / Treatment Agents

View : Grid List
Filter

9 Item(s)

Set Ascending Direction
  1. Gloss Adjuster for Water-based Gloss Paints (Mixing Type)
    Kanpe Hapio Gloss Adjuster for Water-based Gloss Paints (Mixing Type)
    ■[Adjust water-based glossy paint to your desired gloss] By mixing a certain amount, you can adjust the water-based glossy paint to your desired gloss. ■[Possible to paint on vinyl cloth by adjusting!] By using this adjusting agent and diluting it by about 25%, you can also paint water-based glos... Read More
    Feature  Glossy  Color  Milky white  Classification of the Hazardous  Non-dangerous goods  Diluent  Please mix it with the paint as it is. 
    from S$12.99
    Min. 2 days
  2. Water-based Paint Colorant Tone Colorant 7000
    ROCK PAINT Water-based Paint Colorant Tone Colorant 7000
    Colorant for low VOC, low odor water-based paint Since VOC (volatile organic compounds) are not used and there is almost no odor, it can be used for toning low-VOC, low-odor water-based paint without impairing its features. We use carefully selected pigments with excellent weather resistance, so ... Read More
    Classification of the Hazardous  Non-dangerous goods  Where to Use  Outdoors  Type  Water-based paint colorant  Feature  Weather resistance 
    Rating:
    87%
    from S$24.99
    Min. 2 days
  3. Safety Waltz Polyurethane thinner
    OTANI PAINT Safety Waltz Polyurethane thinner
    from S$139.90
    Min. 6 days
  4. Flame-retardant paint thinner
    WASHIN PAINT Flame-retardant paint thinner
    If the viscosity of the oil-based paint is high and difficult to apply, add thinner to adjust the viscosity. It is used to wash the brush used for oil-based paint. It is a non-dangerous material with no flash point. For diluting oil-based paints and cleaning painting tools.
    Classification of the Hazardous  Non-dangerous goods 
    from S$279.90
    Min. 7 days
  5. Waterproof solvent (epoxy thinner)
    DAN Chemical Waterproof solvent (epoxy thinner)
    Classification of the Hazardous  Non-dangerous goods 
    from S$33.99
    Min. 5 days
  6. Water-based & Oil-based Residual Paint Treatment Agent (Harden & Throw Away(
    Atom House Paint Water-based & Oil-based Residual Paint Treatment Agent (Harden & Throw Away(
    It can easily solidify and treat 1-liquid paints such as water-based, oil-based, lacquer, varnish, and stain paints and thinning liquids. Approximately 400 mL of waste paint can be treated with one 35 g bag of this product. Disposal agents for water-based and oil-based paints, lacquers, varnishes... Read More
    RoHS directive (corresponding to 10 substances)  Correspondence  Classification of the Hazardous  Non-dangerous goods  Processing Capacity  Up to about 400ML with 35g 
    from S$3.09
    Min. 2 days
  7. Waste Paint Solidification Agent (Paintmaster)
    NEXTRY Waste Paint Solidification Agent (Paintmaster)
    If it is a water-based paint, it will exhibit a stable effect on any kind of paint regardless of the type of paint or manufacturer. It may be possible to treat difficult-to-harden paint by mixing it with another hard-to-harden paint. [Features] - If the amount of additive required for the reactio... Read More
    Addition amount  5-8% of paint mass  Ingredient  Diatomaceous earth  Color  Light brown  Included Accessories  Measuring spoon/Instruction manual  Classification of the Hazardous  Non-dangerous goods  Property  Ocher fine powder  Storage Environment  Store in a dark place with low humidity  Main Application  plastic 
    Rating:
    60%
    from S$67.99
    Min. 2 days
  8. building deck green thinner
    DNT building deck green thinner
    Low odor. Isoparaffin-based solvent is used, so there is little adverse effect on people and the environment. Long-lasting strong anti-fungal effect and durability. Good workability and finish. brush, roller, spray * Stir well to make a uniform coating before painting. *Be sure to use the specifi... Read More
    Viscosity  23℃ 85~100KU  Film thickness  30 μm / time  Quantity of the Hazardous  4kg  Heating Residue (%)  70~75  Feature  Antifungal, durable, thinner  Standard Application Amount (kg/m2 Brush, roller: 0.12, airless: 0.14  Diluent  Building deck thinner  Classification of the Hazardous  Designated combustibles  Name of The Hazardous  Flammable liquids  Gloss  Matte 
    from S$99.90
    Min. 7 days
  9. Neo Gosei #300 Thinner
    SHINTO PAINT Neo Gosei #300 Thinner
    * We do not deliver to private homes (detached houses / apartments). * Depending on the delivery location, the delivery date may be postponed and additional shipping charges may be incurred. * Since it will be delivered by a large vehicle of 4 tons or more, we may ask the customer to pick up the ... Read More
    Quantity of the Hazardous  3.5kg  Classification of the Hazardous  Designated combustibles  Name of The Hazardous  Flammable liquids 
    from S$169.90
    Min. 8 days
View : Grid List
Filter

9 Item(s)

Set Ascending Direction