Welding Safety Equipment
Welding curing tools (sheets, fences, etc.) are welding equipment used to protect the surroundings and eyes from sparks and strong ultraviolet rays generated during welding and fusing. Sheets are available in carbonized fibers or flame-resistant fibers coated with silicon resin or carbon. It is used by pulling down or covering the front when welding. Fences are often used for welding shading, and some use soft vinyl film. It is used to prevent retinal burns caused by ultraviolet rays and visible rays.
Other Related Pages
- MonotaRO Spatter sheetThere is no problem of dust and pollution. Welding spark curing sheet, fireproof sheet, flameproof covers * Do not use for anything other than its intended purpose.Instantaneous Operating Temperature (℃) 1300 Continuous Use Temperature (℃) 250 Thickness (mm) About 1.0 Eyelet Inner Diameter (mm) Φ12
- MonotaRO Spatter Sheet LightSingle-sided silicon coating processed product. It is light and has excellent workability. It conforms to JIS A 1323. Spark curing sheet at the time of welding / fusing, spark curing tsuitate, fire prevention curtain * Not suitable for fishing work.Thickness (mm) 0.7 Instantaneous Operating Temperature (℃) 1300 Continuous Use Temperature (℃) 200 Eyelet Spacing (mm) About 450 Eyelet Inner Diameter (mm) Φ12
- Osaka Spirit Carbon SheetA product that is much lighter than conventional spatter sheets and can be easily carried to the site. In addition, there is no need to process eyelets on the product, it can be easily cut to any size on site with scissors, and it can be said that there is no fraying from the cut part. * When wel... Read MoreThickness (mm) 2 Mass (g/m2) 400 Color Black Specification Felt processing
- TRUSCO Spatter Sheet Basic Double SidesJapan Fire Retardant Association Flameproof Performance Test Conformity Test No. CO050010 Double-sided silicone coating of flame-resistant fiber High performance and price does not include harmful fibers such as economy type asbestos and glass fiber that irritates the skin. Type that repels spark... Read MoreWeight (g/m2) 720 Thickness (mm) About 1 JIS Standard JIS A 1323A class passed No. 03A0188 Specification Processing type: Double-sided silicon Eyelet Inner Diameter (mm) Φ12
- YUTAKA MAKE Spark protection sheetPlease use it vertically as a curtain or fence. It is light and has excellent workability. Has excellent spark blocking properties during welding and fusing. Good heat resistance. (Heat-resistant temperature 300 ℃, softening point 800 ℃) Light and strong, good workability. * Cannot be used for st... Read MoreThickness (mm) About 0.3 Specification Class A passing product RoHS directive (corresponding to 10 substances) Correspondence JIS Standard JIS standard A1321 passed product
- MIGHT INDUSTRY TIG torch cover (cloth chuck type) 8mWidth (cm) 11 RoHS directive (corresponding to 10 substances) Correspondence
- MonotaRO Welded shading fenceIt blocks strong ultraviolet rays and visible light, which are said to be harmful to the human body during welding work, and protects the safety of the eyes. * Do not use for anything other than its intended purpose.Sheet Thickness (mm) 0.35 Frame Inner Dimensions, Width W x Height H (mm) 2000×2000 Mass (kg) 8.3 Material (Frame) Steel (resin coating)
- TRUSCO Sputter Sheet DXStandard type. Has excellent flame resistance and heat resistance. Repels the sparks received. It does not contain harmful fibers such as asbestos or glass fibers that are irritating to the skin. Welded spark receiving sheet / fireproof curtain. Curing sheet / duct cover.Thickness (mm) 1 Specification Class A passing product JIS Standard JIS A 1323A class passed No. 32171 Eyelet Inner Diameter (mm) Φ12
- TRUSCO Spatter FeltSpatter felt fabrics are lighter and cheaper than traditional textiles. Since there is no texture, it is difficult for slag to enter and it is easy to remove the attached slag. The cut surface does not fray. For slag receiving work. (Sprinkling water is even more effective) * Cannot be used to pr... Read MoreSpecification Class A passing product Material / Finish 100% flame resistant fiber
- Onaka Industry Spatter Sheet 1230WDouble-sided silicon processing on carbon fiber cedar weave. The twill weave is strong against pulling, and the fabric does not fray even if you cut it freely. There is no skin irritation found in harmful fibers such as asbestos and glass fibers.Thickness (mm) 1.23 Instantaneous Operating Temperature (℃) 1300 Continuous Use Temperature (℃) 250~300 Eyelet Spacing (mm) 450 Material Carbon fiber cedar twill weave Specification Class A passing product Standard Passed JIS A 1323A class test
- YOSHINO Spatter sheet Premium PlatinumIt is a premium sputter sheet that exceeds class A and has withstood the manufacturer's test (steel plate thickness more than twice, oxygen pressure more than 3 times) under stricter conditions than class A. It has excellent tensile strength and is thick yet supple and easy to handle. (Non-as... Read MoreThickness (mm) About 1.2 JIS Standard JIS A 1323 Class A Passed No. 09A0154
- MonotaRO Replacement Film for Welding Light Shielding FenceReplacement film for light-shielding fences. It blocks strong ultraviolet rays and visible light, which are said to be harmful to the human body during welding work, and protects the safety of the eyes. Partitions and curtains at welding work sites and factories * Cannot be used as a light-shield... Read MoreThickness (mm) 0.35 Number of Eyelets 16 Dimensions (Width W x Height H) (mm) 1970×1970 Mass (kg) 2.15 Eyelet Spacing (mm) About 480 Material Soft vinyl film Eyelet Inner Diameter (mm) Φ12
- TRUSCO Sputter sheet AlphaAffordable, affordable, plain weave economy type. Repels the sparks received. It does not contain harmful fibers of asbestos or glass fibers that are irritating to the skin. It does not burn even when exposed to flames in the air, and does not melt or shrink. Welding spark receiving sheet / fire ... Read MoreThickness (mm) 0.7 Specification Class C passing product Color Sheet: Gray (silicon is white) / Black Eyelet Inner Diameter (mm) Φ12
- TRUSCO Spark curing sheetLightweight and excellent in workability. Since it is orange and stands out, it is ideal for spark curing and flameproof curing. A type that repels sparks. It is a non-asbestos safe product.Width (mm) 920 Thickness (mm) 0.21
- Osaka Spirit Carbon sheet single side silicone coatingIt is a product that has the characteristics of SG-250 and has a higher drop-out strength than SG-250. Welding of refractory sheets for construction ・ Flame-retardant test for welding sparks JIS A 1323 Class A passed product. The silicone-based resin-coated surface has good spark repelling (perf... Read MoreMass (g/m2) 590 Thickness (mm) 2 Color Black x single sided silicon Type Single-sided silicon coating
- Asahi Sangyo (Tarp) Sputtered sheet silica clothIt is a flexible material that can withstand temperatures above 1000 ° C. Withstands rapid heating and cooling. There is little smoke. Has excellent dimensional stability. Attach the received sparks. JIS A 1323 Class A passed For the front curtain / cover for slow coolingThickness (mm) 0.64 Specification Class A passing product RoHS directive (corresponding to 10 substances) Correspondence JIS Standard JIS A 1323 Class A Eyelet Inner Diameter (mm) Φ12
- WELDTEC Cable CoverRoHS directive (corresponding to 10 substances) Correspondencefrom S$109.90Min. 2 days
- MonotaRO Spark screenProtects safety during welding work. Uses a flameproof certified sheet with excellent flame retardancy. The sheet is a fabric in which glass fiber is coated on both sides with special silicon. JIS A 1323 Class B accepted product * Do not use for anything other than its intended purpose.Thickness (mm) 0.38 Frame Inner Dimensions, Width W x Height H (mm) 2000×2000 Mass (kg) 9.4 Type Class B passing product Specification With casters
- ESCO Heat-resistant work sheet [850x850mm]Continuous Use Temperature (℃) 1000 Instantaneous heat-resistant temperature (℃) 1650 Melting Point (℃) 1760 Mass (g) 600 Dimension (mm) 850×850 Esco Part No. EA334B
- Asahi Sangyo (Tarp) Incombustible heat insulating matSilica cloth is used for the outer material and a ceramic blanket is used for the inner material. Since the silica cloth used as the outer material is an inorganic fiber, the fiber itself will not catch fire. Because it is a textile product, flexible work and portability are possible. You can wor... Read MoreContinuous use 1000℃ Instant Heat Resistance 1650℃
- TRUSCO Incombustible heat insulating matSputter sheet Gold Alpha (passed JIS A1323A class) is used for the outer material and ceramic blanket is used for the inner material, which can also be used as a heat insulating material in high temperature range. Since the silica fiber (high heat resistant glass fiber), which is the material of ... Read MoreContinuous use 1000℃ Thickness (mm) 15 Instant Heat Resistance 1650℃from S$99.90Min. 2 days
- TRUSCO Welding light shielding fence sheetA replacement sheet for welded light-shielding fences. Japan Fire Retardant Association Flameproof Performance Test Number Acquired AT860027Material / Finish Flameproof soft vinyl chloride film Remark Sheet only
- Asahi Sangyo (Tarp) Sputtered sheet ProudIt lasts longer than conventional spatter sheets. No through holes harmful to fire protection were found in the sheet even when the 19 mm steel plate was gas-cut (* This test is not official and is not guaranteed). The oxygen index of the sheet is 60 or more. Durability is improved at (21 in norm... Read MoreThickness (mm) 1.2 RoHS directive (corresponding to 10 substances) Correspondence JIS Standard JIS A 1323 Class A passed
- TRUSCO Sputter sheet supermarketA lightweight spatter sheet with glass fiber coated on both sides with special silicon. The "playing" and "non-adhesiveness" of sparks have been improved. A type that repels sparks and slag. It is a non-asbestos safe product. Weld fusing spark receiving sheet, welding spark bl... Read MoreThickness (mm) 0.38 JIS Standard JIS A 1323 B class passed No. 05A3881
- Osaka Seisakusho Carbon felt PC400Carbon felt PC400 is a felt-like sheet made of 100% carbon fiber. Lightweight and excellent in workability. Since it is felt-shaped, it can be cut freely and does not fray. It is hard to tear because it has stronger tensile strength than conventional felt. Welding spark receiver simple protective... Read MoreThickness (mm) 2 Color Black Material Carbonized fiber Specification Folding around: None JIS Standard JIS A 1323 Class A Eyelet Nonefrom S$58.99Min. 5 days
- TRUSCO Transparent sheet for screens Flameproof typeA replacement sheet for welded light-shielding fences. The transparent type does not have light-shielding performance. The clear sheet makes it easy to check the work status. It has both flame resistance and autolysis. For safety measures in dustproof work. As a partition between the aisle and th... Read More2018 Trusco page 7 0386 Color Transparent flameproof Material Flameproof soft vinyl chloride filmfrom S$119.90Min. 2 days
- TRUSCO Spatter sheet platinumA type that attaches the received sparks. As the spatter sheet fabric, we have adopted a satin weave that has never been seen before, so the weave is smaller and the tensile strength is higher than the conventional plain weave and cedar twill weave. Unlike silica and glass fibers, it is light, re... Read MoreThickness (mm) 1.3 Eyelet Inner Diameter (mm) Φ12from S$109.90Min. 2 days
- AS ONE Heat Resistant SheetIt has an instantaneous heat resistance temperature of 1300 ° C or higher, a minimum oxygen index of 55 to 62, and excellent non-combustible characteristics. Even if it comes into direct contact with the flame, it only glows red and does not fuse or stick. For preventing sparks from scattering du... Read MoreInstantaneous heat-resistant temperature (℃) 1300 Standard Passed JIS A 1323A class test Material Pyromex R
- TRUSCO Heat shield sheet Super PlatinumHas excellent heat reflectivity and heat resistance. A composite product made by laminating a film (pet) with aluminum vapor deposition layers on both sides of a 6-micron polyester film and a flame-resistant fiber woven fabric, Akiko woven fabric (high-density product). Base cloth (platinum) JIS ... Read MoreHeat Resistance Temperature (℃) 200from S$159.90Min. 2 days
- TRUSCO Spatter Sheet Gold AlphaGold type popular product. Attach the received sparks. There is little spark scattering. Ideal for slag receiving work. (Sprinkling water is even more effective.)Thickness (mm) 0.81 Specification Class A passing product Eyelet Inner Diameter (mm) Φ12
- TRUSCO Single-sided carbon felt ADSingle-sided special flame-retardant resin coating on conventional spatter sheet carbon felt. Durability has been further improved. The special flame-retardant resin coated surface repels sparks well, and the non-coated surface on the back surface absorbs water to improve safety. No sewing on she... Read MoreThickness (mm) 1.65 Specification Class A passing product Eyelet Inner Diameter (mm) Φ12from S$66.99Min. 2 days
- TRUSCO Welding light shielding fence sheetA replacement sheet for welded light-shielding fences.Sheet Thickness (mm) 0.35 Material Flameproof soft vinyl chloride filmfrom S$129.90Min. 2 days
- MIGHT INDUSTRY TIG torch coverWidth (mm) 140 RoHS directive (corresponding to 10 substances) Correspondencefrom S$56.99Min. 2 days
- Osaka Seisakusho Protech sheet SG20Protech Sheet SG20 is a sheet made of glass fabric coated with special silicone on both sides. Has excellent heat resistance and weather resistance. Has excellent dimensional stability. It does not generate toxic gas and does not emit dust. Factory hot air curtains / partitions, radiant heat / sh... Read MoreThickness (mm) 0.35 Continuous Use Temperature (℃) 250 RoHS directive (corresponding to 10 substances) Correspondence Material Glass double-sided silicon Color Gray / silver JIS Standard JIS A 1323 Class Cfrom S$119.90Min. 2 days
- STAR ELECTRIC MANUFACTURING (SUZUKID) Spatter sheetIt is a fire receiving sheet for welding. Flame resistant fiber is processed into felt. Welding fire receiving sheetDimension (mm) 1000×1000 Thickness (mm) About 2.8 JIS Standard JIS A 1323A class passed
- Osaka Seisakusho Carbon cloth # 3000NCarbon cloth # 3000N is a domestically produced sheet made of 100% carbon fiber plain weave and impregnated with a flameproofing agent. Since the carbon fiber is impregnated with a flameproofing agent, it has excellent fire resistance and heat resistance. Because it is thick, it can be used as a ... Read MoreThickness (mm) 2.3 Color Black JIS Standard JIS A 1323 Class Afrom S$139.90Min. 6 days
- TRUSCO Spatter sheet deluxe (double-sided coating)Japan Fire Retardant Association Flameproof Performance Test Conformity Test No. C2120018. The flame-resistant fiber raw cloth is coated on both sides with special silicone. It is a type that repels the received sparks and slag. It does not contain harmful fibers such as asbestos or glass fibers ... Read MoreNumber of Eyelets None Thickness (mm) About 1 JIS Standard JIS A 1323 Class A Passed 08A3823 Mass (kg) 0.3 Dimensions, Length L x Width W (mm) 610×610 Trusco Part No. 786-8871from S$63.99Min. 2 days
- TRUSCO Spatter sheet deluxe (double-sided coating)Japan Fire Retardant Association Flameproof Performance Test Conformity Test No. C2120018. Since the eyelet metal fittings are not attached, it will not cause damage to the work. As a welding spark receiving sheet, fire prevention curtain, curing sheet, duct cover.Thickness (mm) About 1 JIS Standard JIS A 1323 Class A Passed 08A3823 Number of Eyelets Nonefrom S$85.99Min. 2 days
Filter by categories