Wire & Cable Support Hardware
A support bracket is a bracket that is attached to support piping or wiring. By attaching support brackets, pipes and wiring installed inside and outside the building can be fixed, and even if vibrations such as running water vibrations or earthquakes occur, they can be prevented from moving and stay in place. In the category of electric circuit support material / support metal fittings, various support metal fittings and related parts such as bolts are handled, and the shape and type can be selected, so they can be used according to the place of use and purpose of use.
Other Related Pages
- MIRAI INDUSTRY Cable Trolley (Type 200 for I Type Steel)A simple type that can be easily installed and easily expanded or relocated! *Delivery to private residences is not possible. *Delivery may be refused in some areas. *We cannot deliver products directly from the manufacturer to individual homes. *Please note that this includes cases where the bui... Read MoreSuitable for For I-shaped Beam 125/150 mm Type 200 type
- MIRAI INDUSTRY Bolt hanging bracket for Super E deck*We cannot deliver products directly from the manufacturer to individual homes. *Please note that this includes cases where the building name cannot be distinguished from the exterior of the building.Applicable bolt diameter W3/8 Acceptable static load (N [kgf]) 294(30)from S$18.99Min. 2 days
- Akagi Deck hanging bracket (for synthetic slab structure)For synthetic slab structures * Be sure to use the metal fittings that match the deck manufacturer. Be sure to tighten the hanging bolts. The tightening torque for the hanging bolt (W3 / 8) is 7.8 to 9.8 Nm (80 to 100 kgf / cm). After mounting, do not use it to deform the hardware such as bending... Read More
- ELEPHANT CHAIN BLOCK I beam yo hangerMade of reinforced plastic and has excellent durability.Type I-beam hangerfrom S$76.99Min. 2 days
- NEGUROSU DENKO Neglock (spring clip)Installation is completed simply by sandwiching it with pliers. A spring clip that does not require screw tightening.Surface Treatment Dacrotized paint
- NEGUROSU DENKO Eyebolt* In consideration of the environment, the plating process will be changed from hexavalent chrome plating to trivalent chrome plating. (The color changes from a color close to gold to a color close to silver) Please note that it may be mixed depending on the product because it will be switched se... Read Morefrom S$4.69Min. 16 days
- NEGUROSU DENKO Steel Pipe Support Bracket "Pylac"A metal fitting that supports a conduit by using a clip together with general shaped steel. The conduit can be supported at any angle at the back and bottom. The tip of the screw is dented so that it can bite into the construction material widely and large. It is hard to loosen against vibration ... Read More
- NEGUROSU DENKO Solid Wall Wire Duct (without Hole)Some pipe support brackets such as ductor clips have knurls in the grooves to improve the catching of the claws. Some have a center line as a guide when drilling a ductor. A hanger used to support electrical conduits, round cables, cable racks, ducts, etc. * Delivery may not be possible if the de... Read More
- NEGUROSU DENKO Pylac Clip (Conduit Support Clip)A clip that supports conduits to various shaped steel materials in combination with Pilak. For outdoor use, hot dip galvanized finish and stainless steel are also available. * 3 1C28C and above cannot be used for PH1S. (Can be used for 15C, 19C, 25C22C, 16C) * The surface treatment of electrogalv... Read More
- NEGUROSU DENKO Suspension Bolt Support Clamp for General Shape Structural SteelScrews with a Kubomi structure are used so that they can be reliably supported against tension. Economy type pyrac type hanging bracket. It is a metal fitting that supports various equipment by lowering hanging bolts from shaped steel. * Do not use stainless steel products in an environment conta... Read More
- MIRAI INDUSTRY PF pipe piece saddleUsed for fixing when PF pipes are exposed pipes. Can be firmly fixed with a single screw. *We cannot deliver products directly from the manufacturer to individual homes. *Please note that this includes cases where the building name cannot be distinguished from the exterior of the building.
- NEGUROSU DENKO Duct ClipThe edge of the clip is cut up to prevent the cable coating from being damaged. It is a metal fitting that supports the pipe to the ductor channel. * Allowable static load value varies depending on the mounting direction. * The surface treatment of electrogalvanized products will be changed from ... Read More
- Akagi Screwed T BrakectMetal fittings for connecting hanging bolts * Use A pin, screw, etc. for fixing.Material Electrogalvanized finish Size W3/8
- NEGUROSU DENKO WORLD DUCTOR (Terminal Protection Cap)Material Soft vinyl chloride
- NEGUROSU DENKO World Ductor (Dactor channel perforated type)Since the ductor channel has long holes and round holes, you can save the trouble of drilling and save labor. * Do not use stainless steel products in an environment containing chlorine ions, such as an indoor pool. There is a risk of "stress corrosion cracking" where the material crack... Read More
- NEGUROSU DENKO FV RackA metal fitting that supports a VVF cable on general shaped steel. To install it, just push it in with the handle of a screwdriver. You can easily unfold the clip on the cable support with the tip of a flat-blade screwdriver.Surface Treatment Dacrotized paint
- NEGUROSU DENKO World Ductor (for ceilings and walls)* Do not use stainless steel products in an environment containing chlorine ions, such as an indoor pool. There is a risk of "stress corrosion cracking" where the material cracks locally.
- MIRAI INDUSTRY Crocodile piece saddle (combined type)The saddle diameter can be adjusted, and it can be fixed to any type such as CD pipe, PF pipe, VE pipe, steel pipe, and cable. *We cannot deliver products directly from the manufacturer to individual homes. *Please note that this includes cases where the building name cannot be distinguished from... Read More
- MIRAI INDUSTRY PF pipe saddle*Please use the manufacturer's pole band (stainless steel) for the stainless steel band. *We cannot deliver products directly from the manufacturer to individual homes. *Please note that this includes cases where the building name cannot be distinguished from the exterior of the building.
- NEGUROSU DENKO WORLD DUCTOR (Ductor Middle Nut)Easy to install and remove from the ductor channel (D15, D20, D1 type) opening. In combination with D15, it is ideal for adjusting the position of fixtures in high-quality apartments, etc., where the double-ceilinged foot roller tends to be held low. * Bolts with hot-dip galvanized finish may not... Read More
- MIRAI INDUSTRY Cable Trolley (Type 0 for Messenger Wire)A simple type that can be easily installed and easily expanded or relocated. For power tools / power trucks, trolley power / electric hoists, and overhead crane power supplies. *Delivery to private residences is not possible. *Delivery may be refused in some areas. *We cannot deliver products dir... Read MoreType Type 0
- NEGUROSU DENKO World Ductor (for channel support)* Do not use stainless steel products in an environment containing chlorine ions, such as an indoor pool. There is a risk of "stress corrosion cracking" where the material cracks locally. * The surface treatment of electrogalvanized products will be changed from colored chromate (hexava... Read More
- Toshiba Lighting & Technology Prevention outlet plug (for lighting rail)* Please use at 1500W or less. It may cause overheating and burning.Rated Voltage (V) 125 Rated Current (A) 15
- MIRAI INDUSTRY Saddle with PF / VE standThe protrusion on the inside of the saddle gets stuck in the valley of the pipe and can be fixed securely, so the pipe does not shift. * Please use the manufacturer's pole band (stainless steel) for the stainless steel band. *We cannot deliver products directly from the manufacturer to indivi... Read More
- NEGUROSU DENKO Level Adjustment SpacerSince it has a U-shape, it can be inserted from the side even after installing the mount / equipment on the anchor bolt. The height can be adjusted by stacking them. * In consideration of the environment, the plating process will be changed from hexavalent chrome plating to trivalent chrome plati... Read More
- BAKUMA INDUSTRIAL Hanging BracketSince it uses bolts with a dented tip structure, it can be reliably supported against pulling. General shaped steel / lip groove shaped steel * Do not use in a vibrating place.Material SPHC (chromate plating) Suitable Bolt (Whitworth Thread) W3/8
- NEGUROSU DENKO Ductor Clip (S-DC)The edge of the clip is cut up to prevent the cable coating from being damaged. It is a metal fitting that supports the pipe to the ductor channel. * Do not use stainless steel products in an environment containing chlorine ions, such as an indoor pool. There is a risk of "stress corrosion c... Read More
- NEGUROSU DENKO World Ductor (level adjustment spacer)Since it has a U-shape, it can be inserted from the side even after installing the mount / equipment on the anchor bolt. The height can be adjusted by stacking them.Suitable for Anchor bolt Φ16mm or less Material Stainless steel (SUS)
- MIRAI INDUSTRY SV single saddle (for SV cable, TL flexible cable, conduit, coaxial cable)*We cannot deliver products directly from the manufacturer to individual homes. *Please note that this includes cases where the building name cannot be distinguished from the exterior of the building.
- NEGUROSU DENKO Support Bracket (for General Shape Steel)The mounting surface is flat, and wooden boards, boards, ductor channels, etc. can be mounted stably. * Do not use in a vibrating place. There is a risk of loosening or falling. * Please hang the hanging bolt vertically. There is a risk of slipping and falling. * The surface treatment of electrog... Read MoreSurface Treatment Electrogalvanized
- Kameda Denki Auxiliary Metal Fittings LK HKIt is a convenient metal fitting for ducts, wiring, mounting small parts, etc. Since the holes are continuous grooves, it can be positioned freely. By adding bending, it can be used in places where installation is difficult.RoHS directive (corresponding to 10 substances) Correspondence
- INABA DENKO Bolt hangerUses screws with a dented tip structure that can reliably support tension. Used when attaching bolts (W3 / 8) to H-steel. * Avoid using in a vibrating place.Surface Treatment UNIQLO (indoor use only) Applicable hanging bolt W3/8
- SOTOYAMA ELECTRIC Half SaddleMaterial Steel plate Surface Treatment Electrogalvanized
- NEGUROSU DENKO Special nut* □ -DH8N may not be attached to hot-dip galvanized bolts depending on the adhesion of the plating, so use stainless steel bolts. * The surface treatment of electrogalvanized products will be changed from colored chromate (hexavalent) to trivalent chromate. The color of the exterior changes from ... Read More
- NEGUROSU DENKO Suspension bracket (for H-shaped and I-shaped steel)Bolts with a recessed structure are used to ensure reliable support against pulling. It can be supported even if the channel opening is facing up. (However, the applicable flange thickness is 7 to 24 mm.) * Due to environmental friendliness, the plating process will be changed from hexavalent chr... Read More
- NEGUROSU DENKO Hanging bolt support bracketA screw with a dented tip structure is used so that it can be reliably supported against pulling. It can be set on the lower bracket with the nut attached to the hanging bolt. * The surface treatment of electrogalvanized products will be changed from colored chromate (hexavalent) to trivalent chr... Read More
Filter by categories