Bearing Units
A bearing unit is a component consisting of a bearing housing and a bearing box with bolt holes for mounting the bearing. Necessary when installing the bearing mechanism. It is used in various mechanical devices equipped with a bearing mechanism, and is used in many general machines including conveyors and rotating rollers. There are various types of bearing units, such as pillow type, square flange type, and diamond flange type, so select the appropriate type according to the unit installation space.
Other Related Pages
- FYH (NIPPON PILLOW BLOCK) UCF Square flange type (without cylindrical hole / cover)The photo is a photo without a cover. The cover is not attached to the type with a cover mounting groove. A bearing unit that combines a ball bearing for the unit and a bearing box with a square flange. Suitable for mounting on a vertical surface such as the side of a machine. The bearing box is ... Read MoreRoHS directive (corresponding to 10 substances) Correspondence Shape Square flange typefrom S$19.99Min. 4 days
- Yokota Kikou Rolling bearing adapter H30 seriesRoHS directive (corresponding to 10 substances) Correspondence Type adapterfrom S$119.90Min. 6 days
- ASAHI SEIKO Hanger type plastic seriesDimension l (mm) 21 RoHS directive (corresponding to 10 substances) Correspondence Dimension N (mm) M16×2from S$139.90Min. 5 days
- FYH (NIPPON PILLOW BLOCK) Pillow unit UCP typeThis is the most typical type of rolling bearing unit. Since ribs are provided at the base of the bearing box mounting part, it has a high-strength structure against loads in all directions. The bearing box is attached to the machine body with two bolts. Transmission equipment, general machinery,... Read MoreRoHS directive (corresponding to 10 substances) Correspondence Shaft Hole Type Cylindrical hole (with set screw) Shape Pillow unit Grease Nipple With grease nipple Cover Without cover
- NTN Pillow Type Unit Lubrication TypeThis is a typical type of bearing unit, and is equivalent to a combination of a widely used plummer block, an automatically widely used plummer block, and a self-aligning ball bearing. It can be easily tightened by simply tightening it, and is most often used in transmission devices and general m... Read MoreShaft Hole Type Cylindrical hole type (with set screw) Shape Pillow unit
- NTN Pillow Type Lubrication-Free TypeThis is a typical type of bearing unit, and is equivalent to the combination of a plummer block and a self-aligning bearing, which have been widely used in the past. And most often used in general machinery. * Since the bearing boxes of UCP201 to 203 are common, P203 is used for all.Shaft Hole Type Cylindrical hole type (with set screw) Shape Pillow unit
- ASAHI SEIKO Pillow UnitReasonable self-aligning The bearing and the bearing box are completely sealed, so that only the bearing can be replaced due to the complete compatibility between the dust-proof bearing and the bearing box. Uses to maintain a beautiful luster for a long time with good adhesion of the coating filmRoHS directive (corresponding to 10 substances) Correspondence Shape Pillow unit
- FYH (NIPPON PILLOW BLOCK) Adapter for bearing H300X / H2300XIt can be used for pillow blocks whose manufacturer part number starts with UK (type that stops the shaft with an adapter). Washers, sleeves and lock nuts can be replaced individually. Fix the shaftType adapter
- FYH (NIPPON PILLOW BLOCK) UFL Compact / Lightweight Rhombic Flange TypeA diamond flange type unit that combines a lightweight unit ball bearing and a special light alloy bearing box. An oil-free, compact, lightweight, clean bearing unit that incorporates bearings with a diameter series of 0. Bearing boxes do not rust for long periods of time, making them ideal for u... Read MoreRoHS directive (corresponding to 10 substances) Correspondence Shaft Hole Type Cylindrical hole type (with set screw) Shape Diamond shape flange type Material High carbon chromium bearing steel
- NTN Square Flanged Units Cast Housing Set Screw TypeThe shape of the bearing box is square and it is attached to the side wall of the machine with four bolts. Due to the simple structure around the bearing and easy installation, it is the most widely used flange type.Shape Square flange unit
- ASAHI SEIKO Square flange unitSince the shape of the bearing box is square and it is mounted on the side wall of the machine, the structure of the bearing mounting part is simplified and it has a wide range of applications.RoHS directive (corresponding to 10 substances) Correspondence Shaft Hole Type Cylindrical hole with set screw Grease Nipple Included Load Rank Included Cover None Shape Square flange unit
- NTN Diamond flange type oil-free typeThe shape of the bearing box is rhombus, and it can be mounted on the frame with two bolts, and it can be mounted side by side in a narrow space, so it is suitable for places where the mounting pitch of the bearing unit is limited, such as a conveyor. .. Also, the mounting bolt hole pitch is the ... Read MoreShape Diamond flange unit
- ASAHI SEIKO Ball bearing for unit (for light load)A spherical outer diameter surface is used for alignment, and the wide inner ring is fixed to the shaft with two hexagon socket head bolts on each side. It is completely sealed by double seals on both sides.Shape Ball bearing for unit RoHS directive (corresponding to 10 substances) Correspondence Shaft Hole Type Cylindrical hole with set screw Type For light loads Suitable Model (Main Unit) UC
- FYH (NIPPON PILLOW BLOCK) Square flange unitA bearing unit that combines a ball bearing for the unit and a bearing box with a square flange. Suitable for mounting on a vertical surface such as the side of a machine. The bearing box is attached to the machine body with four bolts.RoHS directive (corresponding to 10 substances) Correspondence Shaft Hole Type Cylindrical hole (with set screw) Cover None Shape Square flange unit
- FYH (NIPPON PILLOW BLOCK) Sealed flange type flange unitA bearing unit that combines a ball bearing for the unit, a round flange, and a bearing box with a wax on the mounting surface. To attach the bearing box to the machine body, insert the brazing part into the mounting hole of the machine body and use four bolts. The bearing box can be mounted in t... Read MoreRoHS directive (corresponding to 10 substances) Correspondence Shaft Hole Type Cylindrical hole (with set screw) Cover None Shape Sealed flange type flange unit
- NTN Diamond flange unit oil supply typeThe shape of the bearing box is rhombus, and it can be mounted on the frame with two bolts, and it can be mounted side by side in a narrow space, so it is suitable for places where the mounting pitch of the bearing unit is limited, such as a conveyor. .. Also, the mounting bolt hole pitch is the ... Read MoreShape Diamond flange unit
- ASAHI SEIKO Rhombic Flange Type UnitSince the bearing box is shaped like a rhombus and attached with two bolts, it does not take up much space and can be easily attached to a machine.RoHS directive (corresponding to 10 substances) Correspondence Shape Diamond flange unit
- Shimizu Seiko Flange Bearing UnitSurface Treatment (Flange) Black oxide Material (Flange) SPCC
- KMT Lightweight bearing unit Set screw type pillow type unitLubricant Lithium grease
- FYH (NIPPON PILLOW BLOCK) UP Compact and lightweight pillow typeA pillow type unit that combines a lightweight unit ball bearing and a special light alloy bearing box. An oil-free, compact, lightweight, clean bearing unit that incorporates bearings with a diameter series of 0. Bearing boxes do not rust for long periods of time, making them ideal for use in cl... Read MoreRoHS directive (corresponding to 10 substances) Correspondence Shaft Hole Type Cylindrical hole (with set screw) Material High carbon chromium bearing steel Shape Pillow type
- KMT Lightweight bearing unit Set screw type diamond flange type unitLubricant Lithium grease
- NTN Steel plate pillow unitThe bearing box is made of steel plate by precision pressing, and it is lightweight and compact, but it has great rigidity, so it is suitable for packing equipment with limited mounting space and weight, small blowers, printing machines, agricultural machines, etc. .. * Allowable load is applied ... Read MoreShape Pillow unit
- FYH (NIPPON PILLOW BLOCK) Pillow unit UKP type* Adapter is sold separately. (* A separate adapter is required to use with the indicated shaft diameter.)Other Adapter sold separately RoHS directive (corresponding to 10 substances) Correspondence Shape Pillow unit Shaft Hole Type Tapered hole type
- NTN Mini Pillow UnitA lightweight and compact bearing unit that combines an oil-impregnated bearing with many features due to its unique manufacturing technology and a steel plate housing. The housing is made of steel plate that is locally reinforced by press working, making it highly rigid, lightweight and compact.... Read MoreType Pillow unit Shape Pillow unit
- NTN Lightweight cast iron diamond flange unitShape Diamond flange unit Cover Without cover
- ASAHI SEIKO Silver Series Rhombic Flange UnitCompared to conventional ball bearing units, it is smaller and lighter, and the mechanical equipment is made more compact. Since the bearing box has a center mark, positioning is easy.RoHS directive (corresponding to 10 substances) Correspondence Shaft Hole Type Cylindrical bore with eccentric ring Shape Diamond flange unit Material (Rubber Seal) Nitrile rubber (NBR) Grease Nipple None
- FYH (NIPPON PILLOW BLOCK) Diamond flange unitA bearing unit that combines a ball bearing for the unit and a bearing box with a diamond-shaped flange. Suitable for mounting on a vertical surface such as the side of a machine. Compared to the square flange type unit, the mounting space is smaller and the unit mass is also smaller. The pitches... Read MoreRoHS directive (corresponding to 10 substances) Correspondence Shaft Hole Type Cylindrical hole (with set screw) Shape Diamond flange unit Cover None
- FYH (NIPPON PILLOW BLOCK) Lightweight diamond flange unitA diamond flange type unit designed for weight reduction. The bearing box is attached to the machine body with two bolts.RoHS directive (corresponding to 10 substances) Correspondence Shaft Hole Type Cylindrical hole (with set screw) Shape Diamond flange unit Cover None
- NTN Square flange unit without oil supplyThe shape of the bearing box is square and it is attached to the side wall of the machine with four bolts. Due to the simple structure around the bearing and easy installation, it is the most widely used flange type. * Since the bearing boxes of UCF201 to 204 are common, F204 is used for all.Shape Square flange unit
- NTN 4-Bolts Round Flange Unit Lubrication TypeA cylindrical marking wax is provided on the mounting surface of the bearing box, and it is fitted into the frame. There is little eccentricity during mounting, positioning is accurate, and it is suitable for drum pulleys.Shape Sealed flange type flange unit
- Yokota Kikou Rolling bearing adapter H23 seriesAn adapter that combines an adapter sleeve, lock nut, and washer. It is used to easily fix a bearing with a tapered hole to any position on the shaft. Washers and washers can be replaced with the applicable part numbers listed.
- FYH (NIPPON PILLOW BLOCK) Ball Bearing for SB Unit (Cylindrical Hole)A series of bearings that are lighter than UC type bearings. An oil-free grease-sealed deep groove ball bearing with a spherical outer diameter outer ring and a wide inner ring with a set screw for a cylindrical hole. It is fixed to the shaft with two set screws attached to the inner ring. Lightw... Read MoreRoHS directive (corresponding to 10 substances) Correspondence Shaft Hole Type Cylindrical hole with set screw Load Rank For light loads Shape SB Type Standard goods
- NTN Ball bearing for unitShank Diameter (Φmm) - Shape Cylindrical hole type Load Rank For light loads Suitable Model (Main Unit) UC
- ASAHI SEIKO Take-up unit cast iron with set screw● Grease nipple: With grease nipple ● Load type: For light load ● Cover: Without cover ● Shaft hole type: Cylindrical hole typeRoHS directive (corresponding to 10 substances) Correspondence Shape Take-up unit
- NTN Mini Flange UnitA lightweight and compact bearing unit that combines an oil-impregnated bearing with many features due to its unique manufacturing technology and a steel plate housing. The housing is made of steel plate that is locally reinforced by press working, making it highly rigid, lightweight and compact.... Read MoreShaft Hole Type Cylindrical hole type Type Diamond flange unit
- OILES Oiles Pillow # 80 Diamond Flange UnitOILES Pillow 80 is a self-aligning bearing composed of OILES # 80 and reinforced plastic. It is oil-free, lightweight, and has excellent rust resistance. It can be easily attached to places where it is difficult to form an oil film, and has excellent load resistance, wear resistance, and speed ch... Read MoreShape Diamond flange unit
- FYH (NIPPON PILLOW BLOCK) Take-up unitA bearing unit that combines a ball bearing for the unit and a bearing box with a slide groove. By moving the bearing box in the radial direction along the slide groove, the support position at the center of the shaft can be adjusted.RoHS directive (corresponding to 10 substances) Correspondence Shaft Hole Type Cylindrical hole (with set screw) Shape Take-up unit