Spherical Plain Bearings
A spherical plain bearing is a bearing in which the inner ring and outer ring make spherical contact. Spherical plain bearings that excel in self-alignment and can handle radial and axial loads are resistant to vibration and tilting motions, and are suitable for low-speed rotational motions. In addition to the type used for lubrication, the type with excellent self-lubricating properties such as those with a Teflon finish on the inner surface of the race is a convenient item that keeps the surrounding environment normal because there is no contamination due to lubrication. It can also be used at food processing sites where refueling is not possible. It is a good idea to choose items that are appropriate for your work purpose and the equipment you are using.
Other Related Pages
- THK Spherical Bearing PB TypeRoHS directive (corresponding to 10 substances) Correspondence Type PB type
- IKO (NIPPON THOMPSON) Pillow Ball Spherical Plain Bearing PBThis bearing is a wear-resistant and rigid bearing in which a familiar special copper alloy bush is inserted between the inner ring and the outer ring, which are precision-finished after quenching and hardening and chrome-plated on the spherical surface. is. Shaft and housingSpecification 1N≒0.102kgf Type Refueling type
- IKO (NIPPON THOMPSON) Oil lubricated spherical plain bearings GE □ ES-2RS (with seal)A bearing with a large load capacity that operates with low torque and has excellent wear resistance. Especially suitable for alternating loads and impact loads. Industrial machinery, construction machinery, etc.Type GE-ES-2RS Presence of seal With seal
- IKO (NIPPON THOMPSON) Oil-free spherical plain bearing GEEC type (no seal)It is an international bearing with the same main dimensions as the GE-ES series. A maintenance-free spherical plain bearing with little creep deformation due to compressive load and excellent wear resistance. Especially suitable for applying a load in a certain direction. For fields that dislike... Read MoreAngle α1 (°) - Specification 1N≒0.102Kgf Type GE-EC type Presence of seal Without seal
- IKO (NIPPON THOMPSON) Lubrication spherical plain bearings GEE, ES type (no seal)High carbon chrome bearing steel is used for both the inner and outer rings, and the sliding surface is treated with a phosphate film and covered with a dry film of molybdenum disulfide (MoS2), so it operates with low torque and has wear resistance. A bearing with excellent load capacity. Especia... Read MoreType Without seal Presence of seal Without seal
- IKO (NIPPON THOMPSON) Lubricated spherical plain bearing SB □ A (without seal)A bearing with a large load capacity that operates with low torque and has excellent wear resistance. Suitable when alternating load or impact load works. Industrial machinery, construction machinery, etc.Type SB-A type
- IKO (NIPPON THOMPSON) Oil-free spherical plain bearings GE □ EC type (with seal)Angle α (°) - Type GE-EC-2RC Presence of seal With seal
- Igus (R) Igubal® spherical bearingsBearing Press-fit spherical bearing Maximum static compression load (N) Radial: Axial: Series E seriesfrom S$13.99Min. 5 days
- IKO (NIPPON THOMPSON) Lubricated spherical plain bearing SB (without seal)Type SB typefrom S$22.99Min. 3 days
- CCTY Bearing Japan Lubrication type spherical plain bearing with sealRoHS directive (corresponding to 10 substances) Correspondence Type GE-ES typefrom S$14.99Min. 2 days
- IKO (NIPPON THOMPSON) Lubrication type spherical plain bearing inch series SBBType SBB typefrom S$23.99Min. 5 days
- IKO (NIPPON THOMPSON) Lubricated spherical plain bearing SB-AThe outer ring is split into one, and the inner and outer rings are not separated, making it easy to handle before installation and to install in the housing.from S$199.90Min. 4 days
- CCTY Bearing Japan CCVI lubricated spherical plain bearingRoHS directive (corresponding to 10 substances) Correspondencefrom S$68.99Min. 6 days
- CCTY Bearing Japan Oil-Free Spherical Plain BearingRoHS directive (corresponding to 10 substances) Correspondence
- NMB (Minebea) Spherical PTFE Type Standard TypeA Teflon liner is adhered to the inner diameter surface of the race, and it slides on the spherical surface of the ball and the Teflon liner surface. Since the Teflon liner is self-lubricating, no lubricant such as grease is required. Therefore, it is effective for use in places where oil is disl... Read MoreRoHS directive (corresponding to 10 substances) Correspondence Material (Lace) SUS410 Material (Ball) SUS440C Material (Lining) TFE (tetrafluoroethylene)
- CCTY Bearing Japan CCVI lubricated spherical plain bearings wide typeRoHS directive (corresponding to 10 substances) Correspondencefrom S$11.99Min. 6 days
- CCTY Bearing Japan Lubricated spherical plain bearingsRoHS directive (corresponding to 10 substances) Correspondencefrom S$399.90Min. 8 days
- CCTY Bearing Japan CCVI lubricated spherical plain bearing with sealRoHS directive (corresponding to 10 substances) Correspondencefrom S$89.99Min. 6 days
- Igus (R) Igball Resin spherical bearingIt can be used in adverse environments. Compatible with metal housings. Conveyors, packaging machines, etc.Set Contents Igball Spherical bearing Material / Finish Igridur Jfrom S$29.99Min. 5 days
- CCTY Bearing Japan CCVI lubricated spherical plain bearings wide type with sealRoHS directive (corresponding to 10 substances) Correspondencefrom S$29.99Min. 6 days
- IKO (NIPPON THOMPSON) Pillow ball spherical plain bearing PB (insert type)A wear-resistant and rigid bearing with a familiar special copper alloy bush inserted between the inner ring and the outer ring, which are precision-finished after quenching and chrome-plated on the spherical part. It is used by attaching it to.Discontinued
- IKO (NIPPON THOMPSON) Oil-free spherical plain bearings GE-ECIt is an international bearing with the same main dimensions as the refueling spherical plain bearing GE-ES. Since a special PTFE liner reinforced with a copper alloy net is used for the sliding surface, it is a maintenance-free spherical plain bearing with little creep deformation due to pressur... Read MoreDiscontinued
- No Brand Spherical bearing SB typeThe material and other parts are the same as the GE type, but the width and thickness are larger than the GE, making it suitable for heavier load applications. The outer ring has a split structure, and the inner and outer rings have oil grooves and oil holes. * Please refuel regularly. Lithium-ba... Read MoreDiscontinued
- IKO (NIPPON THOMPSON) Lubricated spherical plain bearing SBThe outer ring is divided into two, and a ring is attached to the outer peripheral groove of the outer ring to hold the inner and outer rings.Discontinued