Linear Motors
- ORIENTAL MOTOR Linear head LH series 5L typeThe basic speed is based on the value calculated based on the synchronous rotation speed of the motor (50Hz: 1500r / min). The actual speed will vary depending on the size of the load and the power frequency. The maximum load is the limit of the load capacity determined by the strengthening of th... Read MoreMaximum Load (kg) (50 / 60Hz) 140 Rack Speed (mm/s) 20 Type Linear motor Power Supply Alternating currentfrom S$749.90Min. 2 days
- ORIENTAL MOTOR Linear head LH series 2L typeThe basic speed is based on the value calculated based on the synchronous rotation speed of the motor (50Hz: 1500r / min). The actual speed will vary depending on the size of the load and the power frequency. The maximum load is the limit of the load capacity determined by the strengthening of th... Read MoreVoltage (V) 100 Type Linear motor Frequency (Hz) 50/60 Rack moving direction Parallel to the mounting leg surface Power Supply Single-phasefrom S$269.90Min. 11 days
- ORIENTAL MOTOR Linear head LH series 4L typeThe basic speed is based on the value calculated based on the synchronous rotation speed of the motor (50Hz: 1500r / min). The actual speed will vary depending on the size of the load and the power frequency. The maximum load is the limit of the load capacity determined by the strengthening of th... Read MoreRack Speed (mm/s) 10 Type Linear motor Maximum Load (kg) (50 / 60Hz) 70/70 Gear Head Mounting Square Dimension (mm) 80 Power Supply Alternating current Rack moving direction Parallel to the mounting leg surfacefrom S$329.90Min. 11 days
- ORIENTAL MOTOR Linear head LH series 4L typeThe basic speed is based on the value calculated based on the synchronous rotation speed of the motor (50Hz: 1500r / min). The actual speed will vary depending on the size of the load and the power frequency. The maximum load is the limit of the load capacity determined by the strengthening of th... Read MoreType Linear motor Power Supply Alternating current Maximum Load (kg) (50 / 60Hz) 35/31 Rack moving direction Vertical to the mounting leg surface Rack Speed (mm/s) 45 Gear Head Mounting Square Dimension (mm) 80from S$329.90Min. 10 days
- ORIENTAL MOTOR Linear head LH series 0L typeThe basic speed is based on the value calculated based on the synchronous rotation speed of the motor (50Hz: 1500r / min). The actual speed will vary depending on the size of the load and the power frequency. The maximum load is the limit of the load capacity determined by the strengthening of th... Read MoreOutput (kW) 0.001 Type Linear motor / reversible motor Rack moving direction Parallel to the mounting leg surface Power Supply Single-phasefrom S$399.90Min. 11 days
- ORIENTAL MOTOR Linear head LH series 4L typeThe basic speed is based on the value calculated based on the synchronous rotation speed of the motor (50Hz: 1500r / min). The actual speed will vary depending on the size of the load and the power frequency. The maximum load is the limit of the load capacity determined by the strengthening of th... Read MoreMaximum Load (kg) (50 / 60Hz) 35/31 Rack Speed (mm/s) 45 Type Linear motor Gear Head Mounting Square Dimension (mm) 80 Power Supply Alternating current Rack moving direction Parallel to the mounting leg surfacefrom S$329.90Min. 11 days
- ORIENTAL MOTOR Linear head LH series 5L typeThe basic speed is based on the value calculated based on the synchronous rotation speed of the motor (50Hz: 1500r / min). The actual speed will vary depending on the size of the load and the power frequency. The maximum load is the limit of the load capacity determined by the strengthening of th... Read MoreRack Speed (mm/s) 10 Maximum Load (kg) (50 / 60Hz) 140 Type Linear motor Power Supply Alternating currentfrom S$749.90Min. 10 days
- ORIENTAL MOTOR Linear head LH series 5L typeThe basic speed is based on the value calculated based on the synchronous rotation speed of the motor (50Hz: 1500r / min). The actual speed will vary depending on the size of the load and the power frequency. The maximum load is the limit of the load capacity determined by the strengthening of th... Read MoreMaximum Load (kg) (50 / 60Hz) 140 Rack Speed (mm/s) 20 Type Linear motor Power Supply Alternating currentfrom S$749.90Min. 10 days
- ORIENTAL MOTOR Linear head LH series 4L typeThe basic speed is based on the value calculated based on the synchronous rotation speed of the motor (50Hz: 1500r / min). The actual speed will vary depending on the size of the load and the power frequency. The maximum load is the limit of the load capacity determined by the strengthening of th... Read MoreRack Speed (mm/s) 10 Type Linear motor Maximum Load (kg) (50 / 60Hz) 70/70 Gear Head Mounting Square Dimension (mm) 80 Power Supply Alternating current Rack moving direction Vertical to the mounting leg surfacefrom S$329.90Min. 10 days
- ORIENTAL MOTOR Linear head LH series 0L typeThe basic speed is based on the value calculated based on the synchronous rotation speed of the motor (50Hz: 1500r / min). The actual speed will vary depending on the size of the load and the power frequency. The maximum load is the limit of the load capacity determined by the strengthening of th... Read MoreOutput (kW) 0.001 Type Linear motor / reversible motor Power Supply Single-phase Rack moving direction Vertical to the mounting leg surfacefrom S$399.90Min. 11 days
- ORIENTAL MOTOR Linear head LH series 4L typeThe basic speed is based on the value calculated based on the synchronous rotation speed of the motor (50Hz: 1500r / min). The actual speed will vary depending on the size of the load and the power frequency. The maximum load is the limit of the load capacity determined by the strengthening of th... Read MoreRack Speed (mm/s) 20 Type Linear motor Maximum Load (kg) (50 / 60Hz) 67/58 Gear Head Mounting Square Dimension (mm) 80 Power Supply Alternating current Rack moving direction Parallel to the mounting leg surfacefrom S$329.90Min. 11 days
- ORIENTAL MOTOR Linear head LH series 4L typeThe basic speed is based on the value calculated based on the synchronous rotation speed of the motor (50Hz: 1500r / min). The actual speed will vary depending on the size of the load and the power frequency. The maximum load is the limit of the load capacity determined by the strengthening of th... Read MoreRack Speed (mm/s) 20 Type Linear motor Maximum Load (kg) (50 / 60Hz) 67/58 Gear Head Mounting Square Dimension (mm) 80 Power Supply Alternating current Rack moving direction Vertical to the mounting leg surfacefrom S$329.90Min. 10 days
- ORIENTAL MOTOR Linear head LH series 2L typeThe basic speed is based on the value calculated based on the synchronous rotation speed of the motor (50Hz: 1500r / min). The actual speed will vary depending on the size of the load and the power frequency. The maximum load is the limit of the load capacity determined by the strengthening of th... Read MoreVoltage (V) 100 Type Linear motor Frequency (Hz) 50/60 Power Supply Single-phase Rack moving direction Vertical to the mounting leg surfacefrom S$269.90Min. 13 days
- ORIENTAL MOTOR Linear head LH series 5L typeThe basic speed is based on the value calculated based on the synchronous rotation speed of the motor (50Hz: 1500r / min). The actual speed will vary depending on the size of the load and the power frequency. The maximum load is the limit of the load capacity determined by the strengthening of th... Read MoreMaximum Load (kg) (50 / 60Hz) 111/104 Rack Speed (mm/s) 45 Type Linear motor Power Supply Alternating currentfrom S$689.90Min. 10 days
- ORIENTAL MOTOR Linear head LH series 5L typeThe basic speed is based on the value calculated based on the synchronous rotation speed of the motor (50Hz: 1500r / min). The actual speed will vary depending on the size of the load and the power frequency. The maximum load is the limit of the load capacity determined by the strengthening of th... Read MoreMaximum Load (kg) (50 / 60Hz) 111/104 Rack Speed (mm/s) 45 Type Linear motor Power Supply Alternating currentfrom S$689.90Min. 10 days
- ORIENTAL MOTOR Linear head LH series 5L typeThe basic speed is based on the value calculated based on the synchronous rotation speed of the motor (50Hz: 1500r / min). The actual speed will vary depending on the size of the load and the power frequency. The maximum load is the limit of the load capacity determined by the strengthening of th... Read MoreRack Speed (mm/s) 10 Maximum Load (kg) (50 / 60Hz) 140 Type Linear motor Power Supply Alternating currentfrom S$749.90Min. 10 days
- ORIENTAL MOTOR Lineard motor LD series (with terminal box) R type lineard motorThe basic speed is calculated based on the synchronous rotation speed of the motor (50Hz: 1500rpm). The actual speed is 2 to 20% less than the displayed value depending on the size of the load. The overrun value is the value when the rack is operated horizontally. The values in parentheses are th... Read MoreType Terminal box type Rack moving direction Vertical to the mounting leg surface Gear Head Mounting Square Dimension (mm) 80Discontinued
- MIKI PULLEY Linear shaft drive SHM-16 + SHD2-06Ambient Humidity (% RH) 80 or less (no condensation)Discontinued
- ORIENTAL MOTOR Linear motor with contactless circuit LU series (with terminal box)For linear motors that can easily obtain linear operation with a motor and rack and pinion mechanism, Since the non-contact controller pack is set, control can be performed easily. In addition, the optional linear controller has a built-in typical operation pattern for linear motion, making it ea... Read MoreRack Speed (mm/s) 10 Type Terminal box type Motor Type Lineard motorDiscontinued
- ORIENTAL MOTOR Linearized motor LU series with contactless circuit (type with electromagnetic brake)The basic speed is based on the value calculated based on the synchronous rotation speed of the motor (50Hz: 1500rpm). When moving vertically, the load that can be driven is the maximum load minus the rack mass (0.5 to 1.2 kg depending on the stroke). When receiving a load with a guide or the lik... Read MoreRack Speed (mm/s) 20 Motor Type Lineard motor Type Type with electromagnetic brakeDiscontinued
- ORIENTAL MOTOR Linear motor LD series (with electromagnetic brake)The basic speed is based on the value calculated based on the synchronous rotation speed of the motor (50Hz: 1500rpm). The actual speed depends on the size of the load and the power frequency. When moving vertically, the load that can be driven is the maximum load minus the rack mass. When receiv... Read MoreRack Speed (mm/s) 100Discontinued
- ORIENTAL MOTOR Linearized motor LU series with contactless circuit (type with electromagnetic brake)The basic speed is based on the value calculated based on the synchronous rotation speed of the motor (50Hz: 1500rpm). When moving vertically, the load that can be driven is the maximum load minus the rack mass (0.5 to 1.2 kg depending on the stroke). When receiving a load with a guide or the lik... Read MoreRack Speed (mm/s) 10 Type Type with electromagnetic brake Motor Type Lineard motorDiscontinued
- ORIENTAL MOTOR Linear motor with contactless circuit LU series (with terminal box)For linear motors that can easily obtain linear operation with a motor and rack and pinion mechanism, Since the non-contact controller pack is set, control can be performed easily. In addition, the optional linear controller has a built-in typical operation pattern for linear motion, making it ea... Read MoreRack Speed (mm/s) 20 Type Terminal box type Motor Type Lineard motorDiscontinued
- ORIENTAL MOTOR Linearized motor LU series with contactless circuit (type with electromagnetic brake)The basic speed is based on the value calculated based on the synchronous rotation speed of the motor (50Hz: 1500rpm). When moving vertically, the load that can be driven is the maximum load minus the rack mass (0.5 to 1.2 kg depending on the stroke). When receiving a load with a guide or the lik... Read MoreType Type with electromagnetic brake Motor Type Lineard motor Rack Speed (mm/s) 10Discontinued
- ORIENTAL MOTOR Linearized motor LU series with contactless circuit (type with electromagnetic brake)The basic speed is based on the value calculated based on the synchronous rotation speed of the motor (50Hz: 1500rpm). When moving vertically, the load that can be driven is the maximum load minus the rack mass (0.5 to 1.2 kg depending on the stroke). When receiving a load with a guide or the lik... Read MoreRack Speed (mm/s) 10 Motor Type Lineard motor Type Type with electromagnetic brakeDiscontinued
- ORIENTAL MOTOR Linearized motor LU series with contactless circuit (type with electromagnetic brake)The basic speed is based on the value calculated based on the synchronous rotation speed of the motor (50Hz: 1500rpm). When moving vertically, the load that can be driven is the maximum load minus the rack mass (0.5 to 1.2 kg depending on the stroke). When receiving a load with a guide or the lik... Read MoreType Type with electromagnetic brake Rack Speed (mm/s) 20 Motor Type Lineard motorDiscontinued
- ORIENTAL MOTOR Linear motor LD series (with electromagnetic brake)The basic speed is based on the value calculated based on the synchronous rotation speed of the motor (50Hz: 1500rpm). The actual speed depends on the size of the load and the power frequency. When moving vertically, the load that can be driven is the maximum load minus the rack mass. When receiv... Read MoreRack Speed (mm/s) 100Discontinued
- ORIENTAL MOTOR Lineard motor LD series (with terminal box) R type lineard motorThe basic speed is calculated based on the synchronous rotation speed of the motor (50Hz: 1500rpm). The actual speed is 2 to 20% less than the displayed value depending on the size of the load. The overrun value is the value when the rack is operated horizontally. The values in parentheses are th... Read MoreRack moving direction Vertical to the mounting leg surface Type Terminal box type Gear Head Mounting Square Dimension (mm) 80Discontinued
- ORIENTAL MOTOR Linear motor with contactless circuit LU series (without linear controller)Type Without linear controller Rack Speed (mm/s) 45 Motor Type Lineard motorDiscontinued
- ORIENTAL MOTOR Linear motor LD series (with electromagnetic brake)The basic speed is based on the value calculated based on the synchronous rotation speed of the motor (50Hz: 1500rpm). The actual speed depends on the size of the load and the power frequency. When moving vertically, the load that can be driven is the maximum load minus the rack mass. When receiv... Read MoreRack moving direction Vertical to the mounting leg surface Gear Head Mounting Square Dimension (mm) 80 Type Type with electromagnetic brakeDiscontinued
- ORIENTAL MOTOR Linear motor with contactless circuit LU series (without linear controller)Rack Speed (mm/s) 20 Type Without linear controller Motor Type Lineard motorDiscontinued
- ORIENTAL MOTOR Linear motor with contactless circuit LU series (with terminal box)For linear motors that can easily obtain linear operation with a motor and rack and pinion mechanism, Since the non-contact controller pack is set, control can be performed easily. In addition, the optional linear controller has a built-in typical operation pattern for linear motion, making it ea... Read MoreMotor Type Lineard motor Rack Speed (mm/s) 45 Type Terminal box typeDiscontinued
- ORIENTAL MOTOR Linearized motor LU series with contactless circuit (type with electromagnetic brake)The basic speed is based on the value calculated based on the synchronous rotation speed of the motor (50Hz: 1500rpm). When moving vertically, the load that can be driven is the maximum load minus the rack mass (0.5 to 1.2 kg depending on the stroke). When receiving a load with a guide or the lik... Read MoreRack Speed (mm/s) 100Discontinued
- ORIENTAL MOTOR Linear motor with contactless circuit LU series (without linear controller)Rack Speed (mm/s) 10 Type Without linear controller Motor Type Lineard motorDiscontinued
- ORIENTAL MOTOR Linearized motor LU series with contactless circuit (type with electromagnetic brake)The basic speed is based on the value calculated based on the synchronous rotation speed of the motor (50Hz: 1500rpm). When moving vertically, the load that can be driven is the maximum load minus the rack mass (0.5 to 1.2 kg depending on the stroke). When receiving a load with a guide or the lik... Read MoreRack Speed (mm/s) 20 Type Type with electromagnetic brake Motor Type Lineard motorDiscontinued
- ORIENTAL MOTOR Linearized motor LU series with contactless circuit (type with electromagnetic brake)The basic speed is based on the value calculated based on the synchronous rotation speed of the motor (50Hz: 1500rpm). When moving vertically, the load that can be driven is the maximum load minus the rack mass (0.5 to 1.2 kg depending on the stroke). When receiving a load with a guide or the lik... Read MoreRack Speed (mm/s) 100Discontinued
- ORIENTAL MOTOR Lineard motor LD series (with terminal box) R type lineard motorThe basic speed is calculated based on the synchronous rotation speed of the motor (50Hz: 1500rpm). The actual speed is 2 to 20% less than the displayed value depending on the size of the load. The overrun value is the value when the rack is operated horizontally. The values in parentheses are th... Read MoreType Terminal box typeDiscontinued