Torsion Springs
- SHK Torsion Spring (Packed)A spring used by receiving a torsional moment around the coil shaft. It is widely used for opening and closing manhole covers, strong nippers, opening and closing doorknobs, and pinching clips.
- Tsuchino Kick spring* Please use after confirming the proper load. * Please refrain from using it for any other purpose. * Please do not use it in a deformed or damaged state.RoHS directive (corresponding to 10 substances) Correspondence
- WAKI Stainless steel kick springSmall box Nebuta, plastic model, toysMaterial Stainless steel SUS304from S$1.59Min. 2 days
- WAKI Iron kick springSmall box Nebuta, plastic model, toysMaterial Chromate steel wire Wire diameter (mm) 2
- WAKI Black plated kick springSmall box Nebuta, plastic model, toysMaterial Black plated steel wirefrom S$1.49Min. 3 days
- Tsuchino Chromate band spring* Please use after confirming the proper load. * Please refrain from using it for any other purpose. * Please do not use it in a deformed or damaged state.Material Chromate steel wire RoHS directive (corresponding to 10 substances) Correspondencefrom S$4.49Min. 7 days
- TRUSCO Torsion Spring (Stainless Steel)A spring that uses a cylindrically wound spring in a twisting direction with respect to the coil center line. When used in the direction of closing the arm angle, the diameter of the spring support rod is ideally about 90% of the coil inner diameter at maximum load because the coil diameter is re... Read MoreMaterial / Finish Stainless steel (SUS304-WPB) Spring Type Torsion springfrom S$29.99Min. 3 days
- TRUSCO Torsion Spring (Stainless) 135 ° TypeA spring that uses a cylindrically wound spring in a twisting direction with respect to the coil center line. When used in the direction of closing the arm angle, the diameter of the spring support rod is ideally about 90% of the coil inner diameter at maximum load because the coil diameter is re... Read MoreMaterial / Finish Stainless steel (SUS304-WPB)from S$29.99Min. 3 days
- TRUSCO Torsion Spring (Stainless) 180 ° TypeA spring that uses a cylindrically wound spring in a twisting direction with respect to the coil center line. When used in the direction of closing the arm angle, the diameter of the spring support rod is ideally about 90% of the coil inner diameter at maximum load because the coil diameter is re... Read MoreMaterial / Finish Stainless steel (SUS304-WPB)from S$29.99Min. 3 days
- TRUSCO Torsion Spring (Stainless Steel)A spring that uses a cylindrically wound spring in a twisting direction with respect to the coil center line. When used in the direction of closing the arm angle, the diameter of the spring support rod is ideally about 90% of the coil inner diameter at maximum load because the coil diameter is re... Read MoreSpring Type Torsion springfrom S$24.99Min. 3 days
- TRUSCO Torsion spring (stainless steel)A spring that uses a cylindrically wound spring in a twisting direction with respect to the coil center line. When used in the direction of closing the arm angle, the diameter of the spring support rod is ideally about 90% of the coil inner diameter at maximum load because the coil diameter is re... Read MoreDiscontinued