Tooth Brushing
Toothpaste is a sanitary product that cleans teeth and gums. It is indispensable for daily oral care such as prevention of tooth decay, periodontal disease, and bad breath. Toothbrushes can be selected according to the purpose, such as the size of the head, the hardness of the bristles, and the shape of the bristles. increase. Toothpaste (toothpaste) generally contains medicinal ingredients such as fluoride and bactericides, and has a refreshing flavor. Mouthwashes that can cleanse the oral cavity without using a toothbrush include alcohol-based mouthwashes that provide a refreshing feel and non-alcoholic types that give a mild sensation.
Other Related Pages
- LION Systema Dental Tuft Periodontal Pocket Intensive CareA tuft brush for partial polishing that allows intensive care by aiming at the periodontal pocket with pinpoint because it is a small head. Since the tips of the hair are ultra-fine, the dirt in the back of the targeted periodontal pocket is thoroughly scraped off together with the periodontal di... Read MoreTarget For adults Series Systemafrom S$4.49Min. 2 days
- HUKUBA DENTAL Kiss You FlatA toothbrush that doesn't need to be scuffed to remove dirt and is gentle and squishy. Lightly moisten the ends of the hair and put the palm or the terminal (silver part) on the palm or Negative ions flow into your mouth from the built-in battery just by brushing with your finger touchingTarget For adultsfrom S$2.89Min. 3 days
- SUNSTAR Gum Advance Dental Brush # 528 Compact"Multifunctional flocking" + "three tips" effectively removes periodontal plaque from the interdental papilla where the causative bacteria of periodontal disease are lurking.Target For adults Series GUM Hardness Normalfrom S$6.99Min. 3 days
- LION Biteen HabrushThe mountain cutting cut is perfect between teeth! A toothbrush that cleans the space between teeth. * Color cannot be specified.Dimensions, Width W x Height H x Depth D (mm) 33×230×14 Series Bitine Target For adults
- DENTALPRO Fresh toothbrush Tip flockingThe tip is hardened and the plaque is scraped off from the back teeth!Target For adults
- Create Dent Fine YamakiriGet in firmly and remove plaqueTarget For adults
- LION Dentistima Lion Lion BrushAll hair tips are ultra-fine hair, toothbrush for periodontal disease care.Dimensions, Width W x Height H x Depth D (mm) 33×230×14 Series Systema
- EBISU Premium care toothbrush, 7-row regularIt is wide, has about twice the number of pores (compared to the manufacturer), has a large amount of flocked hair, and has a wide contact surface with teeth, so it can be easily and efficiently polished. Wide head shape that covers teeth more widely by increasing one row horizontally. Two types ... Read MoreTarget For adults
- DENTALPRO Fresh Toothbrush Tip SpiralSince the hair at the tip is spiral, dirt can be removed even on the side of the hair.Target For adults Material Saturated polyester resin
- Nishiwaki Kogyo Slim F toothbrush chamfer CThe chevron cut scrapes out the teeth and plaque on the teeth.Target For adults
- DENTALPRO Fresh toothbrush M-cutThe jagged M-cut removes dirt between teeth that is difficult to remove!Heat Resistance Temperature (℃) 80 degrees Target For adults Material Saturated polyester resin
- Nishiwaki Kogyo Black Odin HabrushThe black pearl component makes it easier to remove stains on the paper surface due to the micro irregularities on the surface. Since all the tips are tapered, it penetrates deeper into the periodontal pocket and removes plaque.Target For adults
- LION EX One TuftA partial brush for cleaning areas that tend to be left unpolished, such as the interdental area, cervical area, crowding area, distal part of molars, periodontal pocket, and around the orthodontic appliance. We have a lineup of 3 types of hair tips that can be used according to various cases. S:... Read More
- LION Biteen Habrush Clear ColorThe tips of small mountain-cut hairs can penetrate between teeth and small dents to remove plaque firmly. * Color cannot be specified.Dimensions, Width W x Height H x Depth D (mm) 33×230×14 Series Bitine Target For adultsfrom S$2.39Min. 2 days
- LION Sistemaha brush firm hair typeA toothbrush for periodontal disease care that has an evolved thin head and can easily reach the periodontal pocket at the back of the mouth, which was difficult to reach until now. Ultra-fine hair with a double-core structure for a firm brushing feel. The inverted U-shaped flocking that wraps ar... Read MoreTarget For adults Series Systemafrom S$3.89Min. 2 days
- DENTALPRO Fresh extra fine hair MThe tips of ultra-fine hair get into the periodontal pocket and remove plaque!Target For adults
- Feed Toothbrush set with toothpasteMade in Japan with peace of mind for toothbrushes and toothpaste. Ready to use! Toothbrush with toothpaste. Contains naturally derived sweetener and xylitol.Overall Length (mm) 150 Target For adults Specification Number of pores: 21 holes Material (Bristle) Polypropylene Material (Handle) Polypropylene
- Nishiwaki Kogyo Nishiwaki Doctor OdinTapered hair gets into periodontal pockets and between teeth to remove plaqueTarget For adults
- EBISU Medifit Clear Toothbrush Super Tapered HairUltra-tapered toothbrush suitable for periodontal disease control. Ultra-tapered bristles reach the periodontal pocket to thoroughly scrape plaque, and flat bristles remove dirt on the tooth surface.Target For adults
- ANNECY Toothbrush toothbrushA set of 6 disposable toothbrushes for travel and visitors.Heat Resistance Temperature (℃) 80 Target For adults Material (Bristle) Polypropylene Material (Handle) Polypropylene
- EBISU The Premium Care Huber RegularYou can polish it smoothly with a super-tight brush. Plaque is efficiently removed by flocking in stages where the hardness of the hair increases toward the center. A thin head that is easy to polish.Target For adultsfrom S$5.99Min. 2 days
- EBISU NEW Ebisu Pig HairA pig hair toothbrush that gently protects tooth enamel. Since it uses high quality Chinese Chongqing pig hair, it is effective for gingival massage with its moderate firmness. In addition, even after repeated use, the flocked part does not open and the hair itself wears, so there is no need to w... Read MoreTarget For adults
- SUNSTAR Gum dental brush # 191 super compact headTapered bristles (tapered bristles) and satinized bristles remove periodontal plaque at the boundary between teeth and haguki.Target For adults Series GUMfrom S$4.49Min. 2 days
- EBISU Premium care toothbrush, 6-row regularSince it has 48 holes, which is about twice the size of the conventional head (compared to the manufacturer), the amount of flocking is large and the contact surface with the teeth is wide, so plaque can be removed easily and efficiently. Two types of bristles that use ultra-tapered bristles to e... Read MoreTarget For adults
- LION Systema Haguki Plus HabrushSystema Haguki Plus Haguki is a toothbrush that can be used to care for periodontal disease for those who are concerned about the melting of their teeth. Since it has stepped hair transplantation, it fits gently into both periodontal pockets and toothpaste, and it features high-density ultra-fine... Read MoreTarget For adults Series Systemafrom S$4.79Min. 2 days
- SUNSTAR Gum dental brush # 202 3-row compactMicro hair penetrates into narrow gaps and boundaries, and the strength of the hair removes periodontal plaque that causes periodontal disease. * Color cannot be specified.Target For adults Series GUM Hardness Normalfrom S$4.19Min. 2 days
- LION CLINICA ADVANTAGE HABRUSHJapan's highest level ultra-thin head / ultra-fine neck that reaches deeper into the back teeth-Super slim / dentist recommended design-Japan's highest level "ultra-thin head" / "ultra-fine neck" that reaches deeper into the back teeth Flat cut with "elastic fit h... Read MoreSeries Clinica Target For adultsfrom S$3.59Min. 2 days
- DENTALPRO Dental Pro Black Ultra Fine Hair Ultra Compact"Even with water alone, teeth are slippery!" Dental Pro Black series using "black special hair" that has a 15% higher plaque removal rate than normal polyester hair. The definitive version of the black toothbrush has become a thin head and will be newly released with improveme... Read MoreTarget For adultsfrom S$4.49Min. 2 days
- Kobayashi Pharmaceutical Shoyou Interdental ToothbrushA toothbrush to prevent alveolar pyorrhea that allows you to brush between teeth at the same time because the central interdental cleaning bristles enter between teeth.Target For adults Series Fresh leaves Hardness Normalfrom S$4.49Min. 2 days
- LION CLINICA ADVANTAGE Toothbrush 3 Rows"Ultra-thin head" with extremely thin head that reaches deeper into the back teeth "Resilient fit hair" that firmly scrapes out plaque between gaps "Hexagonal slim handle" that is easy to hold with a pen grip and easy to polish with a light force 3rd row: "Taper... Read MoreSeries Clinica Target For adultsfrom S$3.79Min. 2 days
- SUNSTAR Do clear toothbrush compact"Double tip flocking" and "tapered head" can be used to polish the back of the molars. By cutting the thickness of the long slim neck, head, and neck, which are easy to bend, by 10% (compared to conventional products), the operability in the mouth is greatly improved and it is... Read MoreTarget For adultsfrom S$2.99Min. 2 days
- SUNSTAR Gum Dental Brushes # 211, 3 Rows CompactTapered bristles (tapered bristles) and satinized bristles remove periodontal plaque at the boundary between teeth and haguki.Target For adults Series GUMfrom S$4.49Min. 2 days
- Nishiwaki Kogyo Dr. Odin finish brushing brushed taperBrushing gently on delicate milk teethTarget For adults
- LION CLINICA Advantage Toothbrush CompactJapan's highest level ultra-thin head / ultra-fine neck that reaches deeper into the back teeth-Super slim / dentist recommended design-Japan's highest level "ultra-thin head" / "ultra-fine neck" that reaches deeper into the back teeth Flat cut with "elastic fit h... Read MoreSeries Clinica Target For adultsfrom S$3.59Min. 3 days
- Lion Dental Products Lion + DENT. EX Systema +44The popular Dent Systema series has been renewed and the handle color has increased to 5 colors. Lion's unique super-tapered hair reaches the periodontal pockets and interdental areas without difficulty, Great for plaque control. 42 is a regular head, 44 is a compact head, and the hardness of... Read MoreTarget For adultsfrom S$4.49Min. 2 days
- DENTALPRO Fresh black toothbrush"Even with water alone, teeth are slippery!" Dental Pro Black series using "black special hair (special hair with platinum colloid ceramic)" that has a 15% higher plaque removal rate than normal polyester hair. Standard model of "Dental Pro Black Series". If you get ... Read MoreTarget For adults
- DENTALPRO Fresh extra fine hairThe tips of ultra-fine hair get into the periodontal pocket and remove plaque!Hardness Soft Target For adults
- SUNSTAR Gum dental brush # 166 3 rows super compactUltra-tapered hair (ultra-tapered hair tips) & satinized hair tips reach the depths of the periodontal pockets and expel periodontal plaque.Target For adults Series GUM Hardness Softfrom S$4.49Min. 2 days
Filter by categories