Plug-in Air Fresheners
- S.T. Deodorant Plug TypeDeodorize a large space with electronic power.Where to Use Indoor Classification of the Hazardous Non-dangerous goods Fragrance Unscented
- S.T. Deodorizing plug automaticallyA battery-powered auto-spray type deodorant air freshener that sprays deodorant fragrance components at regular intervals while adjusting the number of sprays with an optical sensor, so you can always feel the fresh scent and effect until the final spatter! "Spatter" spray at regular in... Read MoreType BodyDiscontinued
- S.T. Deodorizing plug automaticallyFirmly deodorizes anxious odors. The deodorant effect and fresh scent last from the beginning to the end of use. W effect of the sensor that responds to brightness! When it gets dark, the number of sprays is reduced, and when it gets bright, it is sprayed for the effect. With 3 levels of fragranc... Read MoreDimensions, Width W x Height H x Depth D (mm) 78×170×60 Type Body Mass (g) 245 Ingredient Fragrance, ethanolDiscontinued
- S.T. Deodorizing plug automaticallyBy automatic spraying, the deodorant fragrance effect spreads in the space where odors tend to be muffled at a certain timing, so the constant deodorant effect lasts from the beginning to the end, and you can always feel the fresh scent and effect. It is a battery-powered automatic deodorant spra... Read MoreCapacity (mL) 41 Ingredient Fragrance, ethanolDiscontinued
- S.T. Deodorizing plug automaticallySpray every time the time comes. The deodorant effect lasts until the end. Feel the fresh scent at any time. If you want to deodorize immediately, use the spray button to instantly deodorize. Ideal for spaces where odors tend to be muffled. It is an economical replacement ceremony. 3-step fragran... Read MoreCapacity (mL) 41 Main Unit Dimensions, Width W x Depth D x Height H (mm) 75×47×140 Type Body Included Accessories Sample battery (AA) x 2, spray can Ingredient Fragrance, ethanolDiscontinued
- S.T. Spray for changing spuds and deodorant plugs automaticallyAutomatic deodorization at regular intervals! A fresh space always continues. Ideal for spaces where odors tend to be muffled. It can be used for both old and new designs. Entrance, washroom, toilet, etc. * Keep your face away from the injection port. * Do not use near flames or fire. Do not plac... Read MoreType DistributionDiscontinued
- S.T. Deodorant plug typeSince it is an outlet type, it deodorizes large rooms such as LDK (about 16 tatami mats) and continuous spaces such as entrances and corridors with electronic power, and the scent spreads. A constant deodorant effect and fragrance lasts from the beginning to the end of use. The effect lasts for a... Read MoreSeries Deodorizing powerDiscontinued
- S.T. Deodorant plug type for tobaccoSince it is an outlet type, it deodorizes large rooms such as LDK (about 16 tatami mats) and continuous spaces such as entrances and corridors with electronic power, and the scent spreads. A constant deodorant effect and fragrance lasts from the beginning to the end of use. The effect lasts for a... Read MoreFragrance Marine soap Series Deodorizing powerDiscontinued
- S.T. Deodorant plugIngredient Plant essential oils, flavors Quantity 20mL Capacity (mL) 20Discontinued
- S.T. Replace with deodorant plug typeA constant deodorant effect and fragrance lasts from the beginning to the end of use. The effect lasts for about 60 days when used 24 hours a day. (It depends on the usage situation.) It can also be used for all outlet type deodorant plugs.Series Deodorizing power Where to Use IndoorDiscontinued