Mascaras
- Sosu Masturbation for exclusive use of Bittreat MatsuekuDon't pull out your hair! A long glossy mascara that is loved by a single coat and can be applied evenly from the root to the tip of the hair with a single coat to create beautifully separated glossy long lashes. It is non-fiber and does not dry, and the film stretches smoothly, giving the fi... Read MoreColor Blackfrom S$17.99Min. 6 days
- Stella Seed Dazzle Carat MascaraA long mascara containing diamond (diamond powder: moisturizing) that gives a wet luster and improves the degree of moisture. "Long forming polymer" and extension fiber that blends well with eyelashes are entwined neatly up to the tips of the hair, and long and splendid long eyelashes a... Read Morefrom S$21.99Min. 6 days
- Sosu Masturbation for exclusive use of Bittreat MatsuekuBlack coating that fills the gap The black film naturally fills the gaps in the false eyelashes that have slipped out over time, giving a healthy luster. Separate without getting caught with a triangular brush Uses a triangle brush that prevents hair from getting caught in false eyelashes and reg... Read MoreColor Black brownfrom S$17.99Min. 6 days
- Spa treatment Beauty Rush + SensitiveEssence allergy tested beauty rush for patch re-eye makeup !! A type of eyelash serum that can be used by those who are concerned about their skin. It guides the eyes in a patchy and impressive way. Eyelash serum * It does not mean that allergies do not occur in all people.RoHS directive (corresponding to 10 substances) Correspondencefrom S$69.99Min. 6 days
- AVANCE AVANCE + False Eyelashes + Protect Mascara (Mascara for false eyelashes)from S$21.99Min. 5 days
- Spa treatment Beauty Rush + OriginResurrection of the old prescription Origin is the revival of the prescription that was the origin of Beauty Lush. It has re-appeared due to the voices of many patronage customers. It leads to more attractive eyes. Eyelash serumRoHS directive (corresponding to 10 substances) Correspondencefrom S$76.99Min. 6 days
- Picomonte Japan Picomonte DE eyebrow mascaraEasy to apply and doesn't stick to the skinDimensions, Width W x Height H x Depth D (mm) 101×173×41from S$11.99Min. 7 days
- Chez Moi Magical Liner Extension MascaraKeep beautiful eyelashes with a single coat without bleeding until night! Easy off with hot water! False eyelashes compatible mascara. * Carefully check that you have no abnormalities on your skin before using. * If the cosmetics do not suit your skin, that is, in the following cases, discontinue... Read MoreRoHS directive (corresponding to 10 substances) Correspondence Type Extension mascarafrom S$22.99Min. 6 days
- Spa treatment Beauty rush + mascaraEyes are perfect with mascara! The more you apply it, the more impressive your lashes will be, giving them firmness and elasticity, and giving them a natural luster and luster. mascaraRoHS directive (corresponding to 10 substances) Correspondencefrom S$66.99Min. 6 days
- ELIZABETH Vivo All-in MascaraThis one is a quick and mature beauty eyelash. With curl lock polymer, it curls upward all day long. Two types of fibers are entwined straight and long. Volume up with high adhesion smooth film prescription. Contains rush care complex. Originally developed brush without lumps. Easy and beautiful.... Read MoreColor BlackDiscontinued
- Kokuryudo Privacy + mascara curl + keep baseEliminates the problem of curling of eyelashes that fall off quickly! A curl-keeping base that can be removed with hot water for film mascara.Discontinued
- TOKIWA Pharmaceutical Sana Newborn W Mascara EXTwo functions with one, volume & long W function mascara is like +100 eyelashes! Volume mascara makes each one thicker and keeps curl! Long mascara can be stretched to any extent.Discontinued
- ISEHAN Heavy rotation extra long mascaraLong upward beauty with no lumps even when stacked.Color Rich blackDiscontinued