Cloth Rags
Cloth waste is a piece of cloth that is used as a rag to wipe off dirt during maintenance and cleaning of machines and equipment. Because of its excellent water absorption, it is used for wiping after car washing and machine maintenance in factories. A cloth waste called virgin waste made from an unused material. Recycled waste is the reuse of clothing that has already been used. Materials include elastic knitted fabrics, used pile fabrics, cotton, and polyester. Since the size is different, it can be selected according to the application.
Other Related Pages
- MonotaRO White Knitted Fabric Used FabricMade from used clothing from home. It is an excellent product among waste products. It is a recycled product. Cut. * Since used clothes are washed and then processed into waste cloth, a light bluish waste cloth may be mixed in due to the influence of the cleaning agent.Dimensions (cm) About 30-60 square Color White Classification second hand Type second hand
- YOSHIKAWA SANGYO Wet towel AA 100% cotton recycled waste cloth that collects the leftovers of "Oshibori" used in coffee shops. A well-shaped waste cloth with all four sides sewn. Hard fabric is for the part where you want to remove dirt firmly. Use soft linen where you don't want to scratch it. * Items other t... Read MoreType A Dimensions (cm) About 30 square RoHS directive (corresponding to 10 substances) Correspondence Material Cotton Classification second hand
- MonotaRO Knitted waste, no nails typeSince new knitted fabric is bleached and washed, it is hygienic and has excellent moisture and oil absorption. However, the elasticity and absorbency of fibers are slightly inferior to those of used products. * Since it is commercialized as a new fabric, its moisture absorption is slightly inferior.Dimensions (cm) About 30-50 square Classification Brand new Type Brand new Type of Fabric Knitting Color White
- MonotaRO White Wipes Used FabricIt absorbs oil and water and is white even when using a solvent, so you can use it without worrying about color stains. Because it is a Y-shirt material, its absorbency and wiping ability are slightly inferior to those of white knitted fabrics, but its white color makes it suitable for final fini... Read MoreDimensions (cm) About 30-60 square Color White Classification second hand Type second hand
- MonotaRO Used fabricMade from used clothing from home. (T-shirts and polo shirts) * Not suitable for work using solvents.Dimensions (cm) About 30-60 square Mass (g) Approximately 100 (per sheet) Color Assorted colors (pastel) Material T-shirt, polo shirt, trainer Classification second hand Type second hand
- OHTSUKA BRUSH MFG. T luxury knitted fabricA brand new white knitted fabric with carefully selected fabrics generated during the T-shirt production process. As it is an ALL knit fabric, it has a soft touch and excellent hygroscopicity. The absorbency of pure water is lower than that of recycled waste, but it is most suitable for the absor... Read MoreDimensions (cm) About 45 × 50 Type Brand new Classification Brand new RoHS directive (corresponding to 10 substances) Correspondence Type of Fabric Knitting Color White
- TAKADA SHOJI Maintenance waste for pure cotton knitting proThe size of a general waste cloth is often about 30 cm x 50 cm, and the size of this product is not a standard size, but it is about 20 cm x 20 cm in the palm size, so it is easy to use and there is no waste. It can be used for a wide range of purposes such as cleaning printing machines and vendi... Read MoreMaterial 100% cotton Dimensions (cm) About 20 × 20 Type Brand new Classification Brand new Type of Fabric Knitting Color White
- MonotaRO Shimaues NishikiuesLow cost and can be used for any work except solvent work. Y-shirts, sheets, sweatshirts, etc. are used. * Not suitable for work using solvents.Color Assorted colors (pastel)
- AS ONE Towel Waste ClothA pile cloth made by cutting towels, bath towels, etc., and has excellent absorbency.Classification second hand
- MonotaRO Knitted cloth Tsugihagi typeA price-oriented new white knitted fabric made by sewing 3 to 5 pieces of fabric into one piece. For wiping off oil, solvent, and ink. * Since new fabrics are spliced together and commercialized, the elasticity and absorbency of the fibers are slightly inferior to those of used products.Dimensions (cm) About 30-50 square Type Brand new Classification Brand new Type of Fabric Knitting Color White
- MonotaRO Knitted waste dark used fabricSince it is low cost, it is suitable for cleaning where a large amount of waste is used and for wiping off waste oil. * Not suitable for work using solvents. * Absorption and wiping are slightly inferior to color knitting.Dimensions (cm) About 30-60 square Color Mainly dark colors such as black. Type second hand Classification second hand
- AS ONE White Towel Waste ClothA waste cloth made by cutting towels, bath towels, etc., and has excellent water absorption and oil absorption.As ONE Part Number 3-7275-01 Type 75×35cm Classification second hand
- ESCO 2.2kg SheetwesA recycled waste cloth made from sheets.Dimension (mm) Approximately 508 x 635 (Hagire) Mix Rate (%) Cotton 70, polyester 30 Esco Part No. EA929AC-1
- TAKADA SHOJI 1 kg of new cherry knitted screen wasteA one-piece type with 100% cotton white knitted cloth and no seams. It has a soft texture and excellent water absorption. The size is about 40 x 40 cm, which is ideal for wiping paint, water, oil, etc.Material 100% cotton Dimensions (cm) About 40 × 40 Type Brand new Classification Brand new Type of Fabric Knitting Processing method Pack packaging and bleach cleaning Color White
- TRUSCO Knitted cloth (flexible type)Uses the finest knitted fabric carefully selected. Excellent water absorption !! The best feeling of use like tissue. It has a soft texture and does not scratch the product. A versatile type that is ideal for finishing processes and all kinds of workThickness (mm) 0.4 Trusco Part No. 215-3572 Dimension (mm) 350×350 Quantity (Sheets) Approx. 60 (1 bag) Classification Brand new Type of Fabric Knitting Color White
- ESCO 9.1kg Sheet wasteA recycled waste cloth made from sheets.Dimension (mm) Approximately 508 x 635 (Hagire) Mix Rate (%) Cotton 70, polyester 30 Esco Part No. EA929AC-4
- Handy Crown Professional wasteUses 100% high-grade cotton. Excellent water absorption and water retention! The soft, high-grade knitted fabric makes it easy to wipe off water, oil, and paint. Painting work, maintenance work, WAX finishingMaterial 100% cotton Dimension (mm) 400×500 RoHS directive (corresponding to 10 substances) Correspondencefrom S$12.99Min. 2 days
- YOSHIKAWA SANGYO YK Finest Knitted WoolIt is an unused fabric that came out when T-shirts were produced. * Since it is commercialized as a new fabric, its moisture absorption is slightly inferior.Type Brand new Dimensions (cm) 20 × 40 or more Classification Brand new Type of Fabric Knitting Color White
- TRUSCO α knitted waste (general-purpose type)A knitted cloth that can be used for all purposes. It is hygienic because the fabric is bleached and washed. The thickness is about 0.55 mm. Machine maintenance, oil wiping, etc.Thickness (mm) 0.55 Material 100% cotton (unused knitted fabric) Dimension (mm) 350×350 Classification Brand new Type of Fabric Knitting Color White
- AS ONE Knitted Waste ClothSince it is knitted with knitting, it has good elasticity and is suitable for wiping off moisture, oil and dirt.As ONE Part Number 3-1813-31 Type of Fabric Knitting Type White new goods 2kg
- Clean Cherry Pure cotton color knit + maintenance wasteUses cut knitted fabric from a famous Japanese underwear maker. Easy-to-use palm size! Since it is pure cotton, it can be used for a wide range of purposes, from polishing products to wiping dirt. Ideal for wiping printing equipment, vending machines, and small itemsMaterial 100% cotton Dimensions (cm) 20×20 Type of Fabric Knitting Size Palm sizefrom S$5.89Min. 2 days
- MonotaRO Dark colored cloth Used clothAlthough it has poor absorbency, its cost is low and it is suitable for work that uses a large amount of heavy oil, oil, etc. regardless of the cotton content. We use thick plain weave fabrics such as jeans, work clothes, shirts, trousers, and kimono. It is the cheapest in the waste. * Not suitab... Read MoreDimensions (cm) About 30-60 square Color Miscellaneous color (dark color) Type second hand Classification second hand
- AS ONE Oshibori Waste ClothIt is a towel cloth towel cloth. Since there are no cut points, there is little fraying. * Since the used hand towels are washed and treated with a waste cloth, there may be some stains.Dimension (mm) 300-500 square Material Cotton, synthetic fiber Color White
- COSCHEM Stainless Steel Cloth Tresimmon Cloth[Stainless steel cloth] Tresimon cloth, which is an ultra-fine fiber with a thickness of about 1/300 of that of hair, uses a unique amount of fiber and weave to prevent unevenness in the hairline and vibration-processed stainless steel material. Increase efficiency. We recommend that you use it i... Read MoreDimension (mm) 300×400 Type of Fabric Microfiber Material Polyesterel, nylon
- Handy Crown HC Special Knitted Cloth 1KGUses 100% cotton fabric with excellent water absorption. For painting work, cleaning work, oil wiping work, and tool / parts polishing work.Material 100% cotton Classification Brand new RoHS directive (corresponding to 10 substances) Correspondence Specification There is a toothpick Color White
- AX BRAIN HypercrossMade of 100% cotton, the soft texture is ideal for vulnerable surfaces. Excellent wiping property (wide dry property) of water and oil. Since it is made of 100% natural cotton, there is no need to worry about static electricity. Even if it contains liquid, it has almost the same strength as when ... Read MoreSize Per Sheet (mm) 280×400 Color White Material cotton
- TAKADA SHOJI Eco Maple Sarashi Recycled Towel WasteEco-friendly eco-waste! Because it is a towel material, it has a soft texture and excellent water absorption. For wiping paint, water and oilMaterial 100% cotton Dimensions (cm) Approx. 30 × 60 (irregular) Color Sarashi Classification second hand
- ESCO Cotton wasteMass (kg) (1 box) 5 Material 100% cotton Size (mm) About 400 × 450 Quantity (Sheets) Approximately 100 to 110 sheets Classification Brand new Esco Part No. EA929B-2
- Hayashi Shoji Bath mat wasteIt may contain a slight mixture of synthetic fibers, but the main material is a highly absorbent fabric. Ideal for wiping off large amounts of ink and oil stains. It is also reused as a mat for absorbing overflowed sewage and for removing terrible mud stains on shoe soles at civil engineering and... Read MoreDimensions (cm) About 30 x about 40 Classification second handfrom S$44.99Min. 2 days
- AS ONE White Knitted Waste Cloth (Economy) WhiteIt is a product with excellent cost performance. Since it is knitted with knitting, it has good elasticity and is suitable for wiping off moisture, oil and dirt. It also contains Kanoko dough and has excellent water absorption.Type 1 set (2kg x 5 bags) As ONE Part Number 3-1815-02 Classification second handfrom S$85.99Min. 2 days
- Asahipen White waste (recycled fabric)Wipe off paint and oil stains * Do not pile up oil-based paint, lacquer-based paint, or waste cloth from which oil has been wiped off, as there is a risk of spontaneous combustion, and do not pack it in a container or bag. Be sure to soak the waste cloth used for these in water and dispose of it ... Read MoreRoHS directive (corresponding to 10 substances) Correspondence Classification second hand
- Hayashi Shoji Bath towel cut wasteAs it is a recycled bath towel, it has excellent water absorption. It is easy to use because it is about 42 x 34 in size.Dimensions (cm) About 42 x about 34 Color Assorted Material Recycled bath towels Classification second handfrom S$55.99Min. 2 days
- YOSHIKAWA SANGYO Pure Cotton Knit ClothSize 500g RoHS directive (corresponding to 10 substances) Correspondence Type of Fabric Knitting
- No Brand KnitwessIdeal for car / motorcycle maintenance for all work in the factory (printing, painting, sheet metal, car cleaning, etc.). It's soft and fluffy, and it's easy to use. Can be washed and reused. It does not easily generate lint and has excellent water absorption and oil absorption. It is a s... Read MoreMaterial 100% cotton knitted fabric Dimension (mm) About 200 × 400 Classification Brand newfrom S$21.99Min. 2 days
- Asahipen Towel cloth (recycled fabric)Wipe off paint and oil stains * Colored patterns are mixed. * Do not pile up oil-based paint, lacquer-based paint, or waste cloth from which oil has been wiped off, as there is a risk of spontaneous combustion, and do not pack it in a container or bag. Be sure to soak the waste cloth used for the... Read MoreRoHS directive (corresponding to 10 substances) Correspondence Classification second hand
- AS ONE White Waste ClothAs ONE Part Number 3-1817-01 Material Cotton, synthetic fiber Color White Classification second handfrom S$64.99Min. 4 days
- AS ONE Knitted Waste Cloth Light Color SetA knitted cloth suitable for wiping off moisture, oil, dirt, etc.Type (2kg x 5 bags) As ONE Part Number 3-1865-11 Classification second handfrom S$64.99Min. 4 days
- TAKADA SHOJI Sakura new knitted screen waste cloth 1kg100% cotton white knitted cloth, sewn type with no stitches. It has a soft texture and excellent water absorption. The size is about 40 x 40 cm, which is ideal for wiping paint, water, oil, etc.Material 100% cotton Dimensions (cm) About 40 × 40 Classification Brand new Type Brand new Type of Fabric Knitting Processing method Pack packaging and bleach cleaning Color Whitefrom S$17.99Min. 2 days
- ESCO 2.2kg towel wasteA recycled waste cloth for high-class towels.Dimension (mm) Approximately 381 x 610 (Hagire) Esco Part No. EA929AC-2 Mix Rate (%) cotton 100from S$63.99Min. 2 days
- Mitani Gloves Cotton pile wasteCotton pile waste that is durable and hard to tear because the fabric is layeredDimensions (cm) 30×30 Standard Mass (g) About 850 Classification Brand new Material Cottonfrom S$29.99Min. 2 days
Filter by categories