Fishing Floats
- NISHIMURA KP floatStyrofoam float with extremely large buoyancy. It is not affected by seawater and rainwater. It is strongly and evenly filled to the inside, there is no worry of flooding and sinking, and buoyancy does not decrease. It is light, so it is very easy to carry and move. About with band ・ The band so... Read More
- Intercom Marine Foam Float (EVA Float)It is a buoy mainly used for fishing, and the material is vinyl acetate resin (EVA). It has excellent impact resistance and durability, there is almost no concern about cracks, and it has no water absorption. Unlike air fenders, all floats are urethane-like and have no puncture, so they can be us... Read More
- Aiwa Sangyo High top float PE orangeMaterial PE (polyethylene) resin Color Orangefrom S$36.99Min. 2 days
- Chuo Kasei Polyten floatEVA resin (ethylene vinyl acetate copolymer) is used, It is highly elastic, has strong impact resistance, and has excellent flexibility, so there is no need to worry about cracks or cracks. In addition, there is no damage in the lifting net machine. It has excellent weather resistance, has stable... Read MoreColor yellow Allowable Tolerance ±5%
- Intercom Marine Foam float (EVA float) 3 linkedIt is a buoy mainly used for fishing, and the material is vinyl acetate resin (EVA). It has excellent impact resistance and durability, there is almost no concern about cracks, and it has no water absorption. Unlike air fenders, all floats are urethane-like and have no puncture, so they can be us... Read More
- BMO Japan Sea anchor floatIf you attach the float to the sea anchor's collection rope, you can easily find the collection rope at the time of collection. A set of floats and recovery ropes.Mass (g) 100 Dimension (mm) 76×126 Included Accessories Rope (diameter: Φ6mm, length: 5m) Hole diameter (inch) Rope hole: 3/8from S$25.99Min. 2 days
- Chuo Kasei Polyten float red / whiteYellow is the standard EVA float, a special production color. EVA resin (ethylene vinyl acetate copolymer) is used, It is highly elastic, has strong impact resistance, and has excellent flexibility, so there is no need to worry about cracks or cracks. In addition, there is no damage in the liftin... Read Morefrom S$47.99Min. 7 days
- NISHIMURA KP float (with cover, band, pipe)Styrofoam float with extremely large buoyancy. A pipe (inner diameter 28 mm) is passed through the center, so you can use it with a rope etc. through it. It is not affected by seawater or rainwater.・ There is no need to worry about sinking and the buoyancy does not decrease. It is light, so it i... Read MorePipe inner diameter (Φmm) 28from S$299.90Min. 13 days
- KONDOTEC Viny (water resistant float) T-type ABSIt has strong pressure resistance, is lightweight and exhibits the required performance when used under water pressure. Bottom trawling and gillnet * The water depth is a guideline value, not a guaranteed value. * The usage limit water depth is set as standard for repeated use with a continuous p... Read MoreMaterial ABSfrom S$269.90Min. 6 days
- KONDOTEC Vinylon (Float for water surface) G type (T)It is lightweight and has high buoyancy performance due to the innumerable fine bubbles existing inside the main body. Since all bubbles are independent, seawater does not penetrate into the main body even if the surface is scratched, and buoyancy is maintained. Stationary, purse seine, etc.from S$299.90Min. 6 days
- KONDOTEC Binny (water pressure float) B type ABSIt has strong pressure resistance, is lightweight and exhibits the required performance when used under water pressure. Bottom trawling / stationary * The water depth is a guideline value, not a guaranteed value. * The usage limit water depth is set as standard for repeated use with a continuous ... Read MoreMaterial ABSfrom S$399.90Min. 6 days
- KONDOTEC Binny (water resistant float) B type PEIt has strong pressure resistance, is lightweight and exhibits the required performance when used under water pressure. Stationary / bottom net * The water depth is a guideline value, not a guaranteed value. * The usage limit water depth is set as standard for repeated use with a continuous press... Read MoreWater depth (m) 200 Material Made of polyethylenefrom S$369.90Min. 6 days
- Aiwa Sangyo Float urethane spray for sign lightsUrethane material is sprayed and painted on the styrofoam material to harden it, and a marker light can be attached to the hole 46 mm to use it as a float.Color Orange Thickness (mm) 50 Material Metal / stainless steel Diameter (Φmm) 250 Hole Diameter (Φmm) 46from S$179.90Min. 6 days
- KONDOTEC Vinylon (Float for water surface) M typeIt is lightweight and has high buoyancy performance due to the innumerable fine bubbles existing inside the main body. Since all bubbles are independent, seawater does not penetrate into the main body even if the surface is scratched, and buoyancy is maintained. Fender Bondenfrom S$499.90Min. 6 days
- KONDOTEC Binny (water resistant float) A type ABSIt has strong pressure resistance, is lightweight and exhibits the required performance when used under water pressure. Bottom trawl * The water depth is a guideline value, not a guaranteed value. * The usage limit water depth is set as standard for repeated use with a continuous pressure time of... Read MoreMaterial ABSfrom S$369.90Min. 6 days
- KONDOTEC Vinylon (Float for water surface) A, K typeIt is lightweight and has high buoyancy performance due to the innumerable fine bubbles existing inside the main body. Since all bubbles are independent, seawater does not penetrate into the main body even if the surface is scratched, and buoyancy is maintained. Fender Bondenfrom S$499.90Min. 6 days
- KONDOTEC Binny (water pressure float) G type ABSIt has strong pressure resistance, is lightweight and exhibits the required performance when used under water pressure. Stationary / aquaculture / harbor civil engineering * The water depth is a guideline value, not a guaranteed value. * The usage limit water depth is set as standard for repeated... Read MoreMaterial ABSfrom S$479.90Min. 6 days
- KONDOTEC Vinylon (Float for water surface) T typeGillnet, small stationary, etc.from S$389.90Min. 33 days
- KONDOTEC Orange float type 5 upper and lower earsIt is used for fixed nets, beaches, mooring, etc. * It is a simple float. There is no pressure resistance. Water depth 0m * The product diagram is for reference only. Different from the actual product.Specification Ear position: Upper and lower ears Color Orange Material PE resinfrom S$229.90Min. 6 days
- KONDOTEC Vinylon (Float for water surface) S typeIt is lightweight and has high buoyancy performance due to the innumerable fine bubbles existing inside the main body. Since all bubbles are independent, seawater does not penetrate into the main body even if the surface is scratched, and buoyancy is maintained. Fender Bondenfrom S$229.90Min. 6 days
- KONDOTEC Binny (water resistant float) T type PEIt has strong pressure resistance, is lightweight and exhibits the required performance when used under water pressure. Stationary / bottom net * The water depth is a guideline value, not a guaranteed value. * The usage limit water depth is set as standard for repeated use with a continuous press... Read MoreWater depth (m) 100 Type 12T1B Buoyancy (kg) 19.7 Weight (kg) 3.22 Diameter (mm) 310 Length (mm) 402 Hole Diameter (mm) 50 Material Made of polyethylenefrom S$459.90Min. 6 days
- KONDOTEC Vinylon (Float for water surface) T type (T)Gillnet, small stationary, etc.from S$379.90Min. 6 days
- No Brand BuoyJIS-F3308 compliant product A buoy used to identify the location of a ship's anchor. * Iron material is painted. If seawater gets inside due to rust, etc., discontinue use and replace with a new one.Overall Length (mm) (Excluding eye) 500 Diameter (Φmm) 300 Mass (kg) About 3.12 Specification Usage (top / bottom) red / whitefrom S$259.90Min. 7 days
- Aiwa Sangyo Float Cover for # 400Styrofoam float replacement cover Since it is 14 x 14 driven, it is durable and long-lasting. It can be used not only as a replacement cover but also as a bag for storing nets etc. Styrofoam float (aquaculture, marine civil engineering, etc.) cover replacement, storage bag for fishing gear, etc. ... Read MoreRoHS directive (corresponding to 10 substances) Correspondence Suitable Size (mm) Float size: Φ680 × 1150from S$29.99Min. 8 days
- Aiwa Sangyo EVA Fishing Net FloatA float made of EVA material with excellent shock absorption. Since it is a foam, it will not puncture. By hanging from the ship, it receives impact and prevents damage to the hull. The mouth is reinforced to prevent damage to the mouth during lifting nets. Lightweight and easy to handle. Purse s... Read MoreRoHS directive (corresponding to 10 substances) Correspondence
- Intercom Marine Foam Float (EVA Float)It is a float mainly used for fishing, and the material is vinyl acetate resin (EVA). It has excellent impact resistance and durability, there is almost no fear of cracks, and it has no water absorption. Unlike air fenders, all floats are urethane-like and have no puncture, so they can be used ev... Read MoreBuoyancy (kg) 10 Mass (g/pack) 1500 Hole Diameter (Φmm) 50 Dimension (Φmm) About 250 dimensions (mm x Φ) Approx. 280 x 250 Material Made of vinyl acetate resin (EVA)from S$55.99Min. 2 days
- Aiwa Sangyo ABS bottom trawl floatA high-strength ABS float for bottom trawling. Polyethylene float can be used in deep areas where it breaks. With rope ears, it can be easily installed. Bottom pulling troll, fixed net, bottom net, gill net, longline * Even if the water is shallower than the water used, it may be damaged due to t... Read MoreRoHS directive (corresponding to 10 substances) Correspondencefrom S$77.99Min. 10 days
- Aiwa Sangyo Polyethylene floatA polyethylene float with good weather resistance and impact resistance. It can be used as a buoyancy material for various purposes such as marine civil engineering work and warning buoys at beaches other than fisheries and aquaculture. Rabbit ear (both ears) type that can be easily attached to r... Read MoreRoHS directive (corresponding to 10 substances) Correspondencefrom S$259.90Min. 11 days
- Zeni Lite Buoy Zeni firefly + solar cell type (shining float)It is a floating ball that emits light on the entire surface with a sense of perspective, presence, and three-dimensionality. It can be used in various places and applications such as the sea, lakes, dams, ponds, and rivers.Diameter (mm) 300 Mass (kg) About 3 Specification Light quality: 5 seconds 1 flash Lighting color Orange Rechargeable Battery Model Small seal lead acid battery (2V 2.5Ah) Output Solar cell output: 3.0V 0.28W Light Source Super bright LEDfrom S$1,199.00Min. 12 days
- Aiwa Sangyo UV float cover for # 300It is a replacement float cover with UV agent added to the raw material for long-term use at sea. The weather resistance saves the trouble of replacement compared to PE cross float cover. We are using Styrofoam float (aquaculture, marine civil engineering, etc.) cover replacement, storage bag for... Read MoreColor Black RoHS directive (corresponding to 10 substances) Correspondence Suitable Size (mm) Float size: Φ600 x 1050from S$49.99Min. 8 days
- DaiichiI Seimo Pneumatic Buoy Poly FoamPolyform A-series buoys / fenders that are highly trusted and acclaimed by fishermen and pleasure boat users around the world. The rope hold and seamless body structure reinforced with its characteristic rib structure are the reasons why it is loved by professional users all over the world, and t... Read MoreColor Redfrom S$119.90Min. 8 days
- Aiwa Sangyo EVA Fishing Float (Flat Type)It is a flat type float made of EVA that is used by attaching it to a rope or net. There are rope grooves on both upper and lower sides, so you can use it by sandwiching the float. It can also be used by attaching it to a bucket, bag, etc. It can also be used as a subsidence prevention float by a... Read MoreBuoyancy (kg) About 0.29 Dimensions (Length L x Width W x Thickness) (mm) About 210 x 60 x 38 Mass (g) About 50 Hole Diameter (mm) About 6 Width W x Depth (mm) Approximately 12 x 5 (rope groove) Color Whitefrom S$5.39Min. 8 days
- KONDOTEC Black High Top Float Type 3 One Ear / 2 EarsIt is used for fixed nets, beaches, mooring, etc. * It is a simple float. There is no pressure resistance. Water depth 0m * The product diagram is for reference only. Different from the actual product.Color Black Specification Ear position: one ear, two ears Material PE resinfrom S$189.90Min. 6 days
- Aiwa Sangyo Polyethylene Fishing Net Float Red / Yellow (1 Piece)A polyethylene float with good weather resistance and impact resistance. It can be used as a buoyant material for various purposes such as marine civil engineering work and warning buoys at beaches other than fishing and aquaculture. Rope ear (both ears) type It can be easily attached to ropes, e... Read MoreRoHS directive (corresponding to 10 substances) Correspondencefrom S$79.99Min. 9 days
- ZEXUS Wireless rechargeable float BrightOnFor popular fish species such as horse mackerel, rockfish, and hairtail, flight distance is one of the important factors that is directly linked to fishing results. Luminescent floats have existed in response to the requests of anglers who want to target highly active individuals in distant spots... Read MoreMass (g) 13 Dimension (mm) 25.0×51.2 Battery Capacity (mAh) 40(20×2) Lighting Time (hours) About 4-5 Buoyancy (g) Remaining: 2 Luminous body Ultra-compact high-brightness LEDfrom S$28.99Min. 8 days
- KONDOTEC Orange High Top Float Type 3 One Ear / 2 EarsIt is used for fixed nets, beaches, mooring, etc. * It is a simple float. There is no pressure resistance. Water depth 0m * The product diagram is for reference only. Different from the actual product.Specification Ear position: one ear, two ears Color Orange Material PE resinfrom S$189.90Min. 6 days