A wax-coated thread. It is waterproof and is mainly used when sewing sails and canvas.
For sale
* The length is about. It is not a guaranteed value. * Since the wax adhesion rate changes and the thickness of low-pulled yarn changes in summer and winter, we manage products by weight, not length.
This is a typical synthetic rope product that uses raw yarn that is melt-spun polyethylene resin. It has excellent cost performance and is used in all situations. It has a specific gravity of 0.95 and floats on water. It does not harden even when wet, does not lose strength, has excellent weather... Read More
It is a fiber with excellent weather resistance and chemical resistance, and it also has strength. A versatile thread. It has the property of shrinking when it gets wet with water.
As a tailoring thread for fishing nets. Creating a hand net, etc. As a little binding thread indoors and outdoors. D... Read More
Quantity per Set (pieces) (Number of twists) Thread Gauge 20 Mass (g) 500 string / thread type Twisted yarn
It is a fiber with excellent weather resistance and chemical resistance, and it also has strength. A versatile thread. It has the property of shrinking when it gets wet with water.
As a tailoring thread for fishing nets. Creating a hand net, etc. As a little binding thread indoors and outdoors. D... Read More
Height (mm) 105 / roll Mass (g) 200 Diameter (Φmm) 65 / vol string / thread type Twisted yarn
It is a fiber with excellent weather resistance and chemical resistance, and it also has strength. A versatile thread. It has the property of shrinking when it gets wet with water.
As a tailoring thread for fishing nets. Creating a hand net, etc. As a little binding thread indoors and outdoors. D... Read More
Height (mm) 105 / roll Mass (g) 200 Diameter (Φmm) 65 / vol string / thread type Twisted yarn
Uses raw yarn made by melt-spinning polypropylene resin. Along with polyethylene, it is a representative product of synthetic rope. It has a lighter specific gravity (0.91) than polyethylene and floats on water. It is a powerful and cost-effective product. In addition, since the rope has a low el... Read More
This is the original fluorocarbon line of Yamada Kogyo's original brand "Blue Fin". The original special processing improves transparency and wear resistance (strength against friction).
Fishing thread fishery
Uses PP (polypropylene). It is a 6-stroke braided rope. It is bobbin-wound and has a shape that makes it easy to pull out by passing a core rod through it.
Gillnet buoy rope, etc.
Spun (short fiber) nylon twisted yarn. It is a thread that is bulky, has a soft texture, and is easy to handle.
For gill nets and other net tailoring threads. As reinforcement and other binding threads. It goes well with marine dyes and can be dyed in your favorite color for decoration.
Spun (short fiber) nylon twisted yarn. It is a thread that is bulky, has a soft texture, and is easy to handle.
For gill nets and other net tailoring threads. As reinforcement and other binding threads. It goes well with marine dyes and can be dyed in your favorite color for decoration.
A "spun yarn" rope made of polyester material. It is one of the heaviest ropes in general synthetic ropes. It is also relatively strong in terms of durability and chemical resistance, and is one of the heavy and strong ropes as a whole. Among spun yarn ropes, this rope is the most unaff... Read More
Since lead is evenly contained in the core material, it is difficult to deform. A rope that is easy to tailor and easy to handle.
As a weight for fishing nets and a weight for booms.
Instead of bobbin winding, it is hung on cardboard.
Core Material Lead string / thread type Sink (weight) Material Tetoron
It has a double structure with a joint that gives strength to the center and a non-joint that gives flexibility to the surface.
It is used as a fishing line for inshore vessels.
Length Per Roll (m) 1000 Color Clear Material Nylon string / thread type Tegus
This is a twisted yarn made by applying Taslan processing to polyester filament. Compared to ordinary long fibers, the yarn is bulkier, more flexible, and more resistant to threading. In addition, it is a thread that stretches well when a nodule is made and is easy to handle.
As a net tailoring t... Read More
It is used to clean the rope by sliding the recessed part on the left and in the middle with a plate thickness of about 5 mm.
Fishing gear for onboard work
Material Made of iron Overall Length (cm) About 25
Easy to tailor, just attach the net. It is a product with even weight and good netting.
For gill nets, fixed nets, aquaculture nets, booms, and curtain weight cords.
Length (m) 100 Wire diameter (mm) 5 Mass (kg) 6 2018 Trusco page 6 1678 Trusco Part No. 829-1189 Color Black Packaging Drum winding Specification Drum winding Material Polyester, lead
It has a double structure with a joint that gives strength to the center and a non-joint that gives flexibility to the surface.
It is used as a fishing line for inshore vessels.
Length Per Roll (m) 1000 Color Gray Material Nylon string / thread type Tegus
This is the original nylon line of Yamada Kogyo's original brand "Blue Fin". The manufacturer's original special processing improves transparency and wear resistance (strength against friction).
Fishery fishing thread horticulture
* The photo is a transparent photo. Please refer... Read More
A general-purpose rope that is easy to tie, strong, and has excellent cost performance. It is a unique mix manufacturing method, and because it contains a large amount of polyethylene, it floats on water.
It is used for fixing luggage during transportation and for cargo handling. It is also used ... Read More
This is the original nylon line of Yamada Kogyo's original brand "Blue Fin". The manufacturer's original special processing improves transparency and wear resistance (strength against friction).
Fishery fishing thread horticulture
* The photo is a transparent photo. Please refer... Read More
A special composite yarn with a unique core-sheath structure that uses polyester filament as the core yarn and Cremona spun yarn (vinylon) as the sheath yarn. It is a yarn that combines the high strength, low elongation, and dimensional stability of polyester filament with the feel, ease of handl... Read More
Mass (kg / roll) 1 string / thread type Twisted yarn
This is the original nylon line of Yamada Kogyo's original brand "Green Fin". We have a lineup of transparent and yellow that birds dislike. Can also be used for other gardening
Fishing thread horticulture agriculture
Due to its water absorption, it deteriorates relatively quickly. Also, it is vulnerable to ultraviolet rays and friction, but the unit price is relatively low.
Used for fishing
* If you do not have a fishing right, you will be punished by law. In some areas, the size of the mesh that can be used ... Read More
Thickness (mm) 0.284 Number No. 3 Thread Thickness (mm) 0.284 Color Blue GG
Due to its water absorption, it deteriorates relatively quickly. Also, it is vulnerable to ultraviolet rays and friction, but the unit price is relatively low.
Used for fishing
* If you do not have a fishing right, you will be punished by law. In some areas, the size of the mesh that can be used ... Read More
Thickness (mm) 0.234 Thread Thickness (mm) 0.234 Number No. 2 Color Blue GG
A rope with excellent strength, weather resistance and flexibility using high quality polyester spun yarn. It is a very comfortable rope that uses spun yarn. A convenient rope that does not harden even when it gets wet.
Basket fishing (trunk rope, branch rope), bottom tow net, anchor rope, moorin... Read More
Length (m) 200 RoHS directive (corresponding to 10 substances) Correspondence Material Polyester (spun yarn) Color With white / blue line string / thread type rope
High-quality fluorocarbon tegus for professionals exclusively for fishermen The surface is treated with fluorine to maintain water-repellent, antifouling, and scratch-proof effects. The refractive index of light is close to that of water, so it dissolves in water and becomes difficult to see. Hig... Read More
Length (m) 100 Shape 100m spool x 5 connection RoHS directive (corresponding to 10 substances) Correspondence string / thread type Tegus Color Transparent
Floats on water (specific gravity 0.95) -Resistant to friction in water-Power does not decrease even when wet-Excellent weather resistance and flexibility does not change
Fisheries / Fisheries / Ships = Aquaculture cages, rafts, fixed nets, etc. Land = Golf nets, batting nets, goal nets, etc.
* ... Read More
Material Polyethylene Color White string / thread type rope
A rope made of high-strength polyethylene. It is a lightweight and easy-to-use rope that does not absorb water.
For aquaculture (float binding, raft connection, hanging rope, etc.), for various fisheries, for ships. Various multipurpose uses such as agriculture and forestry
* It is a non-heat-tre... Read More
Length (m) 200 Color Black RoHS directive (corresponding to 10 substances) Correspondence Material Polyethylene string / thread type rope
An ultra hybrid line rope, a new item rope from Intercom Marine's flagship line. A rope made of high molecular weight polyethylene, commonly known as Dyneema rope, which is thin but strong and is used as a mooring rope for super-large ships of 250,000 to 300,000 tons. This ultra hybrid line r... Read More