Boat Fender
Other Related Pages
- Intercom Marine Air fender twin eyeIt is a fender that is mainly produced and sold for Europe and the United States, and the product is packed with many years of experience and achievements. It is a low-priced, high-quality recommended product that has been highly evaluated by customers. This twin-eye type air fender has rope moun... Read More
- Intercom Marine Fender ropeA rope for fenders made from a high-strength and highly durable double-blade polyester rope. This product has eye processing (eye size is about 60 mm) on one end, so it can be easily attached without tying it to various fenders. Available in white and navy.Rope Diameter (Φmm) 10 Length (m) 2 Dimension (mm) Eye: 60
- Intercom Marine Air fender with twin eye coverIt is a fender that is mainly produced and sold for Europe and the United States, and the product is packed with many years of experience and achievements. It is a low-priced, high-quality recommended product that has been highly evaluated by customers. This twin-eye type air fender has rope moun... Read MoreType (Cover) Standard
- BMO Japan Air fenderIt is an air fender made of PVC. Ideal for small and medium-sized boats. It absorbs shocks flexibly and protects the boat safely.from S$29.99Min. 2 days
- Intercom Marine Air fender twin eye with premium coverIt is a fender that is mainly produced and sold for Europe and the United States, and the product is packed with many years of experience and achievements. It is a low-priced, high-quality recommended product that has been highly evaluated by customers. This twin-eye type air fender has rope moun... Read MoreType (Cover) Premium Color (Body) White
- Intercom Marine Air fender drop eye (tears)It is a round type (tear type) conical fender made by Intercom, and the color is a two-tone color of navy and white. It is heavy-duty, thick, and boasts high strength, so please use it for the bow flare part of the boat.Hole Diameter (Φmm) 20from S$67.99Min. 7 days
- Intercom Marine Premium twin eye air fenderIt is a fender that is mainly produced and sold for Europe and the United States, and the product is packed with many years of experience and achievements. It is a low-priced, high-quality recommended product that has been highly evaluated by customers. This twin-eye type air fender has rope moun... Read MoreSuitable Size 25ft~35ft Hole Diameter (Φmm) 20 Color (Body) White / navyfrom S$79.99Min. 7 days
- BMO Japan No punk fenderThe ultimate no-punk fender that protects the boat from severe impact. Ideal for large boats and commercial boats.
- Intercom Marine Pontoon fenderAn air fender installed at the pier corner of the marina. The probability of damaging the hull is highest when berthing, but with this bumper, you can safely berth at the pier alone, if you are a beginner and you are not confident in maneuvering, or when the wind is strong. You can berth without ... Read MoreMaterial PVCfrom S$42.99Min. 2 days
- Intercom Marine Boat fender holderA fender holder for pole type (pipe clamp) mounting. A rust-resistant all-stainless steel holder with a silver color that grows vividly on the hull. It has a luxurious feel and is durable enough. The stainless steel material is SUS316, which has improved corrosion resistance and durability. (The ... Read MoreMaterial Stainless steel SUS316 Wearable diameter (mm) (Pipe clamp) 22-25from S$88.99Min. 7 days
- Intercom Marine Premium twin eye air fender with premium coverType (Cover) Premium Hole Diameter (Φmm) 20 Color (Body) Whitefrom S$119.90Min. 7 days
- Intercom Marine Fender adjuster strapA strap that allows you to attach the fender rope to the clamp rail. The strap comes with a roller bracket that can be adjusted in length and can be troweled at any position. Rope thickness can be used up to 12 mm. It can also be used as an adjustable mounting bracket for inflatable fenders. This... Read MoreDimension (mm) 40 Pipe Diameter (Φmm) up to 30from S$25.99Min. 7 days
- Intercom Marine Electric air pump ICHB1831 for inflatable fenderIn addition to inflatable fenders, this product is suitable for injecting (exhausting) relatively large inflatable vinyl products such as air beds and vinyl boats. For continuous use, use 15 minutes as a guide. (Intercom Marine's inflatable fender can be filled with air in about 1 minute on a... Read MorePower Input (V) AC100 for home use Included Accessories Various nozzlesfrom S$109.90Min. 2 days
- Intercom Marine Air fender center eyeA rope-penetrating fender with attractive fender effective dimensions. It is a best-selling standard fender that can be used by penetrating a rope and hanging it vertically and horizontally. An upgraded version with improved durability by using anti-UV additives and anti-curing agents.
- Intercom Marine Air dock bumperAn air fender installed on the pier of a marina. Attaching the accessories Set the attachment fittings and attach them to the rails of the marina pier for the best fit. The probability of damaging the hull is highest when berthing, but with this bumper, it is safe to berth alone at the pier, if y... Read MoreDimensions, Width W x Length L (mm) 180×900 Mass (kg) 4.5from S$189.90Min. 5 days
- Intercom Marine Air fender with center eye coverA rope-penetrating fender with attractive fender effective dimensions. It is a best-selling standard fender that can be used by penetrating a rope and hanging it vertically and horizontally. An upgraded version with improved durability by using anti-UV additives and anti-curing agents.Color (Cover) Navyfrom S$99.90Min. 7 days
- Intercom Marine Manual air pump ICHP01 for inflatable fenderManual air pump for inflatable fenders. The foot type can be filled with air from the fender. Although it is manual, it can be easily filled with air.Included Accessories Various nozzlesfrom S$47.99Min. 5 days
- Intercom Marine Air fender inflatable super seriesThis product was developed for mooring 100-foot class mega yachts in Europe and the United States. FRP ships require large air fenders, but since there is no space to store the air fenders, we devised an air fender that can be shrunk using the material of this inflatable boat. Material and streng... Read MoreColor (Body) Navyfrom S$449.90Min. 5 days
- Intercom Marine Air fender inflatableThis product was developed for mooring 100-foot class mega yachts in Europe and the United States. FRP ships require large air fenders, but since there is no space to store the air fenders, we devised an air fender that can be shrunk using the material of this inflatable boat. Material and streng... Read Morefrom S$259.90Min. 5 days
- Intercom Marine Air fender with drop eye coverIt is a round type (tear type) conical fender made by Intercom, and the color is a two-tone color of navy and white. It is heavy-duty, thick, and boasts high strength, so please use it for the bow flare part of the boat. With a cover that not only prevents the hull from getting dirty and darkened... Read MoreHole Diameter (Φmm) 20 Color (Cover) Navyfrom S$129.90Min. 7 days
- Intercom Marine Dock wheelIt is a very convenient dog wheel for berthing on a narrow pier in a marina or boat park. When the wind is strong, it is difficult to berth at the pier, and for a boat with one engine, it will be extremely difficult if a wind of 5 meters or more blows. In such a case, if you install it at the tip... Read MoreMaterial PVC, galvanized steel Mass (kg) 4.3 Diameter (Φmm) 300from S$239.90Min. 7 days
- KONDOTEC EVA fenderAbrasion resistance and tensile strength are outstanding strength. Since it is a closed cell, it is highly flexible and there is no need to worry about water absorption. It has excellent effects on cold resistance, Nikko ultraviolet rays, etc. and does not cause surface cracks. EVA fender is high... Read Morefrom S$189.90Min. 6 days
- Intercom Marine With premium twin eye air fender coverType (Cover) Standard Hole Diameter (Φmm) 20 Color (Body) White / navyfrom S$119.90Min. 7 days
- Aiwa Sangyo EVA hanging fenderA float made of EVA material with excellent shock absorption. Since it is a foam, it will not puncture. By hanging from the ship, it receives impact and prevents damage to the hull. The set includes all the necessary items such as ropes from the beginning, so you can use it immediately by tying i... Read MoreRoHS directive (corresponding to 10 substances) Correspondence Color Whitefrom S$85.99Min. 8 days
- Intercom Marine Air fender inflatable ultra seriesThis product was developed for mooring 100-foot class mega yachts in Europe and the United States. FRP ships require large air fenders, but since there is no space to store the air fenders, we devised an air fender that can be shrunk using the material of this inflatable boat. Material and streng... Read MoreColor (Body) Navyfrom S$2,699.00Min. 7 days
- No Brand Ship's Boat Fender (Poly Coir Rope Fender)Made by a skilled craftsman (domestic), woven with 9mm poly rope, and contains a sphere containing EVA rubber and sponge as cushioning material. Cushioning material (fender) suspended from the side of the ship to prevent damage to the hull when the ship berths * The sphere may be torn due to wear... Read Morefrom S$239.90Min. 2 days